Go to the source code of this file.
|
| int32_t | DSPLIB_min_getHandleSize (DSPLIB_min_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_min_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_min_InitArgs *pKerInitArgs) |
| | This function should be called before the DSPLIB_min_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_min_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_min_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to DSPLIB_min_init function. This function is called with the same parameters as the DSPLIB_min_init, and this function must be called before the DSPLIB_min_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_min_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn1, const void *restrict pOut) |
| | This function checks the validity of the parameters passed to DSPLIB_min_exec function. This function is called with the same parameters as the DSPLIB_min_init, and this function must be called before the DSPLIB_min_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_min_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| | This function is the main kernel compute function. More...
|
| |