![]() |
DSPLIB User Guide
|
Go to the source code of this file.
Macros | |
| #define | SE_PARAM_BASE (0x0000) |
| #define | SE0_PARAM_OFFSET (SE_PARAM_BASE) |
| #define | SE1_PARAM_OFFSET (SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | SA0_PARAM_OFFSET (SE1_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | SA1_PARAM_OFFSET (SA0_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | SA2_PARAM_OFFSET (SA1_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | DSPLIB_MATMUL_DOUBLE_UNROLL_FACTOR (8) |
| #define | DSPLIB_MATMUL_SE_DOUBLE_UNROLL_FACTOR (4) |
| #define | DSPLIB_MATMUL_FLOAT_UNROLL_FACTOR (16) |
| #define | DSPLIB_MATMUL_SE_FLOAT_UNROLL_FACTOR (8) |
Functions | |
| template<typename dataType > | |
| void | setUnrollFactors (int32_t *unrollFactor, int32_t *seUnrollFactor) |
| template<> | |
| void | setUnrollFactors< float > (int32_t *unrollFactor, int32_t *seUnrollFactor) |
| template<> | |
| void | setUnrollFactors< double > (int32_t *unrollFactor, int32_t *seUnrollFactor) |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_matMul_generic_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn0, const DSPLIB_bufParams2D_t *bufParamsIn1, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matMul_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_matMul_generic_init_ci< float > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn0, const DSPLIB_bufParams2D_t *bufParamsIn1, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matMul_InitArgs *pKerInitArgs) |
| template DSPLIB_STATUS | DSPLIB_matMul_generic_init_ci< double > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn0, const DSPLIB_bufParams2D_t *bufParamsIn1, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matMul_InitArgs *pKerInitArgs) |
| template<typename T , typename vec , uint32_t id> | |
| static vec | loadAMatSA (__vpred tmp, void *pIn) |
| template<typename T , typename vec > | |
| static void | writeOutSA1 (__vpred tmp, vec *addr, T pOut, vec out) |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_matMul_generic_core_ci (DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut) |
| template<> | |
| DSPLIB_STATUS | DSPLIB_matMul_generic_core_ci< double > (DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut) |
| template<> | |
| DSPLIB_STATUS | DSPLIB_matMul_generic_core_ci< float > (DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut) |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_matMul_generic_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_matMul_generic_exec_ci< float > (DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut) |
| template DSPLIB_STATUS | DSPLIB_matMul_generic_exec_ci< double > (DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut) |
| #define SE_PARAM_BASE (0x0000) |
Definition at line 52 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define SE0_PARAM_OFFSET (SE_PARAM_BASE) |
Definition at line 53 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define SE1_PARAM_OFFSET (SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 54 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define SA0_PARAM_OFFSET (SE1_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 55 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define SA1_PARAM_OFFSET (SA0_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 56 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define SA2_PARAM_OFFSET (SA1_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 57 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define DSPLIB_MATMUL_DOUBLE_UNROLL_FACTOR (8) |
Definition at line 59 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define DSPLIB_MATMUL_SE_DOUBLE_UNROLL_FACTOR (4) |
Definition at line 60 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define DSPLIB_MATMUL_FLOAT_UNROLL_FACTOR (16) |
Definition at line 62 of file DSPLIB_matMul_generic_size_ci.cpp.
| #define DSPLIB_MATMUL_SE_FLOAT_UNROLL_FACTOR (8) |
Definition at line 63 of file DSPLIB_matMul_generic_size_ci.cpp.
|
inline |
|
inline |
Definition at line 67 of file DSPLIB_matMul_generic_size_ci.cpp.
|
inline |
Definition at line 72 of file DSPLIB_matMul_generic_size_ci.cpp.
| DSPLIB_STATUS DSPLIB_matMul_generic_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn0, | ||
| const DSPLIB_bufParams2D_t * | bufParamsIn1, | ||
| const DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| const DSPLIB_matMul_InitArgs * | pKerInitArgs | ||
| ) |
Definition at line 79 of file DSPLIB_matMul_generic_size_ci.cpp.
| template DSPLIB_STATUS DSPLIB_matMul_generic_init_ci< float > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn0, | ||
| const DSPLIB_bufParams2D_t * | bufParamsIn1, | ||
| const DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| const DSPLIB_matMul_InitArgs * | pKerInitArgs | ||
| ) |
| template DSPLIB_STATUS DSPLIB_matMul_generic_init_ci< double > | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn0, | ||
| const DSPLIB_bufParams2D_t * | bufParamsIn1, | ||
| const DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| const DSPLIB_matMul_InitArgs * | pKerInitArgs | ||
| ) |
|
inlinestatic |
Definition at line 254 of file DSPLIB_matMul_generic_size_ci.cpp.
|
inlinestatic |
Definition at line 267 of file DSPLIB_matMul_generic_size_ci.cpp.
| DSPLIB_STATUS DSPLIB_matMul_generic_core_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn0, | ||
| void *restrict | pIn1, | ||
| void *restrict | pOut | ||
| ) |
|
inline |
Definition at line 284 of file DSPLIB_matMul_generic_size_ci.cpp.
|
inline |
Definition at line 494 of file DSPLIB_matMul_generic_size_ci.cpp.
| DSPLIB_STATUS DSPLIB_matMul_generic_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn0, | ||
| void *restrict | pIn1, | ||
| void *restrict | pOut | ||
| ) |
Definition at line 826 of file DSPLIB_matMul_generic_size_ci.cpp.
| template DSPLIB_STATUS DSPLIB_matMul_generic_exec_ci< float > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn0, | ||
| void *restrict | pIn1, | ||
| void *restrict | pOut | ||
| ) |
| template DSPLIB_STATUS DSPLIB_matMul_generic_exec_ci< double > | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn0, | ||
| void *restrict | pIn1, | ||
| void *restrict | pOut | ||
| ) |