DSPLIB User Guide
DSPLIB_lud_priv.h File Reference

Introduction

Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_lud.

Definition in file DSPLIB_lud_priv.h.

Go to the source code of this file.

Data Structures

struct  DSPLIB_lud_PrivArgs
 Structure that is reserved for internal use by the kernel. More...
 

Macros

#define DSPLIB_LUD_IXX_IXX_OXX_PBLOCK_SIZE   (22 * SE_PARAM_SIZE)
 Macro to define the size of bufPblock array of DSPLIB_lud_PrivArgs structure. More...
 

Typedefs

typedef DSPLIB_STATUS(* pFxnDSPLIB_lud_exec) (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pL, void *restrict pU, void *restrict pP)
 This is a function pointer type that conforms to the declaration of DSPLIB_lud_exec_ci and DSPLIB_lud_exec_cn. More...
 

Functions

template<typename dataType >
DSPLIB_STATUS DSPLIB_lud_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsA, const DSPLIB_bufParams2D_t *bufParamsL, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsP, const DSPLIB_ludInitArgs *pKerInitArgs)
 This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_lud_exec_ci (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pL, void *restrict pU, void *restrict pP)
 This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_exec. More...
 
DSPLIB_STATUS DSPLIB_lud_init_cn (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsA, const DSPLIB_bufParams2D_t *bufParamsL, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsP, const DSPLIB_ludInitArgs *pKerInitArgs)
 This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_lud_exec_cn (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pL, void *restrict pU, void *restrict pP)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_exec. More...
 

Macro Definition Documentation

◆ DSPLIB_LUD_IXX_IXX_OXX_PBLOCK_SIZE

#define DSPLIB_LUD_IXX_IXX_OXX_PBLOCK_SIZE   (22 * SE_PARAM_SIZE)

Macro to define the size of bufPblock array of DSPLIB_lud_PrivArgs structure.

Definition at line 38 of file DSPLIB_lud_priv.h.

Typedef Documentation

◆ pFxnDSPLIB_lud_exec

typedef DSPLIB_STATUS(* pFxnDSPLIB_lud_exec) (DSPLIB_kernelHandle handle, void *restrict pA, void *restrict pL, void *restrict pU, void *restrict pP)

This is a function pointer type that conforms to the declaration of DSPLIB_lud_exec_ci and DSPLIB_lud_exec_cn.

Definition at line 45 of file DSPLIB_lud_priv.h.

Function Documentation

◆ DSPLIB_lud_init_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_lud_init_ci ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams2D_t bufParamsA,
const DSPLIB_bufParams2D_t bufParamsL,
const DSPLIB_bufParams2D_t bufParamsU,
const DSPLIB_bufParams2D_t bufParamsP,
const DSPLIB_ludInitArgs pKerInitArgs 
)

This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_init.

This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_lud_exec_ci would be called later independently by the application. When DSPLIB_lud_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_lud_exec_ci does not lose cycles to determine the hardware configuration.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsA: Pointer to the structure containing dimensional information of input buffer A
[out]bufParamsL: Pointer to the structure containing dimensional information of output buffer L
[out]bufParamsU: Pointer to the structure containing dimensional information of output buffer U
[out]bufParamsP: Pointer to the structure containing dimensional information of output buffer P
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 59 of file DSPLIB_lud_ci.cpp.

◆ DSPLIB_lud_exec_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_lud_exec_ci ( DSPLIB_kernelHandle  handle,
void *restrict  pA,
void *restrict  pL,
void *restrict  pU,
void *restrict  pP 
)

This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_exec.

The function uses streaming engine to load data. The result is then stored at separate location using a streaming address generator.

Parameters
[in]handle: Active handle to the kernel
[in]pA: Pointer to matrix A
[out]pL: Pointer to lower triangular matrix L
[out]pU: Pointer to upper triangular matrix U
[out]pP: Pointer to permutation matrix P
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Performance Considerations:
For best performance,
  • the input and output data buffers are expected to be in L2 memory
  • the buffer pointers are assumed to be 64-byte aligned

Definition at line 976 of file DSPLIB_lud_ci.cpp.

◆ DSPLIB_lud_init_cn()

DSPLIB_STATUS DSPLIB_lud_init_cn ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams2D_t bufParamsA,
const DSPLIB_bufParams2D_t bufParamsL,
const DSPLIB_bufParams2D_t bufParamsU,
const DSPLIB_bufParams2D_t bufParamsP,
const DSPLIB_ludInitArgs pKerInitArgs 
)

This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_init.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsA: Pointer to the structure containing dimensional information of input buffer A
[out]bufParamsL: Pointer to the structure containing dimensional information of output buffer L
[out]bufParamsU: Pointer to the structure containing dimensional information of output buffer U
[out]bufParamsP: Pointer to the structure containing dimensional information of output buffer P
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 41 of file DSPLIB_lud_cn.cpp.

◆ DSPLIB_lud_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_lud_exec_cn ( DSPLIB_kernelHandle  handle,
void *restrict  pA,
void *restrict  pL,
void *restrict  pU,
void *restrict  pP 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_exec.

Parameters
[in]handle: Active handle to the kernel
[in]pA: Pointer to matrix A
[out]pL: Pointer to lower triangular matrix L
[out]pU: Pointer to upper triangular matrix U
[out]pP: Pointer to permutation matrix P
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 179 of file DSPLIB_lud_cn.cpp.