![]() |
DSPLIB User Guide
|
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_lud_inv.
Definition in file DSPLIB_lud_inv_priv.h.
Go to the source code of this file.
Data Structures | |
| struct | DSPLIB_lud_inv_PrivArgs |
| Structure that is reserved for internal use by the kernel. More... | |
Macros | |
| #define | DSPLIB_LUD_INV_IXX_IXX_OXX_PBLOCK_SIZE (10 * SE_PARAM_SIZE) |
| Macro to define the size of bufPblock array of DSPLIB_lud_inv_PrivArgs structure. More... | |
Typedefs | |
| typedef DSPLIB_STATUS(* | pFxnDSPLIB_lud_inv_exec) (DSPLIB_kernelHandle handle, void *restrict pP, void *restrict pL, void *restrict pU, void *restrict pinvA, void *restrict pScratch) |
| This is a function pointer type that conforms to the declaration of DSPLIB_lud_inv_exec_ci and DSPLIB_lud_inv_exec_cn. More... | |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_lud_inv_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsP, const DSPLIB_bufParams2D_t *bufParamsL, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsinvA, const DSPLIB_lud_invInitArgs *pKerInitArgs) |
| This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_init. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_lud_inv_exec_ci (DSPLIB_kernelHandle handle, void *restrict pP, void *restrict pL, void *restrict pU, void *restrict pinvA, void *restrict pScratch) |
| This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_exec. More... | |
| DSPLIB_STATUS | DSPLIB_lud_inv_init_cn (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsP, const DSPLIB_bufParams2D_t *bufParamsL, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsinvA, const DSPLIB_lud_invInitArgs *pKerInitArgs) |
| This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_init. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_lud_inv_exec_cn (DSPLIB_kernelHandle handle, void *restrict pP, void *restrict pL, void *restrict pU, void *restrict pinvA, void *restrict pScratch) |
| This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_exec. More... | |
| #define DSPLIB_LUD_INV_IXX_IXX_OXX_PBLOCK_SIZE (10 * SE_PARAM_SIZE) |
Macro to define the size of bufPblock array of DSPLIB_lud_inv_PrivArgs structure.
Definition at line 40 of file DSPLIB_lud_inv_priv.h.
| typedef DSPLIB_STATUS(* pFxnDSPLIB_lud_inv_exec) (DSPLIB_kernelHandle handle, void *restrict pP, void *restrict pL, void *restrict pU, void *restrict pinvA, void *restrict pScratch) |
This is a function pointer type that conforms to the declaration of DSPLIB_lud_inv_exec_ci and DSPLIB_lud_inv_exec_cn.
Definition at line 47 of file DSPLIB_lud_inv_priv.h.
| DSPLIB_STATUS DSPLIB_lud_inv_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsP, | ||
| const DSPLIB_bufParams2D_t * | bufParamsL, | ||
| const DSPLIB_bufParams2D_t * | bufParamsU, | ||
| const DSPLIB_bufParams2D_t * | bufParamsinvA, | ||
| const DSPLIB_lud_invInitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_init.
This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_lud_inv_exec_ci would be called later independently by the application. When DSPLIB_lud_inv_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_lud_inv_exec_ci does not lose cycles to determine the hardware configuration.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsP | : Pointer to the structure containing dimensional information of input buffer P |
| [in] | bufParamsL | : Pointer to the structure containing dimensional information of input buffer L |
| [in] | bufParamsU | : Pointer to the structure containing dimensional information of input buffer U |
| [out] | bufParamsinvA | : Pointer to the structure containing dimensional information of ouput buffer invA |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 204 of file DSPLIB_lud_inv_ci.cpp.
| DSPLIB_STATUS DSPLIB_lud_inv_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pP, | ||
| void *restrict | pL, | ||
| void *restrict | pU, | ||
| void *restrict | pinvA, | ||
| void *restrict | pScratch | ||
| ) |
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_exec.
The function uses streaming engine to load data in TRANSPOSE MODE. The result is then stored at separate location using a streaming address generator.
| [in] | handle | : Active handle to the kernel |
| [in] | pP | : Pointer to permutation matrix P |
| [in] | pL | : Pointer to lower triangular matrix L |
| [in] | pU | : Pointer to upper triangular matrix U |
| [out] | pinvA | : Pointer to inverse of A matrix |
| [in] | pScratch | : Pointer to scratch buffer |
Definition at line 2030 of file DSPLIB_lud_inv_ci.cpp.
| DSPLIB_STATUS DSPLIB_lud_inv_init_cn | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsP, | ||
| const DSPLIB_bufParams2D_t * | bufParamsL, | ||
| const DSPLIB_bufParams2D_t * | bufParamsU, | ||
| const DSPLIB_bufParams2D_t * | bufParamsinvA, | ||
| const DSPLIB_lud_invInitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_init.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsP | : Pointer to the structure containing dimensional information of input buffer P |
| [in] | bufParamsL | : Pointer to the structure containing dimensional information of input buffer L |
| [in] | bufParamsU | : Pointer to the structure containing dimensional information of input buffer U |
| [out] | bufParamsinvA | : Pointer to the structure containing dimensional information of ouput buffer invA |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 37 of file DSPLIB_lud_inv_cn.cpp.
| DSPLIB_STATUS DSPLIB_lud_inv_exec_cn | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pP, | ||
| void *restrict | pL, | ||
| void *restrict | pU, | ||
| void *restrict | pinvA, | ||
| void *restrict | pScratch | ||
| ) |
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_lud_inv_exec.
| [in] | handle | : Active handle to the kernel |
| [in] | pP | : Pointer to permutation matrix P |
| [in] | pL | : Pointer to lower triangular matrix L |
| [in] | pU | : Pointer to upper triangular matrix U |
| [out] | pinvA | : Pointer to inverse of A matrix |
| [in] | pScratch | : Pointer to scratch buffer |
Definition at line 180 of file DSPLIB_lud_inv_cn.cpp.