![]() |
DSPLIB User Guide
|
Definition in file DSPLIB_lud_inv.cpp.
Go to the source code of this file.
Functions | |
| int32_t | DSPLIB_lud_inv_getHandleSize (DSPLIB_lud_invInitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_lud_inv_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsP, const DSPLIB_bufParams2D_t *bufParamsL, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsinvA, const DSPLIB_lud_invInitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_lud_inv_init function. This function is called with the same parameters as the DSPLIB_lud_inv_init, and this function must be called before the DSPLIB_lud_inv_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_lud_inv_exec_checkParams (DSPLIB_kernelHandle handle, void *restrict pP, void *restrict pL, void *restrict pU, void *restrict pinvA, void *restrict pScratch) |
| This function checks the validity of the parameters passed to DSPLIB_lud_inv_exec function. This function is called with the same parameters as the DSPLIB_lud_inv_exec, and this function must be called before the DSPLIB_lud_inv_exec is called. More... | |
| DSPLIB_STATUS | DSPLIB_lud_inv_init (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsP, const DSPLIB_bufParams2D_t *bufParamsL, const DSPLIB_bufParams2D_t *bufParamsU, const DSPLIB_bufParams2D_t *bufParamsinvA, const DSPLIB_lud_invInitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_lud_inv_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_lud_inv_exec (DSPLIB_kernelHandle handle, void *restrict pP, void *restrict pL, void *restrict pU, void *restrict pinvA, void *restrict pScratch) |
| This function is the main kernel compute function. More... | |