|
| int32_t | DSPLIB_fir_getHandleSize (DSPLIB_fir_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_getSizes (const DSPLIB_fir_InitArgs *pKerInitArgs, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsFilter, DSPLIB_bufParams2D_t *bufParamsOut) |
| | This is a query function to calculate the sizes of input, filter and the output buffers. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsFilter, DSPLIB_bufParams2D_t *bufParamsOut, DSPLIB_fir_InitArgs *pKerInitArgs) |
| | This function should be called before the DSPLIB_fir_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsFilter, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_fir_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to DSPLIB_fir_init function. This function is called with the same parameters as the DSPLIB_fir_init, and this function must be called before the DSPLIB_fir_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut) |
| | This function is the main kernel compute function. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pFilter, const void *restrict pOut) |
| | This function checks the validity of the parameters passed to DSPLIB_fir_exec function. This function is called with the same parameters as the DSPLIB_fir_exec, and this function must be called before the DSPLIB_fir_exec is called. More...
|
| |
| void | DSPLIB_fir_perfEst (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsFilter, const DSPLIB_bufParams2D_t *bufParamsOut, uint64_t *archCycles, uint64_t *estCycles) |
| | This is a utility function that gives an estimate of the cycles consumed for the kernel execution. More...
|
| |