77 0,
"pKerPrivArgs->order: %d pKerPrivArgs->stride: %d pKerPrivArgs->strideCn: %d pKerPrivArgs->enableTest: %d\n",
115 const void *restrict pInA,
116 const void *restrict pOutU,
117 const void *restrict pMul)
122 if ((pInA == NULL) || (pOutU == NULL) || (pMul == NULL)) {
136 void *restrict pOutU,
151 status = pKerPrivArgs->
execute(handle, pInA, pOutU, pMul);
template DSPLIB_STATUS DSPLIB_cholesky_exec_ci< float >(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict pMulBuffer)
template DSPLIB_STATUS DSPLIB_cholesky_init_ci< float >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_cholesky_init_ci< double >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_cholesky_exec_ci< double >(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict pMulBuffer)
template DSPLIB_STATUS DSPLIB_cholesky_exec_cn< float >(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict multiplierPtr)
template DSPLIB_STATUS DSPLIB_cholesky_exec_cn< double >(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict multiplierPtr)
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_cholesky.
#define DSPLIB_DEBUGPRINTFN(N, fmt,...)
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
@ DSPLIB_ERR_NULL_POINTER
@ DSPLIB_ERR_INVALID_TYPE
DSPLIB_STATUS DSPLIB_cholesky_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pInA, const void *restrict pOutU, const void *restrict pMul)
This function checks the validity of the parameters passed to DSPLIB_cholesky_exec function....
int32_t DSPLIB_cholesky_getHandleSize(DSPLIB_cholesky_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_cholesky_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_cholesky_init function....
DSPLIB_STATUS DSPLIB_cholesky_exec(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict pMul)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_cholesky_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_cholesky_exec function is called....
A structure for a 2 dimensional buffer descriptor.
uint32_t data_type
Values are of type DSPLIB_data_type_e.
Structure containing the parameters to initialize the kernel.
int32_t strideCn
stride of output data in cn
int32_t stride
stride of input/output data in ci
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
int32_t enableTest
Flag to enable Positive definiteness check.
int32_t order
order of input data
Structure that is reserved for internal use by the kernel.
int32_t order
Order of input buffer for different batches DSPLIB_cholesky_init that will be retrieved and used by D...
pFxnDSPLIB_cholesky_exec execute
Function pointer to point to the right execution variant between DSPLIB_cholesky_exec_cn and DSPLIB_c...