DSPLIB User Guide
DSPLIB_cascadeBiquad_cn.cpp File Reference

Go to the source code of this file.

Functions

DSPLIB_STATUS DSPLIB_cascadeBiquad_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsFilterCoeff, DSPLIB_bufParams2D_t *bufParamsFilterVar, DSPLIB_bufParams2D_t *bufParamsOut, DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs)
 This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_cascadeBiquad_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_cascadeBiquad_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_cascadeBiquad_exec. More...
 
template DSPLIB_STATUS DSPLIB_cascadeBiquad_exec_cn< float > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut)
 

Function Documentation

◆ DSPLIB_cascadeBiquad_init_cn()

DSPLIB_STATUS DSPLIB_cascadeBiquad_init_cn ( DSPLIB_kernelHandle  handle,
DSPLIB_bufParams2D_t bufParamsIn,
DSPLIB_bufParams1D_t bufParamsFilterCoeff,
DSPLIB_bufParams2D_t bufParamsFilterVar,
DSPLIB_bufParams2D_t bufParamsOut,
DSPLIB_cascadeBiquad_InitArgs pKerInitArgs 
)

This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_cascadeBiquad_init.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[in]bufParamsFilterCoeff: Pointer to the structure containing dimensional information of filter coefficient buffer
[in/out]bufParamsFilterVar : Pointer to the structure containing dimensional information of filter variable buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 31 of file DSPLIB_cascadeBiquad_cn.cpp.

◆ DSPLIB_cascadeBiquad_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_cascadeBiquad_exec_cn ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pFilterCoeff,
void *restrict  pFilterVar,
void *restrict  pOut 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_cascadeBiquad_exec.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to buffer holding the input data
[in]pFilterCoeffPointer to buffer holding the filter coefficient data
[in]pFilterVar: Pointer to buffer holding the filter variable data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 43 of file DSPLIB_cascadeBiquad_cn.cpp.

◆ DSPLIB_cascadeBiquad_exec_cn< float >()

template DSPLIB_STATUS DSPLIB_cascadeBiquad_exec_cn< float > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pFilterCoeff,
void *restrict  pFilterVar,
void *restrict  pOut 
)