|
| template<uint32_t maskType> |
| c7x::uchar_vec | blk_eswap_mask () |
| |
| template<> |
| c7x::uchar_vec | blk_eswap_mask< DSPLIB_UINT16 > () |
| |
| template<> |
| c7x::uchar_vec | blk_eswap_mask< DSPLIB_UINT32 > () |
| |
| template<> |
| c7x::uchar_vec | blk_eswap_mask< DSPLIB_UINT64 > () |
| |
| template<typename dataType > |
| DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| | This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_init. More...
|
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< uint16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< uint32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< uint64_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< int16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< int32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< int64_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< float > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_init_ci< double > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs) |
| |
| template<typename dataType , uint32_t maskType> |
| DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| | This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_exec. More...
|
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< uint16_t, DSPLIB_UINT16 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< uint32_t, DSPLIB_UINT32 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< uint64_t, DSPLIB_UINT64 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< int16_t, DSPLIB_UINT16 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< int32_t, DSPLIB_UINT32 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< int64_t, DSPLIB_UINT64 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< float, DSPLIB_UINT32 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_blk_eswap_exec_ci< double, DSPLIB_UINT64 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| |
template<typename dataType >
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_init.
This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_blk_eswap_exec_ci would be called later independently by the application. When DSPLIB_blk_eswap_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_blk_eswap_exec_ci does not lose cycles to determine the hardware configuration.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 351 of file DSPLIB_blk_eswap_ci.cpp.
template<typename dataType , uint32_t maskType>
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_exec.
The function uses one streaming engine to load the input data then endian swap operation is performed. The result is then stored using streaming address generator.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
- Performance Considerations:
- For best performance,
- the input and output data buffers are expected to be in L2 memory
- the buffer pointers are assumed to be 64-byte aligned
Definition at line 427 of file DSPLIB_blk_eswap_ci.cpp.