TIOVX User Guide
TI VPAC NF (Noise filter) Kernel APIs

Detailed Description

VPAC Noise Filter Kernels.

Modules

 Enumerations
 Enumerations for VPAC NF error events.
 

Data Structures

struct  tivx_vpac_nf_common_params_t
 The configuration data structure used by the TIVX_KERNEL_VPAC_NF_GENERIC and TIVX_KERNEL_VPAC_NF_BILATERAL kernels. More...
 
struct  tivx_vpac_nf_bilateral_params_t
 The configuration data structure used by the TIVX_KERNEL_VPAC_NF_BILATERAL kernel. More...
 
struct  tivx_vpac_nf_bilateral_sigmas_t
 The sigmas data structure used by the TIVX_KERNEL_VPAC_NF_BILATERAL kernel. More...
 
struct  tivx_vpac_nf_hts_bw_limit_params_t
 Configuration parameters used to set HTS BW limit used by TIVX_KERNEL_VPAC_NF kernel. More...
 

Defines

#define TIVX_KERNEL_VPAC_NF_GENERIC_NAME   "com.ti.hwa.vpac_nf_generic"
 vpac_nf_generic kernel name
 
#define TIVX_KERNEL_VPAC_NF_BILATERAL_NAME   "com.ti.hwa.vpac_nf_bilateral"
 vpac_nf_bilateral kernel name
 
#define TIVX_VPAC_NF_CMD_GET_ERR_STATUS   (0x10000002u)
 Control Command to get the combined error status Returns the combined error status of the last processed frame, incorporating error interrupts and watchdog timer error interrupt. A reference to vx_scalar is passed as an argument with this control command. The node returns a bit-mask of the error status in the U32 variable of vx_scalar. More...
 

Functions

void tivxRegisterHwaTargetVpacNfKernels (void)
 Function to register HWA Kernels on the vpac_nf Target.
 
void tivxUnRegisterHwaTargetVpacNfKernels (void)
 Function to un-register HWA Kernels on the vpac_nf Target.
 
VX_API_ENTRY vx_node VX_API_CALL tivxVpacNfGenericNode (vx_graph graph, vx_user_data_object configuration, vx_image input, vx_convolution conv, vx_image output)
 [Graph] Creates a VPAC_NF_GENERIC Node. More...
 
VX_API_ENTRY vx_node VX_API_CALL tivxVpacNfBilateralNode (vx_graph graph, vx_user_data_object configuration, vx_image input, vx_user_data_object sigmas, vx_image output)
 [Graph] Creates a VPAC_NF_BILATERAL Node. More...
 
void tivx_vpac_nf_common_params_init (tivx_vpac_nf_common_params_t *prms)
 Function to initialize NF common Parameters. More...
 
void tivx_vpac_nf_hts_bw_limit_params_init (tivx_vpac_nf_hts_bw_limit_params_t *prms)
 Function to initialize NF HTS bandwidth limit Parameters. More...
 
void tivx_vpac_nf_bilateral_params_init (tivx_vpac_nf_bilateral_params_t *prms)
 Function to initialize NF bilateral Parameters. More...
 
void tivx_vpac_nf_bilateral_sigmas_init (tivx_vpac_nf_bilateral_sigmas_t *sigmas)
 Function to initialize NF bilateral Sigmas. More...
 

Macro Definition Documentation

◆ TIVX_VPAC_NF_CMD_GET_ERR_STATUS

#define TIVX_VPAC_NF_CMD_GET_ERR_STATUS   (0x10000002u)

Control Command to get the combined error status Returns the combined error status of the last processed frame, incorporating error interrupts and watchdog timer error interrupt. A reference to vx_scalar is passed as an argument with this control command. The node returns a bit-mask of the error status in the U32 variable of vx_scalar.

  • Error interrupt status bits (0–29) are directly taken from the nf_obj->err_stat variable.
  • If watchdog timer error is detected (bit 26 in wd_err_status), this is flagged by setting bit 30 in the returned error status.

Definition at line 119 of file hwa_vpac_nf.h.

Function Documentation

◆ tivxVpacNfGenericNode()

VX_API_ENTRY vx_node VX_API_CALL tivxVpacNfGenericNode ( vx_graph  graph,
vx_user_data_object  configuration,
vx_image  input,
vx_convolution  conv,
vx_image  output 
)

[Graph] Creates a VPAC_NF_GENERIC Node.

Parameters
[in]graphThe reference to the graph.
[in]configurationThe input object of a single params structure of type tivx_vpac_nf_common_params_t.
[in]inputThe input image in VX_DF_IMAGE_U8, VX_DF_IMAGE_U16, or TIVX_DF_IMAGE_P12 format.
[in]convThe input convolution matrix. Max columns or rows supported is 5. Scale value is ignored. Coefficients are 9-bit signed.
[out]outputThe output image in VX_DF_IMAGE_U8, VX_DF_IMAGE_U16, or TIVX_DF_IMAGE_P12 format.
See also
TIVX_KERNEL_VPAC_NF_GENERIC_NAME
Returns
vx_node.
Return values
vx_nodeA node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus

◆ tivxVpacNfBilateralNode()

VX_API_ENTRY vx_node VX_API_CALL tivxVpacNfBilateralNode ( vx_graph  graph,
vx_user_data_object  configuration,
vx_image  input,
vx_user_data_object  sigmas,
vx_image  output 
)

[Graph] Creates a VPAC_NF_BILATERAL Node.

Parameters
[in]graphThe reference to the graph.
[in]configurationThe input object of a single params structure of type tivx_vpac_nf_bilateral_params_t.
[in]inputThe input image in VX_DF_IMAGE_U8, VX_DF_IMAGE_U16, or TIVX_DF_IMAGE_P12 format.
[in]sigmasThe input object of a single params structure of type tivx_vpac_nf_bilateral_sigmas_t.
[out]outputThe output image in VX_DF_IMAGE_U8, VX_DF_IMAGE_U16, or TIVX_DF_IMAGE_P12 format.
See also
TIVX_KERNEL_VPAC_NF_BILATERAL_NAME
Returns
vx_node.
Return values
vx_nodeA node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus

◆ tivx_vpac_nf_common_params_init()

void tivx_vpac_nf_common_params_init ( tivx_vpac_nf_common_params_t prms)

Function to initialize NF common Parameters.

Parameters
prms[IN] Pointer to NF common parameters

◆ tivx_vpac_nf_hts_bw_limit_params_init()

void tivx_vpac_nf_hts_bw_limit_params_init ( tivx_vpac_nf_hts_bw_limit_params_t prms)

Function to initialize NF HTS bandwidth limit Parameters.

Parameters
prms[IN] Pointer to NF HTS bandwidth limit parameters

◆ tivx_vpac_nf_bilateral_params_init()

void tivx_vpac_nf_bilateral_params_init ( tivx_vpac_nf_bilateral_params_t prms)

Function to initialize NF bilateral Parameters.

Parameters
prms[IN] Pointer to NF bilateral parameters

◆ tivx_vpac_nf_bilateral_sigmas_init()

void tivx_vpac_nf_bilateral_sigmas_init ( tivx_vpac_nf_bilateral_sigmas_t sigmas)

Function to initialize NF bilateral Sigmas.

Parameters
sigmas[IN] Pointer to NF bilateral sigmas