![]() |
TI Deep Learning Product User Guide
|
This structure contains all the parameters which controls the applet at create time.
Data Fields | |
| IVISION_InArgs | iVisionInArgs |
| int32_t | numInBufs |
| float32_tidl | scale [TIDL_NUM_IN_BUFS] |
| int32_t | enableLayerPerfTraces |
| IVISION_InArgs TIDL_InArgs::iVisionInArgs |
Common inArgs for all ivision based modules
| int32_t TIDL_InArgs::numInBufs |
Number of input buffers
| float32_tidl TIDL_InArgs::scale[TIDL_NUM_IN_BUFS] |
Scale factor for each input tensor
| int32_t TIDL_InArgs::enableLayerPerfTraces |
if enable layer level traces are generated in that particular process call