SDL API Guide for J721E
SDL_ROM_Checksum_obj Struct Reference

Detailed Description

This structure is used to store the resultant value of ROM Checksum.



Data Fields

uint64_t length
 
uint64_t state [8]
 
uint32_t curlen
 
uint8_t buf [128]
 

Field Documentation

◆ length

uint64_t SDL_ROM_Checksum_obj::length

Actual data length

◆ state

uint64_t SDL_ROM_Checksum_obj::state[8]

Random seek value

◆ curlen

uint32_t SDL_ROM_Checksum_obj::curlen

Used to keep track of data length in incomplete block

◆ buf

uint8_t SDL_ROM_Checksum_obj::buf[128]

Memory storage use in padding