![]() |
SDL API Guide for J721E
|
Provides the APIs for POK.
Sub Modules | |
POK Data Structures | |
POK Enum Data defines | |
POK Functions | |
Files | |
file | sdl_pok_def.h |
Header file containing various enumerations, structure definitions and function declarations for the Power System modules such as POK/POR IP. | |
Functions | |
void | sdlGetErrSig (uint32_t id, SDL_POK_Inst *instance, uint32_t *esm_err_sig, bool *usePorCfgFlag) |
void sdlGetErrSig | ( | uint32_t | id, |
SDL_POK_Inst * | instance, | ||
uint32_t * | esm_err_sig, | ||
bool * | usePorCfgFlag | ||
) |