![]() |
SDL API Guide for J721E
|
Typedefs | |
typedef uint32_t | SDL_ECC_MemType |
This enumerator indicate ECC memory type. More... | |
typedef uint32_t | SDL_ECC_MemSubType |
This enumerator indicate ECC memory Sub Type. More... | |
typedef void(* | SDL_ECC_ErrorCallback_t) (uint32_t errorSrc, uint32_t address) |
typedef void(* | SDL_ECC_VIMDEDVector_t) (void) |
typedef uint32_t SDL_ECC_MemType |
This enumerator indicate ECC memory type.
typedef uint32_t SDL_ECC_MemSubType |
This enumerator indicate ECC memory Sub Type.
typedef void(* SDL_ECC_ErrorCallback_t) (uint32_t errorSrc, uint32_t address) |
/brief Format of ECC error Call back function
typedef void(* SDL_ECC_VIMDEDVector_t) (void) |
/brief Format of VIM DED vector function