OTP programming is done using the DMSC. This is needed to convert a field securable device into a HS device.
|
file | sciclient_keywriter.h |
| This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for OTP Key programming.
|
|
|
int32_t | Sciclient_otpProcessKeyCfg (uint32_t *otpKeyCfgAddr, uint32_t timeout, uint32_t *debug_response) |
| Message to request a processor Provides a means for either the “recovery master” host or another host in the permitted access list to request for a physical processor control. More...
|
|
◆ Sciclient_otpProcessKeyCfg()
int32_t Sciclient_otpProcessKeyCfg |
( |
uint32_t * |
otpKeyCfgAddr, |
|
|
uint32_t |
timeout, |
|
|
uint32_t * |
debug_response |
|
) |
| |