![]() |
MMALIB User Guide
|
File to hold common structure, enums, macros and functions for MMALIB.
Definition in file MMALIB_types.h.
Go to the source code of this file.
Macros | |
| #define | MMALIB_DEBUGPRINT 0 |
| Enable debug printf statements. More... | |
| #define | MMALIB_const const |
| #define | __PRAGMA(x) _Pragma(#x) |
| #define | __INLINE_FUNC(x) __PRAGMA(FUNC_ALWAYS_INLINE(x)) |
| #define | MMALIB_PRINTF(fmt, ...) |
| #define | MMALIB_DEBUGPRINTFN(N, fmt, ...) |
| #define | MMALIB_MESG(fmt, ...) |
| #define | MMALIB_SOFT_MMA_RESET 0 |
| #define | MMALIB_STATIC_INLINE static inline |
| #define | MMALIB_PARAM_SIZE 128 |
| Parameter structure size in bytes. More... | |
| #define | MMALIB_BYTE_WIDTH __MMA_A_COLS(sizeof(int8_t)) |
| MMA width in bytes. More... | |
| #define | MMALIB_MMA_ACCUMULATOR_BYTE_WIDTH_8_BIT 4 |
| MMA accumulator width in bytes for 8 bit output data width. More... | |
| #define | MMALIB_MMA_ACCUMULATOR_BYTE_WIDTH_16_BIT 8 |
| MMA accumulator width in bytes for 16 bit output data width. More... | |
| #define | MMALIB_MMA_ACCUMULATOR_BYTE_WIDTH_32_BIT 16 |
| MMA accumulator width in bytes for 32 bit output data width. More... | |
| #define | MMALIB_ALIGN_SHIFT_64BYTES 6 |
| Number of bits to shift for 64-byte memory alignment. More... | |
| #define | MMALIB_ALIGN_SHIFT_128BYTES 7 |
| Number of bits to shift for 128-byte memory alignment. More... | |
| #define | MMALIB_ALIGN_SHIFT_256BYTES 8 |
| Number of bits to shift for 256-byte memory alignment. More... | |
| #define | MMALIB_ALIGN_64BYTES (1 << MMALIB_ALIGN_SHIFT_64BYTES) |
| Align by 64-byte memory alignment. More... | |
| #define | MMALIB_ALIGN_128BYTES (1 << MMALIB_ALIGN_SHIFT_128BYTES) |
| Align by 128-byte memory alignment. More... | |
| #define | MMALIB_ALIGN_256BYTES (1 << MMALIB_ALIGN_SHIFT_256BYTES) |
| Align by 256-byte memory alignment. More... | |
| #define | MMALIB_L2DATA_ALIGN_SHIFT MMALIB_ALIGN_SHIFT_64BYTES |
| Set the default L2 data alignment. More... | |
| #define | MMALIB_L2DATA_ALIGNMENT (((uint32_t)1) << ((uint32_t)MMALIB_L2DATA_ALIGN_SHIFT)) |
| Macro that specifies the alignment of data buffers in L2 memory for optimal performance. More... | |
| #define | MMALIB_MMA_SIZE_8_BIT __MMA_A_COLS(sizeof(int8_t)) |
| MMA size as a function of precision. More... | |
| #define | MMALIB_MMA_SIZE_16_BIT __MMA_A_COLS(sizeof(int16_t)) |
| #define | MMALIB_MMA_SIZE_32_BIT __MMA_A_COLS(sizeof(int32_t)) |
| #define | MMALIB_MMA_BIAS_SIZE_32_BIT __MMA_A_COLS(sizeof(int32_t)) |
| #define | MMALIB_MMA_BIAS_SIZE_64_BIT ((MMALIB_MMA_BIAS_SIZE_32_BIT) >> 1) |
Typedefs | |
| typedef double | MMALIB_D64 |
| Double precision floating point. More... | |
| typedef float | MMALIB_F32 |
| Single precision floating point. More... | |
| typedef MMALIB_STATUS_NAME | MMALIB_STATUS |
| Return value for MMALIB functions. More... | |
| typedef void * | MMALIB_kernelHandle |
| Handle type for MMALIB operations. More... | |
| typedef MMALIB_tensor_format_e | MMALIB_tensor_format |
| #define MMALIB_DEBUGPRINT 0 |
Enable debug printf statements.
Definition at line 74 of file MMALIB_types.h.
| #define MMALIB_const const |
Definition at line 80 of file MMALIB_types.h.
| #define __PRAGMA | ( | x | ) | _Pragma(#x) |
Definition at line 83 of file MMALIB_types.h.
| #define __INLINE_FUNC | ( | x | ) | __PRAGMA(FUNC_ALWAYS_INLINE(x)) |
Definition at line 87 of file MMALIB_types.h.
| #define MMALIB_PRINTF | ( | fmt, | |
| ... | |||
| ) |
Definition at line 95 of file MMALIB_types.h.
| #define MMALIB_DEBUGPRINTFN | ( | N, | |
| fmt, | |||
| ... | |||
| ) |
Definition at line 111 of file MMALIB_types.h.
| #define MMALIB_MESG | ( | fmt, | |
| ... | |||
| ) |
Definition at line 120 of file MMALIB_types.h.
| #define MMALIB_SOFT_MMA_RESET 0 |
Definition at line 141 of file MMALIB_types.h.
| #define MMALIB_STATIC_INLINE static inline |
Definition at line 144 of file MMALIB_types.h.
| #define MMALIB_PARAM_SIZE 128 |
Parameter structure size in bytes.
Definition at line 312 of file MMALIB_types.h.
| #define MMALIB_BYTE_WIDTH __MMA_A_COLS(sizeof(int8_t)) |
MMA width in bytes.
Definition at line 313 of file MMALIB_types.h.
| #define MMALIB_MMA_ACCUMULATOR_BYTE_WIDTH_8_BIT 4 |
MMA accumulator width in bytes for 8 bit output data width.
Definition at line 314 of file MMALIB_types.h.
| #define MMALIB_MMA_ACCUMULATOR_BYTE_WIDTH_16_BIT 8 |
MMA accumulator width in bytes for 16 bit output data width.
Definition at line 315 of file MMALIB_types.h.
| #define MMALIB_MMA_ACCUMULATOR_BYTE_WIDTH_32_BIT 16 |
MMA accumulator width in bytes for 32 bit output data width.
Definition at line 316 of file MMALIB_types.h.
| #define MMALIB_ALIGN_SHIFT_64BYTES 6 |
Number of bits to shift for 64-byte memory alignment.
Definition at line 326 of file MMALIB_types.h.
| #define MMALIB_ALIGN_SHIFT_128BYTES 7 |
Number of bits to shift for 128-byte memory alignment.
Definition at line 328 of file MMALIB_types.h.
| #define MMALIB_ALIGN_SHIFT_256BYTES 8 |
Number of bits to shift for 256-byte memory alignment.
Definition at line 330 of file MMALIB_types.h.
| #define MMALIB_ALIGN_64BYTES (1 << MMALIB_ALIGN_SHIFT_64BYTES) |
Align by 64-byte memory alignment.
Definition at line 333 of file MMALIB_types.h.
| #define MMALIB_ALIGN_128BYTES (1 << MMALIB_ALIGN_SHIFT_128BYTES) |
Align by 128-byte memory alignment.
Definition at line 335 of file MMALIB_types.h.
| #define MMALIB_ALIGN_256BYTES (1 << MMALIB_ALIGN_SHIFT_256BYTES) |
Align by 256-byte memory alignment.
Definition at line 337 of file MMALIB_types.h.
| #define MMALIB_L2DATA_ALIGN_SHIFT MMALIB_ALIGN_SHIFT_64BYTES |
Set the default L2 data alignment.
Definition at line 340 of file MMALIB_types.h.
| #define MMALIB_L2DATA_ALIGNMENT (((uint32_t)1) << ((uint32_t)MMALIB_L2DATA_ALIGN_SHIFT)) |
Macro that specifies the alignment of data buffers in L2 memory for optimal performance.
Definition at line 344 of file MMALIB_types.h.
| #define MMALIB_MMA_SIZE_8_BIT __MMA_A_COLS(sizeof(int8_t)) |
MMA size as a function of precision.
Definition at line 353 of file MMALIB_types.h.
| #define MMALIB_MMA_SIZE_16_BIT __MMA_A_COLS(sizeof(int16_t)) |
Definition at line 354 of file MMALIB_types.h.
| #define MMALIB_MMA_SIZE_32_BIT __MMA_A_COLS(sizeof(int32_t)) |
Definition at line 355 of file MMALIB_types.h.
| #define MMALIB_MMA_BIAS_SIZE_32_BIT __MMA_A_COLS(sizeof(int32_t)) |
Definition at line 358 of file MMALIB_types.h.
| #define MMALIB_MMA_BIAS_SIZE_64_BIT ((MMALIB_MMA_BIAS_SIZE_32_BIT) >> 1) |
Definition at line 359 of file MMALIB_types.h.
| typedef double MMALIB_D64 |
Double precision floating point.
Definition at line 172 of file MMALIB_types.h.
| typedef float MMALIB_F32 |
Single precision floating point.
Definition at line 173 of file MMALIB_types.h.
| typedef MMALIB_STATUS_NAME MMALIB_STATUS |
Return value for MMALIB functions.
Definition at line 277 of file MMALIB_types.h.
| typedef void* MMALIB_kernelHandle |
Handle type for MMALIB operations.
Definition at line 279 of file MMALIB_types.h.
Definition at line 304 of file MMALIB_types.h.
| enum MMALIB_STATUS_NAME |
The enumeration of all status codes.
Definition at line 176 of file MMALIB_types.h.
Enumeration for the style of function implementation.
| Enumerator | |
|---|---|
| MMALIB_FUNCTION_NATC | Natural C implementation of the function |
| MMALIB_FUNCTION_OPTIMIZED | Optimized C implementation of the function for the MMA + C7x architecture |
| MMALIB_FUNCTION_MAX | |
Definition at line 282 of file MMALIB_types.h.
| enum MMALIB_buffer_mode_e |
Buffer structure for input feature maps and coefficients of MMALIB_CNN_convolve_row_ixX_ixX_oxX.
| Enumerator | |
|---|---|
| MMALIB_LINEAR | Linear buffer. |
| MMALIB_SE_CIRCULAR | Circular buffer for input feature map managed by streaming engine |
| MMALIB_BUF_CIRCULAR | Circular buffer for coefficients. |
Definition at line 291 of file MMALIB_types.h.
Tensor format.
| Enumerator | |
|---|---|
| MMALIB_CHW | Used when tensor is in NCHW format. |
| MMALIB_HWC | Used when tensor is in NHWC format. |
Definition at line 299 of file MMALIB_types.h.