![]() |
PDK API Guide for J721E
|
This Module explains about PMIC GPIO driver parameters and APIs usage. PMIC GPIO Driver module covers all GPIO features APIs. Like, set/get gpio pin functions, pull up/down, drive strength, output drain, pin value, enable/disable gpio interrupt and configure nPWRON or ENABLE pin features.
Supported PMIC devices for GPIO Module:
Files | |
| file | pmic_gpio.h |
| PMIC Low Level Driver API/interface file for GPIO API. | |
| file | pmic_gpio_tps6594x.h |
| PMIC TPS6594x Leo PMIC GPIO API/interface file. | |
| file | pmic_gpio_lp8764x.h |
| PMIC LP8764x Hera PMIC GPIO API/interface file. | |
Data Structures | |
| struct | Pmic_GpioCfg_t |
| PMIC GPIO/NPWRON/ENABLE pin configuration structure. Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
Functions | |
| int32_t | Pmic_gpioSetConfiguration (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pin, const Pmic_GpioCfg_t gpioCfg) |
| API to set PMIC GPIO configuration. More... | |
| int32_t | Pmic_gpioGetConfiguration (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pin, Pmic_GpioCfg_t *pGpioCfg) |
| API to get PMIC GPIO configuration. More... | |
| int32_t | Pmic_gpioSetValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pin, const uint8_t pinValue) |
| API to set PMIC GPIO value. More... | |
| int32_t | Pmic_gpioSetDir (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pin, const uint8_t pinDir) |
| int32_t | Pmic_gpioGetValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pin, uint8_t *pPinValue) |
| API to get PMIC GPIO value. More... | |
| int32_t | Pmic_gpioSetIntr (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pin, const uint8_t intrType, const uint8_t maskPol) |
| API to enable/disable GPIO interrupt. More... | |
| int32_t | Pmic_gpioSetNPwronEnablePinConfiguration (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_GpioCfg_t gpioCfg) |
| API to set configuration for NPWRON/Enable pin. More... | |
| int32_t | Pmic_gpioGetNPwronEnablePinConfiguration (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_GpioCfg_t *pGpioCfg) |
| API to get configuration for NPWRON/Enable pin. More... | |
| int32_t | Pmic_gpioTps6594xNPwronPinGetValue (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pPinValue) |
| API to get PMIC GPIO NPWRON/Enable pin value. More... | |
PMIC GPIO Deglitch Time Enable or Disable Configuration | |
| #define | PMIC_GPIO_DEGLITCH_DISABLE (0U) |
| #define | PMIC_GPIO_DEGLITCH_ENABLE (1U) |
PMIC GPIO signal direction | |
| #define | PMIC_GPIO_INPUT (0U) |
| #define | PMIC_GPIO_OUTPUT (1U) |
PMIC GPIO signal type when configured as output | |
| #define | PMIC_GPIO_PUSH_PULL_OUTPUT (0U) |
| #define | PMIC_GPIO_OPEN_DRAIN_OUTPUT (1U) |
PMIC GPIO/NPWRON/ENABLE signal level | |
| #define | PMIC_GPIO_LOW (0U) |
| #define | PMIC_GPIO_HIGH (1U) |
PMIC GPIO Pull-up/pull-down select | |
| #define | PMIC_GPIO_PD_SELECT (0U) |
| #define | PMIC_GPIO_PU_SELECT (1U) |
PMIC GPIO Pull-up/pull-down enable/disable | |
| #define | PMIC_GPIO_PU_PD_DISABLE (0U) |
| #define | PMIC_GPIO_PU_PD_ENABLE (1U) |
PMIC Pmic_GpioCfg_s member configuration type | |
| #define | PMIC_GPIO_CFG_DIR_VALID (0x00U) |
| validParams value used to set/get gpio pin Direction Valid only for GPIO pins only. Invalid for NPWRON/Enable More... | |
| #define | PMIC_GPIO_CFG_OD_VALID (0x01U) |
| validParams value used to set/get output signal type Valid only for GPIO pins only. Invalid for NPWRON/Enable More... | |
| #define | PMIC_GPIO_CFG_PULL_VALID (0x02U) |
| validParams value used to set/get pullup/pull down control More... | |
| #define | PMIC_GPIO_CFG_DEGLITCH_VALID (0x03U) |
| validParams value used to set/get signal deglitch time enable/disable More... | |
| #define | PMIC_GPIO_CFG_PINFUNC_VALID (0x04U) |
| validParams value used to set/get pin mux function More... | |
| #define | PMIC_ENABLE_CFG_POLARITY_VALID (0x05U) |
| validParams value used to set/get pin polarity Valid only for Enable pin for TPS6594x Leo and LP8764x Hera device Invalid for NPWRON pin for TPS6594x Leo device More... | |
PMIC GPIO Pin Configuration Structure Param Bit shift values | |
|
Application can use below shifted values to set the validParams struct member defined in Pmic_GpioCfg_t structure | |
| #define | PMIC_GPIO_CFG_DIR_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_DIR_VALID) |
| #define | PMIC_GPIO_CFG_OD_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_OD_VALID) |
| #define | PMIC_GPIO_CFG_PULL_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_PULL_VALID) |
| #define | PMIC_GPIO_CFG_DEGLITCH_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_DEGLITCH_VALID) |
| #define | PMIC_GPIO_CFG_PINFUNC_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_PINFUNC_VALID) |
| #define | PMIC_ENABLE_CFG_POLARITY_VALID_SHIFT (0x01U << PMIC_ENABLE_CFG_POLARITY_VALID) |
PMIC GPIO pull up/pull down selectionn | |
| #define | PMIC_GPIO_PULL_DISABLED (0x0U) |
| #define | PMIC_GPIO_PULL_DOWN (0x1U) |
| #define | PMIC_GPIO_PULL_UP (0x2U) |
PMIC GPIO Interrupt selection | |
| #define | PMIC_GPIO_FALL_INTERRUPT (0U) |
| #define | PMIC_GPIO_RISE_INTERRUPT (1U) |
| #define | PMIC_GPIO_FALL_RISE_INTERRUPT (2U) |
| #define | PMIC_GPIO_DISABLE_INTERRUPT (3U) |
PMIC GPIO Interrupt Polarity selection | |
| #define | PMIC_GPIO_POL_LOW (0U) |
| #define | PMIC_GPIO_POL_HIGH (1U) |
PMIC GPIO supported pins for TPS6594x Leo Device | |
| #define | PMIC_TPS6594X_GPIO1_PIN (1U) |
| #define | PMIC_TPS6594X_GPIO2_PIN (2U) |
| #define | PMIC_TPS6594X_GPIO3_PIN (3U) |
| #define | PMIC_TPS6594X_GPIO4_PIN (4U) |
| #define | PMIC_TPS6594X_GPIO5_PIN (5U) |
| #define | PMIC_TPS6594X_GPIO6_PIN (6U) |
| #define | PMIC_TPS6594X_GPIO7_PIN (7U) |
| #define | PMIC_TPS6594X_GPIO8_PIN (8U) |
| #define | PMIC_TPS6594X_GPIO9_PIN (9U) |
| #define | PMIC_TPS6594X_GPIO10_PIN (10U) |
| #define | PMIC_TPS6594X_GPIO11_PIN (11U) |
PMIC GPIO pin functions supported for TPS6594x Leo Device | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO (0U) |
| Used to configure GPIO Pin Function. Valid for all GPIO Pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_SCL_I2C2_CS_SPI (1U) |
| Used to configure SCL_I2C2/CS_SPI Pin Function. Valid only for GPIO1 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_GPIO11_TRIG_WDOG (1U) |
| Used to configure TRIG_WDOG Pin Function. Valid only for GPIO2 and GPIO11 pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_GPIO8_CLK32KOUT (1U) |
| Used to configure CLK32KOUT Pin Function. Valid only for GPIO3, GPIO4 and GPIO8 pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO5_SCLK_SPMI (1U) |
| Used to configure SCLK_SPMI Pin Function. Valid only for GPIO5 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO6_SDATA_SPMI (1U) |
| Used to configure SDATA_SPMI Pin Function. Valid only for GPIO6 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO7_NERR_MCU (1U) |
| Used to configure NERR_MCU Pin Function. Valid only for GPIO7 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_PGOOD (1U) |
| Used to configure PGOOD Pin Function. Valid only for GPIO9 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_SYNCCLKIN (1U) |
| Used to configure SYNCCLKIN Pin Function. Valid only for GPIO10 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_GPIO11_NRSTOUT_SOC (2U) |
| Used to configure NRSTOUT_SOC Pin Function. Valid only for GPIO1 and GPIO11 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_SDA_I2C2_SDO_SPI (2U) |
| Used to configure SDA_I2C2/SDO_SPI Pin Function. Valid only for GPIO2 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_NERR_SOC (2U) |
| Used to configure NERR_SOC Pin Function. Valid only for GPIO3 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_GPIO10_SYNCCLKOUT (2U) |
| Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO8 and GPIO10 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_DISABLE_WDOG (2U) |
| Used to configure DISABLE_WDOG Pin Function. Valid only for GPIO9 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_DISABLE_WDOG (3U) |
| Used to configure DISABLE_WDOG Pin Function. Valid only for GPIO8 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_SYNCCLKOUT (3U) |
| Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO9 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_CLK32KOUT (3U) |
| Used to configure CLK32KOUT Pin Function. Valid only for GPIO10 pin. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP1 (4U) |
| Used to configure NSLEEP1 Pin Function. Valid for all GPIO Pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP2 (5U) |
| Used to configure NSLEEP2 Pin Function. Valid for all GPIO Pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_WKUP1 (6U) |
| Used to configure WKUP1 Pin Function. Valid for all GPIO Pins except GPIO3 and GPIO4 pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP1 (6U) |
| Used to configure LP_WKUP1 Pin Function. Valid only for GPIO3 and GPIO4 pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_WKUP2 (7U) |
| Used to configure WKUP2 Pin Function. Valid for all GPIO Pins except GPIO3 and GPIO4 pins. More... | |
| #define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP2 (7U) |
| Used to configure LP_WKUP2 Pin Function. Valid only for GPIO3 and GPIO4 pins. More... | |
PMIC GPIO NPWRON pin functions supported for TPS6594x Leo Device | |
| #define | PMIC_TPS6594X_NPWRON_PINFUNC_ENABLE (0U) |
| Enable Signal Function for NPWRON/ENABLE pin. More... | |
| #define | PMIC_TPS6594X_NPWRON_PINFUNC_NPWRON (1U) |
| NPWRON Signal Function for NPWRON/ENABLE pin. More... | |
| #define | PMIC_TPS6594X_NPWRON_PINFUNC_NONE (2U) |
| None Function for NPWRON/ENABLE pin. More... | |
PMIC GPIO supported pins for LP8764x HERA Device | |
| #define | PMIC_LP8764X_GPIO1_PIN (1U) |
| #define | PMIC_LP8764X_GPIO2_PIN (2U) |
| #define | PMIC_LP8764X_GPIO3_PIN (3U) |
| #define | PMIC_LP8764X_GPIO4_PIN (4U) |
| #define | PMIC_LP8764X_GPIO5_PIN (5U) |
| #define | PMIC_LP8764X_GPIO6_PIN (6U) |
| #define | PMIC_LP8764X_GPIO7_PIN (7U) |
| #define | PMIC_LP8764X_GPIO8_PIN (8U) |
| #define | PMIC_LP8764X_GPIO9_PIN (9U) |
| #define | PMIC_LP8764X_GPIO10_PIN (10U) |
PMIC GPIO pin functions supported by LP8764x HERA PMIC | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO (0U) |
| Used to configure GPIO Pin Function. Valid for all GPIO Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO1_EN_DRV (1U) |
| Used to configure EN_DRV Pin Function. Valid only for GPIO1 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO2_SCL_I2C2 (1U) |
| Used to configure SCL_I2C2 Pin Function. Valid only for GPIO2 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO3_SDA_I2C2 (1U) |
| Used to configure SDA_I2C2 Pin Function. Valid only for GPIO3 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO4_ENABLE (1U) |
| Used to configure ENABLE Pin Function. Valid only for GPIO4 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO5_SYNCCLKIN (1U) |
| Used to configure SYNCCLKIN Pin Function. Valid only for GPIO5 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO6_GPIO7_NERR_MCU (1U) |
| Used to configure nERR_MCU Pin Function. Valid only for GPIO7 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO8_SCLK_SPMI (1U) |
| Used to configure SCLK_SPMI Pin Function. Valid only for GPIO8 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO9_SDATA_SPMI (1U) |
| Used to configure SDATA_SPMI Pin Function. Valid only for GPIO9 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO10_NRSTOUT (1U) |
| Used to configure nRSTOUT Pin Function. Valid only for GPIO10 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO1_GPIO10_NRSTOUT_SOC (2U) |
| Used to configure nRSTOUT_SOC Pin Function. Valid only for GPIO1 and GPIO10 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO2_CS_SPI (2U) |
| Used to configure CS_SPI Pin Function. Valid only for GPIO2 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO3_SDO_SPI (2U) |
| Used to configure SDO_SPI Pin Function. Valid only for GPIO3 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO4_TRIG_WDOG (2U) |
| Used to configure TRIG_WDOG Pin Function. Valid only for GPIO4 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO5_GPIO6_SYNCCLKOUT (2U) |
| Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO5 and GPIO6 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO7_REFOUT (2U) |
| Used to configure REFOUT Pin Function. Valid only for GPIO7 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO8_VMON2 (2U) |
| Used to configure VMON2 Pin Function. Valid only for GPIO8 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO9_PGOOD (2U) |
| Used to configure PGOOD Pin Function. Valid only for GPIO9 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO1_GPIO6_PGOOD (3U) |
| Used to configure PGOOD Pin Function. Valid only for GPIO1 and GPIO6 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO2_TRIG_WDOG (3U) |
| Used to configure TRIG_WDOG Pin Function. Valid only for GPIO2 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO4_BUCK1_VMON (3U) |
| Used to configure BUCK1_VMON Pin Function. Valid only for GPIO4 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO5_NRSTOUT_SOC (3U) |
| Used to configure nRSTOUT_SOC Pin Function. Valid only for GPIO5 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO7_VMON1 (3U) |
| Used to configure VMON1 Pin Function. Valid only for GPIO7 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_GPIO9_SYNCCLKIN (3U) |
| Used to configure SYNCCLKIN Pin Function. Valid only for GPIO9 Pin. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_NSLEEP1 (4U) |
| Used to configure NSLEEP1 Pin Function. Valid only for GPIO1 to GPIO10 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_NSLEEP2 (5U) |
| Used to configure NSLEEP2 Pin Function. Valid only for GPIO1 to GPIO10 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_WKUP1 (6U) |
| Used to configure WKUP1 Pin Function. Valid only for GPIO1 to GPIO10 Pins. More... | |
| #define | PMIC_LP8764X_GPIO_PINFUNC_WKUP2 (7U) |
| Used to configure WKUP2 Pin Function. Valid only for GPIO1 to GPIO10 Pins. More... | |
| #define PMIC_GPIO_DEGLITCH_DISABLE (0U) |
| #define PMIC_GPIO_DEGLITCH_ENABLE (1U) |
| #define PMIC_GPIO_INPUT (0U) |
| #define PMIC_GPIO_OUTPUT (1U) |
| #define PMIC_GPIO_PUSH_PULL_OUTPUT (0U) |
| #define PMIC_GPIO_OPEN_DRAIN_OUTPUT (1U) |
| #define PMIC_GPIO_LOW (0U) |
| #define PMIC_GPIO_HIGH (1U) |
| #define PMIC_GPIO_PD_SELECT (0U) |
| #define PMIC_GPIO_PU_SELECT (1U) |
| #define PMIC_GPIO_PU_PD_DISABLE (0U) |
| #define PMIC_GPIO_PU_PD_ENABLE (1U) |
| #define PMIC_GPIO_CFG_DIR_VALID (0x00U) |
validParams value used to set/get gpio pin Direction Valid only for GPIO pins only. Invalid for NPWRON/Enable
| #define PMIC_GPIO_CFG_OD_VALID (0x01U) |
validParams value used to set/get output signal type Valid only for GPIO pins only. Invalid for NPWRON/Enable
| #define PMIC_GPIO_CFG_PULL_VALID (0x02U) |
validParams value used to set/get pullup/pull down control
| #define PMIC_GPIO_CFG_DEGLITCH_VALID (0x03U) |
validParams value used to set/get signal deglitch time enable/disable
| #define PMIC_GPIO_CFG_PINFUNC_VALID (0x04U) |
validParams value used to set/get pin mux function
| #define PMIC_ENABLE_CFG_POLARITY_VALID (0x05U) |
validParams value used to set/get pin polarity Valid only for Enable pin for TPS6594x Leo and LP8764x Hera device Invalid for NPWRON pin for TPS6594x Leo device
| #define PMIC_GPIO_CFG_DIR_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_DIR_VALID) |
| #define PMIC_GPIO_CFG_OD_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_OD_VALID) |
| #define PMIC_GPIO_CFG_PULL_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_PULL_VALID) |
| #define PMIC_GPIO_CFG_DEGLITCH_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_DEGLITCH_VALID) |
| #define PMIC_GPIO_CFG_PINFUNC_VALID_SHIFT (0x01U << PMIC_GPIO_CFG_PINFUNC_VALID) |
| #define PMIC_ENABLE_CFG_POLARITY_VALID_SHIFT (0x01U << PMIC_ENABLE_CFG_POLARITY_VALID) |
| #define PMIC_GPIO_PULL_DISABLED (0x0U) |
| #define PMIC_GPIO_PULL_DOWN (0x1U) |
| #define PMIC_GPIO_PULL_UP (0x2U) |
| #define PMIC_GPIO_FALL_INTERRUPT (0U) |
| #define PMIC_GPIO_RISE_INTERRUPT (1U) |
| #define PMIC_GPIO_FALL_RISE_INTERRUPT (2U) |
| #define PMIC_GPIO_DISABLE_INTERRUPT (3U) |
| #define PMIC_GPIO_POL_LOW (0U) |
| #define PMIC_GPIO_POL_HIGH (1U) |
| #define PMIC_TPS6594X_GPIO1_PIN (1U) |
| #define PMIC_TPS6594X_GPIO2_PIN (2U) |
| #define PMIC_TPS6594X_GPIO3_PIN (3U) |
| #define PMIC_TPS6594X_GPIO4_PIN (4U) |
| #define PMIC_TPS6594X_GPIO5_PIN (5U) |
| #define PMIC_TPS6594X_GPIO6_PIN (6U) |
| #define PMIC_TPS6594X_GPIO7_PIN (7U) |
| #define PMIC_TPS6594X_GPIO8_PIN (8U) |
| #define PMIC_TPS6594X_GPIO9_PIN (9U) |
| #define PMIC_TPS6594X_GPIO10_PIN (10U) |
| #define PMIC_TPS6594X_GPIO11_PIN (11U) |
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO (0U) |
Used to configure GPIO Pin Function. Valid for all GPIO Pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_SCL_I2C2_CS_SPI (1U) |
Used to configure SCL_I2C2/CS_SPI Pin Function. Valid only for GPIO1 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_GPIO11_TRIG_WDOG (1U) |
Used to configure TRIG_WDOG Pin Function. Valid only for GPIO2 and GPIO11 pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_GPIO8_CLK32KOUT (1U) |
Used to configure CLK32KOUT Pin Function. Valid only for GPIO3, GPIO4 and GPIO8 pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO5_SCLK_SPMI (1U) |
Used to configure SCLK_SPMI Pin Function. Valid only for GPIO5 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO6_SDATA_SPMI (1U) |
Used to configure SDATA_SPMI Pin Function. Valid only for GPIO6 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO7_NERR_MCU (1U) |
Used to configure NERR_MCU Pin Function. Valid only for GPIO7 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_PGOOD (1U) |
Used to configure PGOOD Pin Function. Valid only for GPIO9 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_SYNCCLKIN (1U) |
Used to configure SYNCCLKIN Pin Function. Valid only for GPIO10 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_GPIO11_NRSTOUT_SOC (2U) |
Used to configure NRSTOUT_SOC Pin Function. Valid only for GPIO1 and GPIO11 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_SDA_I2C2_SDO_SPI (2U) |
Used to configure SDA_I2C2/SDO_SPI Pin Function. Valid only for GPIO2 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_NERR_SOC (2U) |
Used to configure NERR_SOC Pin Function. Valid only for GPIO3 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_GPIO10_SYNCCLKOUT (2U) |
Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO8 and GPIO10 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_DISABLE_WDOG (2U) |
Used to configure DISABLE_WDOG Pin Function. Valid only for GPIO9 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_DISABLE_WDOG (3U) |
Used to configure DISABLE_WDOG Pin Function. Valid only for GPIO8 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_SYNCCLKOUT (3U) |
Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO9 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_CLK32KOUT (3U) |
Used to configure CLK32KOUT Pin Function. Valid only for GPIO10 pin.
| #define PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP1 (4U) |
Used to configure NSLEEP1 Pin Function. Valid for all GPIO Pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP2 (5U) |
Used to configure NSLEEP2 Pin Function. Valid for all GPIO Pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_WKUP1 (6U) |
Used to configure WKUP1 Pin Function. Valid for all GPIO Pins except GPIO3 and GPIO4 pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP1 (6U) |
Used to configure LP_WKUP1 Pin Function. Valid only for GPIO3 and GPIO4 pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_WKUP2 (7U) |
Used to configure WKUP2 Pin Function. Valid for all GPIO Pins except GPIO3 and GPIO4 pins.
| #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP2 (7U) |
Used to configure LP_WKUP2 Pin Function. Valid only for GPIO3 and GPIO4 pins.
| #define PMIC_TPS6594X_NPWRON_PINFUNC_ENABLE (0U) |
Enable Signal Function for NPWRON/ENABLE pin.
| #define PMIC_TPS6594X_NPWRON_PINFUNC_NPWRON (1U) |
NPWRON Signal Function for NPWRON/ENABLE pin.
| #define PMIC_TPS6594X_NPWRON_PINFUNC_NONE (2U) |
None Function for NPWRON/ENABLE pin.
| #define PMIC_LP8764X_GPIO1_PIN (1U) |
| #define PMIC_LP8764X_GPIO2_PIN (2U) |
| #define PMIC_LP8764X_GPIO3_PIN (3U) |
| #define PMIC_LP8764X_GPIO4_PIN (4U) |
| #define PMIC_LP8764X_GPIO5_PIN (5U) |
| #define PMIC_LP8764X_GPIO6_PIN (6U) |
| #define PMIC_LP8764X_GPIO7_PIN (7U) |
| #define PMIC_LP8764X_GPIO8_PIN (8U) |
| #define PMIC_LP8764X_GPIO9_PIN (9U) |
| #define PMIC_LP8764X_GPIO10_PIN (10U) |
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO (0U) |
Used to configure GPIO Pin Function. Valid for all GPIO Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO1_EN_DRV (1U) |
Used to configure EN_DRV Pin Function. Valid only for GPIO1 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO2_SCL_I2C2 (1U) |
Used to configure SCL_I2C2 Pin Function. Valid only for GPIO2 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO3_SDA_I2C2 (1U) |
Used to configure SDA_I2C2 Pin Function. Valid only for GPIO3 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO4_ENABLE (1U) |
Used to configure ENABLE Pin Function. Valid only for GPIO4 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO5_SYNCCLKIN (1U) |
Used to configure SYNCCLKIN Pin Function. Valid only for GPIO5 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO6_GPIO7_NERR_MCU (1U) |
Used to configure nERR_MCU Pin Function. Valid only for GPIO7 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO8_SCLK_SPMI (1U) |
Used to configure SCLK_SPMI Pin Function. Valid only for GPIO8 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO9_SDATA_SPMI (1U) |
Used to configure SDATA_SPMI Pin Function. Valid only for GPIO9 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO10_NRSTOUT (1U) |
Used to configure nRSTOUT Pin Function. Valid only for GPIO10 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO1_GPIO10_NRSTOUT_SOC (2U) |
Used to configure nRSTOUT_SOC Pin Function. Valid only for GPIO1 and GPIO10 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO2_CS_SPI (2U) |
Used to configure CS_SPI Pin Function. Valid only for GPIO2 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO3_SDO_SPI (2U) |
Used to configure SDO_SPI Pin Function. Valid only for GPIO3 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO4_TRIG_WDOG (2U) |
Used to configure TRIG_WDOG Pin Function. Valid only for GPIO4 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO5_GPIO6_SYNCCLKOUT (2U) |
Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO5 and GPIO6 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO7_REFOUT (2U) |
Used to configure REFOUT Pin Function. Valid only for GPIO7 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO8_VMON2 (2U) |
Used to configure VMON2 Pin Function. Valid only for GPIO8 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO9_PGOOD (2U) |
Used to configure PGOOD Pin Function. Valid only for GPIO9 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO1_GPIO6_PGOOD (3U) |
Used to configure PGOOD Pin Function. Valid only for GPIO1 and GPIO6 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO2_TRIG_WDOG (3U) |
Used to configure TRIG_WDOG Pin Function. Valid only for GPIO2 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO4_BUCK1_VMON (3U) |
Used to configure BUCK1_VMON Pin Function. Valid only for GPIO4 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO5_NRSTOUT_SOC (3U) |
Used to configure nRSTOUT_SOC Pin Function. Valid only for GPIO5 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO7_VMON1 (3U) |
Used to configure VMON1 Pin Function. Valid only for GPIO7 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_GPIO9_SYNCCLKIN (3U) |
Used to configure SYNCCLKIN Pin Function. Valid only for GPIO9 Pin.
| #define PMIC_LP8764X_GPIO_PINFUNC_NSLEEP1 (4U) |
Used to configure NSLEEP1 Pin Function. Valid only for GPIO1 to GPIO10 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_NSLEEP2 (5U) |
Used to configure NSLEEP2 Pin Function. Valid only for GPIO1 to GPIO10 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_WKUP1 (6U) |
Used to configure WKUP1 Pin Function. Valid only for GPIO1 to GPIO10 Pins.
| #define PMIC_LP8764X_GPIO_PINFUNC_WKUP2 (7U) |
Used to configure WKUP2 Pin Function. Valid only for GPIO1 to GPIO10 Pins.
| int32_t Pmic_gpioSetConfiguration | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| const uint8_t | pin, | ||
| const Pmic_GpioCfg_t | gpioCfg | ||
| ) |
API to set PMIC GPIO configuration.
Requirement: REQ_TAG(PDK-5808), REQ_TAG(PDK-5844), REQ_TAG(PDK-9111), REQ_TAG(PDK-9157) Design: did_pmic_gpio_cfg_readback, did_pmic_lpstandby_wkup_cfg Architecture: aid_pmic_gpio_cfg
This function is used to set the required configuration for the
specified GPIO pin when corresponding validParam bit field is set in
the Pmic_GpioCfg_t
For more information \ref Pmic_GpioCfg_t
Note: Application has to ensure to do proper configuration of GPIO
pin when connected to Enable pin of other peripherals on the
board. If not configured properly then it may down the
peripheral or system
| pPmicCoreHandle | [IN] PMIC Interface Handle. |
| pin | [IN] PMIC GPIO pin number. Valid values for TPS6594x Leo Device Pmic_Tps6594xLeo_GpioPin. Valid values for LP8764x HERA Device Pmic_Lp8764xHera_GpioPin. |
| gpioCfg | [IN] Set required configuration for the specified GPIO pin. |
| int32_t Pmic_gpioGetConfiguration | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| const uint8_t | pin, | ||
| Pmic_GpioCfg_t * | pGpioCfg | ||
| ) |
API to get PMIC GPIO configuration.
Requirement: REQ_TAG(PDK-5808) Design: did_pmic_gpio_cfg_readback Architecture: aid_pmic_gpio_cfg
This function is used to read the configuration for the specified
GPIO pin when corresponding validParam bit field is set in
the Pmic_GpioCfg_t
For more information \ref Pmic_GpioCfg_t
| pPmicCoreHandle | [IN] PMIC Interface Handle |
| pin | [IN] PMIC GPIO pin number. Valid values for TPS6594x Leo Device Pmic_Tps6594xLeo_GpioPin. Valid values for LP8764x HERA Device Pmic_Lp8764xHera_GpioPin. |
| pGpioCfg | [IN/OUT] Pointer to store specified GPIO pin configuration |
| int32_t Pmic_gpioSetValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| const uint8_t | pin, | ||
| const uint8_t | pinValue | ||
| ) |
API to set PMIC GPIO value.
Requirement: REQ_TAG(PDK-5808), REQ_TAG(PDK-9111) Design: did_pmic_gpio_cfg_readback Architecture: aid_pmic_gpio_cfg
This function is used to configure the signal level of the
specified GPIO pin.
| pPmicCoreHandle | [IN] PMIC Interface Handle. |
| pin | [IN] PMIC GPIO pin number. Valid values for TPS6594x Leo Device Pmic_Tps6594xLeo_GpioPin. Valid values for LP8764x HERA Device Pmic_Lp8764xHera_GpioPin. |
| pinValue | [IN] PMIC GPIO signal level High/Low to be configured. Valid values Pmic_Gpio_SignalLvl. |
| int32_t Pmic_gpioSetDir | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| const uint8_t | pin, | ||
| const uint8_t | pinDir | ||
| ) |
| int32_t Pmic_gpioGetValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| const uint8_t | pin, | ||
| uint8_t * | pPinValue | ||
| ) |
API to get PMIC GPIO value.
Requirement: REQ_TAG(PDK-5808) Design: did_pmic_gpio_cfg_readback Architecture: aid_pmic_gpio_cfg
This function is used to read the signal level of the gpio pin
| pPmicCoreHandle | [IN] PMIC Interface Handle |
| pin | [IN] PMIC GPIO pin number. Valid values for TPS6594x Leo Device Pmic_Tps6594xLeo_GpioPin. Valid values for LP8764x HERA Device Pmic_Lp8764xHera_GpioPin. |
| pPinValue | [OUT] To store PMIC GPIO signal level High/Low. Valid values Pmic_Gpio_SignalLvl |
| int32_t Pmic_gpioSetIntr | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| const uint8_t | pin, | ||
| const uint8_t | intrType, | ||
| const uint8_t | maskPol | ||
| ) |
API to enable/disable GPIO interrupt.
Requirement: REQ_TAG(PDK-5808), REQ_TAG(PDK-9159), REQ_TAG(PDK-9329) Design: did_pmic_gpio_cfg_readback Architecture: aid_pmic_gpio_cfg
This function is used to enable/disable GPIO pin Interrupts
| pPmicCoreHandle | [IN] PMIC Interface Handle. |
| pin | [IN] PMIC GPIO number. Valid values for TPS6594x Leo Device Pmic_Tps6594xLeo_GpioPin. Valid values for LP8764x HERA Device Pmic_Lp8764xHera_GpioPin. |
| intrType | [IN] Interrupt type Pmic_GpioInterruptCfg |
| maskPol | [IN] FSM trigger masking polarity select for GPIO Valid values refer Pmic_GpioInterruptPolCfg. |
| int32_t Pmic_gpioSetNPwronEnablePinConfiguration | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| const Pmic_GpioCfg_t | gpioCfg | ||
| ) |
API to set configuration for NPWRON/Enable pin.
Requirement: REQ_TAG(PDK-5808), REQ_TAG(PDK-9111), REQ_TAG(PDK-9162) Design: did_pmic_gpio_cfg_readback Architecture: aid_pmic_gpio_cfg
This function is used to set the required configuration for the
NPWRON OR ENABLE pin when corresponding validParam bit field is set
in the Pmic_GpioCfg_t
For more information \ref Pmic_GpioCfg_t
NPWRON is valid only for TPS6594x Leo Device.
Note: In this API, the default PMIC device is assumed as TPS6594x
LEO PMIC. While adding support for New PMIC device, developer
need to update the API functionality for New PMIC device
accordingly.
| pPmicCoreHandle | [IN] PMIC Interface Handle |
| gpioCfg | [IN] Set NPWRON or ENABLE GPIO pin configuration |
| int32_t Pmic_gpioGetNPwronEnablePinConfiguration | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| Pmic_GpioCfg_t * | pGpioCfg | ||
| ) |
API to get configuration for NPWRON/Enable pin.
Requirement: REQ_TAG(PDK-5808) Design: did_pmic_gpio_cfg_readback Architecture: aid_pmic_gpio_cfg
This function is used to read the configuration for the
NPWRON OR ENABLE pin when corresponding validParam bit field is set
in the Pmic_GpioCfg_t
For more information \ref Pmic_GpioCfg_t
NPWRON is valid only for TPS6594x Leo Device.
Note: In this API, the default PMIC device is assumed as TPS6594x
LEO PMIC. While adding support for New PMIC device, developer
need to update the API functionality for New PMIC device
accordingly.
| pPmicCoreHandle | [IN] PMIC Interface Handle |
| pGpioCfg | [IN/OUT] Pointer to store NPWRON OR ENABLE GPIO pin configuration |
| int32_t Pmic_gpioTps6594xNPwronPinGetValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
| uint8_t * | pPinValue | ||
| ) |
API to get PMIC GPIO NPWRON/Enable pin value.
Requirement: REQ_TAG(PDK-9124) Design: did_pmic_gpio_cfg_readback Architecture: aid_pmic_gpio_cfg
This function is used to read the signal level of the NPWRON/Enable
pin.
| pPmicCoreHandle | [IN] PMIC Interface Handle |
| pPinValue | [OUT] Pointer to store PMIC GPIO signal level High/Low. Valid values Pmic_Gpio_SignalLvl |