Kernel for convolving input data with an input filter.
- The kernel support computation of convolutions of a vector of several inputs in one kernel call.
|
| int32_t | DSPLIB_fir_getHandleSize (DSPLIB_fir_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_getSizes (const DSPLIB_fir_InitArgs *pKerInitArgs, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsFilter, DSPLIB_bufParams2D_t *bufParamsOut) |
| | This is a query function to calculate the sizes of input, filter and the output buffers. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsFilter, DSPLIB_bufParams2D_t *bufParamsOut, DSPLIB_fir_InitArgs *pKerInitArgs) |
| | This function should be called before the DSPLIB_fir_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilter, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_fir_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to DSPLIB_fir_init function. This function is called with the same parameters as the DSPLIB_fir_init, and this function must be called before the DSPLIB_fir_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut) |
| | This function is the main kernel compute function. More...
|
| |
| DSPLIB_STATUS | DSPLIB_fir_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pFilter, const void *restrict pOut) |
| | This function checks the validity of the parameters passed to DSPLIB_fir_exec function. This function is called with the same parameters as the DSPLIB_fir_exec, and this function must be called before the DSPLIB_fir_exec is called. More...
|
| |
| void | DSPLIB_fir_perfEst (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilter, const DSPLIB_bufParams2D_t *bufParamsOut, uint64_t *archCycles, uint64_t *estCycles) |
| | This is a utility function that gives an estimate of the cycles consumed for the kernel execution. More...
|
| |
◆ DSPLIB_fir_getHandleSize()
This is a query function to calculate the size of internal handle.
- Parameters
-
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
- Returns
- Size of the buffer in bytes
◆ DSPLIB_fir_getSizes()
This is a query function to calculate the sizes of input, filter and the output buffers.
- Parameters
-
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of filter buffer |
| [in] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
◆ DSPLIB_fir_init()
This function should be called before the DSPLIB_fir_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of filter buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
◆ DSPLIB_fir_init_checkParams()
This function checks the validity of the parameters passed to DSPLIB_fir_init function. This function is called with the same parameters as the DSPLIB_fir_init, and this function must be called before the DSPLIB_fir_init is called.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of filter buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
◆ DSPLIB_fir_exec()
This function is the main kernel compute function.
Please refer to details under DSPLIB_fir
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pFilter | : Pointer to buffer holding the filter data |
| [out] | pOut | : Pointer to buffer holding the output data |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
- Assumptions:
-
- Performance Considerations:
- For best performance,
- the input and output data buffers are expected to be in L2 memory
- the buffer pointers are assumed to be 64-byte aligned
◆ DSPLIB_fir_exec_checkParams()
This function checks the validity of the parameters passed to DSPLIB_fir_exec function. This function is called with the same parameters as the DSPLIB_fir_exec, and this function must be called before the DSPLIB_fir_exec is called.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pFilter | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output matrix |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
◆ DSPLIB_fir_perfEst()
This is a utility function that gives an estimate of the cycles consumed for the kernel execution.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of the input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of the filter buffer |
| [in] | bufParamsOut | : Pointer to the structure containing dimensional information of the output buffer |
| [out] | archCycles | : Cycles estimated for the compute, startup and teardown |
| [out] | estCycles | : Cycles estimated for the compute, startup, teardown and any associated overhead |