4.19. PMIC

4.19.1. Overview

4.19.1.1. Introduction

The power-management integrated circuit (PMIC) is designed for powering embedded systems or system on chip(SoC) in Automotive or Industrial applications.

The PMIC Driver supports Leo PMIC TPS65941. The Leo PMIC contains eleven GPIOs each with multiple functions and configurable features. The Leo PMIC includes Real Time Clock (RTC) which provides the alarm and time-keeping functions. It provides time information and calendar information. RTC can generate timer interrupts(periodic interrupts) and alarm interrupts (precise interrupts). GPIO can generate interrupts which indicates the High/Rising-Edge or the Low/Falling-Edge detection at the GPIO1 through GPIO11 pins.

The Leo PMIC contains two I2C interface channels. I2C channel 1 (I2C1) is the main channel with access to the registers which control the RTC and GPIO registers. I2C channel 2 (I2C2), which is available through GPIO1 and GPIO2 pins, is dedicated for accessing the Q&A Watchdog communication registers.

4.19.2. Supported PMICS

  1. Leo PMIC - TPS65941 (Texas Instruments)

4.19.3. Directory Structure

The directory structure of PMIC is as follows:

Directory Description
include Contains the interface files for PMIC Driver
src Contains source(.c) files for the driver
test Contains Unit test code for utilizing PMIC interfaces

4.19.4. Build and Run

This section assumes that PDK has been installed at PDK_INSTALL_DIR.

PDK_ROOT_PATH = PDK_INSTALL_DIR/packages
PDK_BUILD_PATH = PDK_INSTALL_DIR/packages/ti/build
PMIC_PATH = PDK_INSTALL_DIR/drv/pmic

4.19.4.1. Build targets

The driver provides targets for building library and unit tests. The library and unit tests can be built from PDK_BUILD_PATH.

  • Change directory to Processor SDK root path cd <PROCESSOR_PDK_ROOT_PATH>
  • Run the setup script to setup build environment setupenv.bat (Windows OS) / source ./setupenv.sh (Linux OS)
  • change directory to build folder cd <PDK_BUILD_PATH>

Windows OS

Target Command Description
Library gmake -s COMP=pmic CORE=mcu1_0 PMIC Driver library #Supported for mcu1_0(R5F) and mcu1_1(R5F)core
pmic_rtc_testapp gmake -s pmic_rtc_testapp CORE=mcu1_0 PMIC RTC Unit test code #Supported for mcu1_0(R5F) and mcu1_1(R5F)core
pmic_gpio_testapp gmake -s pmic_gpio_testapp CORE=mcu1_0 PMIC GPIO Unit test code #Supported for mcu1_0(R5F) and mcu1_1(R5F)core

Linux OS

Target Command Description
Library make -s COMP=pmic CORE=mcu1_0 OS=linux PMIC Driver library #Supported for mcu1_0(R5F) and mcu1_1(R5F)core
pmic_rtc_testapp make -s pmic_rtc_testapp CORE=mcu1_0 OS=linux PMIC RTC Unit test code #Supported for mcu1_0(R5F) and mcu1_1(R5F)core
pmic_gpio_testapp make -s pmic_gpio_testapp CORE=mcu1_0 OS=linux PMIC GPIO Unit test code #Supported for mcu1_0(R5F) and mcu1_1(R5F)core

4.19.5. User Interface

4.19.5.1. API descriptions

API reference for application:

#include <pmic.h>

PMIC Initialization for Main I2C Bus

Steps to be followed for PMIC Initialization of Main I2C Bus

Pmic_CoreCfg_t        pmicConfigData =
{
    PMIC_CFG_DEVICE_TYPE_VALID_SHIFT | PMIC_CFG_COMM_MODE_VALID_SHIFT \
    PMIC_CFG_SLAVEADDR_VALID_SHIFT | PMIC_CFG_COMM_HANDLE_VALID_SHIFT \
    PMIC_CFG_COMM_IO_WR_VALID_SHIFT | PMIC_CFG_COMM_IO_RD_VALID_SHIFT \
    PMIC_CFG_CRITSEC_START_VALID_SHIFT | PMIC_CFG_CRITSEC_STOP_VALID_SHIFT ,
    PMIC_MAIN_INST,
    PMIC_DEV_LEO_TPS6594, // Leo PMIC TPS65941 Slave device
    PMIC_INTF_DUAL_I2C,
    LEO_PMICA_SLAVE_ADDR,
    0,
    false,
    Pmic_regRead,
    Pmic_regWrite,
    NULL,
    NULL,
    Pmic_criticalSectionStartFn,
    Pmic_crit   icalSectionStopFn,
};

// For I2C Interface
pmicStatus = Pmic_i2c_lld_intf_setup(pmicConfigData, PMIC_MAIN_INST);
...
or
// For SPI Interface
pmicStatus = Pmic_spi_lld_intf_setup(pmicConfigData);
...
Pmic_init(pmicConfigData, pPmicCoreHandle);

PMIC Initialization for QA I2C Bus

Steps to be followed for PMIC Initialization of QA I2C Bus

Pmic_CoreCfg_t        pmicCfgData =
{
    PMIC_CFG_QASLAVEADDR_VALID_SHIFT | PMIC_CFG_QACOMM_HANDLE_VALID_SHIFT  ,
    PMIC_QA_INST,
    0,
    0,
    LEO_PMICA_WDG_SLAVE_ADDR,
    false,
    NULL,
    NULL,
    NULL,
    NULL,
    NULL,
    NULL,
};

Pmic_dual_i2c_pin_setup(pmicHandle);
.....
pmicStatus = Pmic_i2c_lld_intf_setup(pmicCfgData, PMIC_QA_INST);
...
Pmic_init(pmicCfgData, pPmicCoreHandle);

Pmic_init() API is called for creating pPmicCoreHandle to be able to talk to driver.

The Pmic_init() API takes a pointer to Pmic_CoreCfg_t as an input. The parameter Pmic_CoreCfg_t contains various parameters which are needed to prepare PMIC driver handle

Definition:

Defined in pimc.h interface file as **Pmic_init()**

Pmic_init() API provides a software initialization for the driver. Any application using PMIC Driver must call this API.

  • Application need to initialize pmicCorehandle structure in two steps for Dual I2C and one step for Single I2C or SPI Interface using validParams struture member
  • Application needs to be provide these functions to PMIC driver. After PMIC driver initialization these function will called by PMIC driver for PMIC register read and write
  • Application need to create pmicCorehandle structure for each PMIC device. For example - Application can create a pmicLeoCorehandle for Leo PMIC device and pmicHeraCorehandle for Hera PMIC device
Pmic_regRead                - PMIC I2C/SPI read function

Pmic_regWrite               - PMIC I2C/SPI write function

Pmic_criticalSectionStartFn - Critical section start function

Pmic_criticalSectionStopFn  - Critical section stop function

Pmic_i2c_lld_intf_setup     - Interface setup function for PMIC to create
instance and initialise the Main/QA I2C Bus for PMIC Communication based on
instance type

Pmic_dual_i2c_pin_setup     - Configures GPIO1 and GPIO2 pins as I2C pins
for QA I2C Bus interface setup

Pmic_spi_lld_intf_setup     - Interface setup function for PMIC to create
instance and initialise the SPI Bus for PMIC Communication

PMIC I2C interface setup for Main I2C Bus - Pmic_i2c_lld_intf_setup()

Interface setup function for PMIC to create instance and initialise the Main/QA I2C Bus for PMIC Communication based on instance type

setConfigI2C(0, CSL_WKUP_I2C0_CFG_BASE);
...
I2C_init();
...
I2C_Params_init(&i2cParams);
...
i2cHandle = I2C_open(0, &i2cParams);
...
pPmicConfigData->pCommHandle = i2cHandle;

Similarly we need to define PMIC I2C interface setup for QA I2C Bus

PMIC de-initialization - Pmic_deinit()

  • De-initialization of PMIC - This de-initialization is specific to the application.
  • It only de-initializes the LLD being used for this Instance

Definition:

Defined in pimc.h interface file as **Pmic_deinit()**

4.19.6. Unit Test code

Name Description Expected Results SoC Supported
RTC test code Verify the features of PMIC RTC Sub System The test code tests all the rtc test cases and prints pass on successful completion SOC_J721E SOC_J7200
GPIO test code Verify the features of PMIC GPIO Sub System The test code tests all the gpio testcases and prints pass on successful completion SOC_J721E SOC_J7200

4.19.7. Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti \drv\PMIC\docs\doxygen\html\index. html