4.20. MMCSD

4.20.1. Introduction

MMCSD module provides an interface between CPU and any MMCSD-bus-compatible device that connects via MMCSD serial bus. External components attached to MMCSD bus can serially transmit/receive data to/from the CPU device through two-wire interface

Key Features

Type of transfers
  •  Read
  •  Write
  •  Write followed by read
Operating modes
  •  Blocking(interrupt or Non interrupt)
  •  Callback mode(interrupt)
Supports only master mode. Slave mode is not supported

4.20.2. User Interface

4.20.2.1. Driver Configuration

Board Specific Configuration

All board specific configurations eg:enabling clock and pin-mux for UART pins are required before calling any driver APIs.By default Board_Init() API supports all initialization sequence for TI supported EVMs. In addition it initializes UART instance for Console/STDIO. Once board specific configuration is complete MMCSD_init() API can be called to initialize driver.

MMCSD Configuration Structure

The MMCSD_soc.c file binds driver with hardware attributes on the board through MMCSD_config structure. This structure must be initialized before the MMCSD_init() function is called and cannot be changed afterwards. For details about the individual fields of this structure, see the API Guide.

4.20.3. Application

4.20.3.1. Examples & Unit tests

Name Description Expected Results Supported SOCs Build Type
MMCSD_TestApp Unit Test application demonstrating write and read a fixed number of bytes into MMCSD card. Verifies written data pattern to conclude PASS/FAIL. Prints on console All tests have passed AM65x J721e J7200 AM64x Makefile
MMCSD_DMA_TestApp Functionally same as MMCSD_TestApp but with DMA enabled Prints on console All tests have passed AM65x J721e J7200 AM64x Makefile
MMCSD_EMMC_TestApp Unit Test application demonstrating write and read a fixed number of bytes into the onboard EMMC.Verifies written data pattern to conclude PASS/FAIL. Prints on console All tests have passed AM65x J721e J7200 AM64x Makefile
MMCSD_EMMC_DMA_TestApp Functionally Same as EMMC_TestApp but using DMA mode Prints on console All tests have passed J7200 AM65x J721e AM64x Makefile
MMCSD_Baremetal_TestApp Baremetal version of MMCSD_TestApp Prints on console All tests have passed J7200 AM65x J721e AM64x Makefile
MMCSD_Baremetal_DMA_TestApp Baremetal version of MMCSD_EMMC_TestApp Prints on console All tests have passed J7200 AM65x J721e AM64x Makefile
MMCSD_Baremetal_EMMC_TestApp Baremetal version of MMCSD_EMMC_TestApp Prints on console All tests have passed J7200 AM65x J721e AM64x Makefile
MMCSD_Baremetal_EMMC_DMA_TestApp Functionally same as MMCSD_Baremetal_EMMC_TestApp but with DMA enabled Prints on console All tests have passed J7200 AM65x J721e AM64x Makefile
MMCSD_Regression_TestApp Menu driven regression test which tests various configurations of SD card Prints on console All tests have passed J7200 AM65x J721e AM64x Makefile
MMCSD_EMMC_Regression_TestApp Menu driven regression test which tests various configurations of EMMC Prints on console All tests have passed J7200 AM65x J721e AM64x Makefile

4.20.4. Building MMCSD Test applications via makefiles

  • MMCSD Test applications and dependent libraries are built from the top level mmcsd makefile
  • Refer to the Processor SDK RTOS Getting Started Guide for details of how to setup the build environment. Once you have setup the build environment, issue the following commands:
    • cd <pdk>/packages/
    • To build: make mmcsd
    • To clean: make mmcsd_clean
  • Similarly, to build at the module level, issue the following commands for rebuilding :
    • cd <pdk>/packages/ti/drv/mmcsd
    • To build: make all
    • To clean: make clean