RTC time configuration. The Pmic_RtcTime_s structure contains set of time parameters to set/get the RTC time.
- Parameters
-
validParams | Validate params Bits. Depending on the parameters want to get/set, corresponding bits should be set in validParam. For valid values: Pmic_RtcTimeValidParamBits |
seconds | Value to represent Seconds. Valid only when PMIC_RTC_TIME_CFG_SEC_VALID bit of validParams is set. |
minutes | Value to represent Minutes. Valid only when PMIC_RTC_TIME_CFG_MIN_VALID bit of validParams is set. |
hour | Value to represent Hours. Valid only when PMIC_RTC_TIME_CFG_HRS_VALID bit of validParams is set. |
timeMode | Value to represent Time Mode. For valid values: Pmic_RtcTimeMode. Valid only when PMIC_RTC_TIME_CFG_TIMEMODE_VALID bit of validParams is set. |
meridianMode | Value to represent Maridian Mode. For valid values: Pmic_RtcMeridienMode. Valid only when PMIC_RTC_TIME_CFG_MERIDIAN_VALID bit of validParams is set. |