PMIC FSM configuration structure. Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs.
- Parameters
-
validParams | Selection of structure parameters to be set, from the combination of Pmic_FsmValidParamCfg and the corresponding member value must be updated Valid values Pmic_FsmValidParamCfg |
fastBistEn | Enable/Disable Fast BIST Valid values Pmic_Fsm_FastBist_Enable Valid only when PMIC_FSM_CFG_FAST_BIST_EN_VALID bit is set |
lpStandbySel | Low Power Standby State Selection Valid values Pmic_Fsm_LpStandby_Sel Valid only when PMIC_FSM_CFG_LP_STANDBYSEL_VALID bit is set |
ilimIntfsmCtrlEn | Enable/Disable Buck/LDO regulators ILIM interrupts affect FSM triggers Valid values Pmic_Fsm_IlimInt_FsmCtrl_En Valid only when PMIC_FSM_CFG_ILIM_INT_FSMCTRL_EN_VALID bit is set |
fsmStarupDestSel | Select FSM Startup Destination Valid values Pmic_FSM_StartupDest_Select Valid only when PMIC_FSM_CFG_FSM_STARTUP_DEST_SEL_VALID bit is set |