PDK API Guide for J721E
|
PMIC Interface Handle. Contains various PMIC driver instance specific information. like, the PMIC device type, PMIC interface mode, Slave addresses, various application defined API function pointers for LLD and Critical sections.
Note: Pmic_init() configures the Pmic Handle information and provide pmic core handle to user application. User should ensure that application shall not modify the PMIC Handle information.
pPmic_SubSysInfo | PMIC driver subsystem information |
drvInitStatus | PMIC Driver initialization status. Valid driver status: For Main instance: DRV_INIT_STATUS | PMIC_MAIN_INST. For QA instance: DRV_INIT_STATUS | PMIC_QA_INST. |
pmicDeviceType | PMIC device type |
pmicDevRev | PMIC device revision ID |
pmicDevSiliconRev | PMIC device silicon revision ID |
commMode | Interface mode - Single I2C, Dual I2C or SPI. |
slaveAddr | Main Interface Slave Address |
qaSlaveAddr | WDOG QA Interface Slave Address |
nvmSlaveAddr | NVM Slave Address which provides only read access to CRC status of Page-1 Application shall use this slave address to read only CRC status. Application shall not do any write operations using this slave address |
i2c1Speed | I2C1 Speed when commMode is Single or Dual I2C |
i2c2Speed | I2C2 Speed when commMode is Dual I2C |
crcEnable | Parameter to enable/disable CRC For Valid Values: Pmic_CrcEnableCfg |
pFnPmicCommIoRead | Pointer to I2C/SPI Comm LLD Read Function |
pFnPmicCommIoWrite | Pointer to I2C/SPI Comm LLD Write Function |
pCommHandle | Pointer to Handle for I2C1/SPI Main Interface |
pQACommHandle | Pointer to Handle for I2C2-QA Interface |
pFnPmicCritSecStart | Pointer to Pmic Critical-Section Start Function |
pFnPmicCritSecStop | Pointer to Pmic Critical-Section Stop Function |
Data Fields | |
const Pmic_DevSubSysInfo_t * | pPmic_SubSysInfo |
uint32_t | drvInitStatus |
uint8_t | pmicDeviceType |
uint8_t | pmicDevRev |
uint8_t | pmicDevSiliconRev |
uint8_t | commMode |
uint8_t | slaveAddr |
uint8_t | qaSlaveAddr |
uint8_t | nvmSlaveAddr |
uint8_t | i2c1Speed |
uint8_t | i2c2Speed |
bool | crcEnable |
void * | pCommHandle |
void * | pQACommHandle |
int32_t(* | pFnPmicCommIoRead )(struct Pmic_CoreHandle_s *pmicCorehandle, uint8_t instType, uint16_t regAddr, uint8_t *pRxBuf, uint8_t bufLen) |
int32_t(* | pFnPmicCommIoWrite )(struct Pmic_CoreHandle_s *pmicCorehandle, uint8_t instType, uint16_t regAddr, uint8_t *pTxBuf, uint8_t bufLen) |
void(* | pFnPmicCritSecStart )(void) |
void(* | pFnPmicCritSecStop )(void) |
const Pmic_DevSubSysInfo_t* Pmic_CoreHandle_t::pPmic_SubSysInfo |
uint32_t Pmic_CoreHandle_t::drvInitStatus |
uint8_t Pmic_CoreHandle_t::pmicDeviceType |
uint8_t Pmic_CoreHandle_t::pmicDevRev |
uint8_t Pmic_CoreHandle_t::pmicDevSiliconRev |
uint8_t Pmic_CoreHandle_t::commMode |
uint8_t Pmic_CoreHandle_t::slaveAddr |
uint8_t Pmic_CoreHandle_t::qaSlaveAddr |
uint8_t Pmic_CoreHandle_t::nvmSlaveAddr |
uint8_t Pmic_CoreHandle_t::i2c1Speed |
uint8_t Pmic_CoreHandle_t::i2c2Speed |
bool Pmic_CoreHandle_t::crcEnable |
void* Pmic_CoreHandle_t::pCommHandle |
void* Pmic_CoreHandle_t::pQACommHandle |
int32_t(* Pmic_CoreHandle_t::pFnPmicCommIoRead) (struct Pmic_CoreHandle_s *pmicCorehandle, uint8_t instType, uint16_t regAddr, uint8_t *pRxBuf, uint8_t bufLen) |
int32_t(* Pmic_CoreHandle_t::pFnPmicCommIoWrite) (struct Pmic_CoreHandle_s *pmicCorehandle, uint8_t instType, uint16_t regAddr, uint8_t *pTxBuf, uint8_t bufLen) |
void(* Pmic_CoreHandle_t::pFnPmicCritSecStart) (void) |
void(* Pmic_CoreHandle_t::pFnPmicCritSecStop) (void) |