![]() |
PDK API Guide for J721E
|
Basic MuxIntcP Output Parameters.
Structure that contains the parameters returned from MuxIntcP_create when creating a MuxIntcP instance.
Data Fields | |
uintptr_t | arg |
uint32_t | eventId |
MuxIntcFxn | muxIntcFxn |
uintptr_t MuxIntcP_outParams::arg |
Argument passed out from the MuxIntc function.
uint32_t MuxIntcP_outParams::eventId |
K2: Mapped CorePac Event Id, input event to CorePac IntC; AM: not used
MuxIntcFxn MuxIntcP_outParams::muxIntcFxn |
K2: CIC dispatch function for Intc; AM: not used