PDK API Guide for J721E
|
MDIO port object.
Data Fields | |
EnetMod_Obj | enetMod |
bool | isMaster |
uint32_t | mdc_halfPeriodInNsec |
EnetMod_Obj Mdio_Obj::enetMod |
EnetMod must be the first member
bool Mdio_Obj::isMaster |
Whether this MDIO object has master behavior or not. When in master role, the module will perform all MDIO configuration. In slave role, MDIO configuration is bypassed.
uint32_t Mdio_Obj::mdc_halfPeriodInNsec |
MDIO bit banging delay in terms of nanosecond. Applicable only when MDIO mode is set to manual mode