![]() |
PDK API Guide for J721E
|
Parameters of the media attached to the controller.
The MMCSD_mediaParams structure contains the characteristics of the media (SD/eMMC/MMC) attached to the controller
Data Fields | |
uint32_t | blockSize |
uint64_t | blockCount |
uint64_t | size |
uint32_t MMCSD_mediaParams::blockSize |
Size of the block in bytes
uint64_t MMCSD_mediaParams::blockCount |
Number of blocks present
uint64_t MMCSD_mediaParams::size |
Size of the media (SD/eMMC/MMC) in bytes