![]() |
PDK API Guide for J721E
|
Basic HeapP Parameters.
Structure that contains the parameters are passed into HeapP_create when creating a HeapP instance.
Data Fields | |
void * | buf |
uint32_t | size |
void* HeapP_Params::buf |
Base address of memory to be used as heap
uint32_t HeapP_Params::size |
Size of memory block that is to be used as heap