![]() |
PDK API Guide for J721E
|
EventCombinerP interface
Files | |
file | EventCombinerP.h |
Event Combiner routines for the RTOS Porting Interface. | |
Functions | |
int32_t | EventCombinerP_disableEvent (uint32_t eventId) |
Function to disable an event inside event combiner. More... | |
int32_t | EventCombinerP_enableEvent (uint32_t eventId) |
Function to enable an event inside event combiner. More... | |
int32_t | EventCombinerP_clearEvent (uint32_t eventId) |
Function to clear an event inside event combiner. More... | |
int32_t | EventCombinerP_dispatchPlug (uint32_t eventId, EventCombinerP_FuncPtr eventIsrRoutine, uintptr_t arg, bool unmask) |
Function to plug an ISR handler to an event inside event combiner. More... | |
int32_t | EventCombinerP_dispatchUnplug (uint32_t eventId) |
Function to unplug an ISR handler to an event inside event combiner. More... | |
HwiP_Handle | EventCombinerP_getHwi (uint32_t groupNum) |
Function to return the Hwi Handle corresponding to an event combiner group number. More... | |
int32_t | EventCombinerP_getIntNum (int32_t groupNum) |
Function to return the interrupt vector number corresponding to a group number (0-3) More... | |
int32_t | EventCombinerP_SingleRegisterInt (int32_t groupNum, int32_t intNum) |
Function to register single event combiner group to a vector number. More... | |
int32_t | EventCombinerP_GroupRegisterInt (int32_t intNum[]) |
Function to register single event combiner group to a vector number. More... | |
Typedefs | |
typedef void(* | EventCombinerP_FuncPtr) (uint32_t arg) |
Osal Event Combiner return Codes | |
#define | OSAL_EVTCOMBINE_GROUPREG_SUCCESS (0) |
#define | OSAL_EVTCOMBINE_ERR_GROUPREG_REGISTER_ERR (-1) |
#define | OSAL_EVTCOMBINE_ERR_GROUPREG_INVALID_INTNUM (-2) |
Osal Event Combiner Defualt Group Interrupts | |
Deafult group interrupt numbers for the Event Combiner These are the system default interrupt numbers if the Event Combiner has already not been registered If applications register Event Combiners during startup, these values may not be used (in SYSBIOS case) If not, these are the interrupts reserved for Event Combiner group events (0-3). These defaults are stored in Osal_HwAttrs.ECM_intNum[] and can be obtained by the application at run time through the OSAL API Osal_getHwAttrs(). These values also can be modified using Osal_setHwAttrs(Osal_HwAttrs,OSAL_HWATTR_SET_ECM_INT) | |
#define | OSAL_ECM_GROUP0_INT 4 |
#define | OSAL_ECM_GROUP1_INT 5 |
#define | OSAL_ECM_GROUP2_INT 6 |
#define | OSAL_ECM_GROUP3_INT 7 |
#define OSAL_EVTCOMBINE_GROUPREG_SUCCESS (0) |
Successful call
#define OSAL_EVTCOMBINE_ERR_GROUPREG_REGISTER_ERR (-1) |
Registration Error
#define OSAL_EVTCOMBINE_ERR_GROUPREG_INVALID_INTNUM (-2) |
Invalid interrupt number
#define OSAL_ECM_GROUP0_INT 4 |
ECM group 0 default interrupt: 4
#define OSAL_ECM_GROUP1_INT 5 |
ECM group 1 default interrupt: 5
#define OSAL_ECM_GROUP2_INT 6 |
ECM group 2 default interrupt: 6
#define OSAL_ECM_GROUP3_INT 7 |
ECM group 3 default interrupt: 7
typedef void(* EventCombinerP_FuncPtr) (uint32_t arg) |
int32_t EventCombinerP_disableEvent | ( | uint32_t | eventId | ) |
Function to disable an event inside event combiner.
eventId | event ID to be disabled in the event combiner |
int32_t EventCombinerP_enableEvent | ( | uint32_t | eventId | ) |
Function to enable an event inside event combiner.
eventId | event ID to be disabled in the event combiner |
int32_t EventCombinerP_clearEvent | ( | uint32_t | eventId | ) |
Function to clear an event inside event combiner.
eventId | event ID to be cleared in the event combiner |
int32_t EventCombinerP_dispatchPlug | ( | uint32_t | eventId, |
EventCombinerP_FuncPtr | eventIsrRoutine, | ||
uintptr_t | arg, | ||
bool | unmask | ||
) |
Function to plug an ISR handler to an event inside event combiner.
eventId | The event id (4-127) |
eventIsrRoutine | The ISR routine for servicing the event |
arg | The argument to the ISR routine |
unmask | Unmask the event |
int32_t EventCombinerP_dispatchUnplug | ( | uint32_t | eventId | ) |
Function to unplug an ISR handler to an event inside event combiner.
eventId | The event id (4-127) |
HwiP_Handle EventCombinerP_getHwi | ( | uint32_t | groupNum | ) |
Function to return the Hwi Handle corresponding to an event combiner group number.
groupNum | The event combiner group id (0-3) |
int32_t EventCombinerP_getIntNum | ( | int32_t | groupNum | ) |
Function to return the interrupt vector number corresponding to a group number (0-3)
groupNum | The event combiner group id (0-3) |
int32_t EventCombinerP_SingleRegisterInt | ( | int32_t | groupNum, |
int32_t | intNum | ||
) |
Function to register single event combiner group to a vector number.
groupNum | The event combiner group id (0-3) |
intNum | The interrupt vector id (4-15) |
int32_t EventCombinerP_GroupRegisterInt | ( | int32_t | intNum[] | ) |
Function to register single event combiner group to a vector number.
intNum | [] List of interrupt vector ids (4-15) per ECM group(0-3) |