![]() |
PDK API Guide for J721E
|
This is the include file for the CLEC CSL-FL module.
Go to the source code of this file.
Data Structures | |
struct | CSL_ClecEventConfig |
This structure contains the parameters to setup a event. More... | |
Macros | |
#define | CSL_CLEC_MAX_EVT_IN (2047U) |
Maximum number of input events supported by CLEC. This is just the maximum registers supported for programming. The actual event supported depends on the SOC. More... | |
#define | CSL_CLEC_MAX_EXT_EVT_OUT (128U) |
Maximum external events. More... | |
#define | CSL_CLEC_MAX_C7X_EVT_OUT (64U) |
Maximum C7x events. More... | |
CLEC route map - Determines where the event will be routed. | |
#define | CSL_CLEC_RTMAP_DISABLE ((uint32_t)((uint32_t) 0x0001U) << 0U) |
Send event to None. More... | |
#define | CSL_CLEC_RTMAP_SYS ((uint32_t)((uint32_t) 0x0001U) << 1U) |
Send event to SOC as Compute Cluster interrupt output. More... | |
#define | CSL_CLEC_RTMAP_CPU_0 ((uint32_t)((uint32_t) 0x0000U) << 2U) |
Send event to CPU 0 - Typically reserved for ARM. More... | |
#define | CSL_CLEC_RTMAP_CPU_1 ((uint32_t)((uint32_t) 0x0001U) << 2U) |
Send event to CPU 1 - Typically reserved for ARM. More... | |
#define | CSL_CLEC_RTMAP_CPU_2 ((uint32_t)((uint32_t) 0x0002U) << 2U) |
Send event to CPU 2 - Typically reserved for ARM. More... | |
#define | CSL_CLEC_RTMAP_CPU_3 ((uint32_t)((uint32_t) 0x0003U) << 2U) |
Send event to CPU 3 - Typically reserved for ARM. More... | |
#define | CSL_CLEC_RTMAP_CPU_4 ((uint32_t)((uint32_t) 0x0004U) << 2U) |
Send event to CPU 4 - Typically C7x core starts from this. More... | |
#define | CSL_CLEC_RTMAP_CPU_5 ((uint32_t)((uint32_t) 0x0005U) << 2U) |
Send event to CPU 5. More... | |
#define | CSL_CLEC_RTMAP_CPU_6 ((uint32_t)((uint32_t) 0x0006U) << 2U) |
Send event to CPU 6. More... | |
#define | CSL_CLEC_RTMAP_CPU_7 ((uint32_t)((uint32_t) 0x0007U) << 2U) |
Send event to CPU 7. More... | |
#define | CSL_CLEC_RTMAP_CPU_8 ((uint32_t)((uint32_t) 0x0008U) << 2U) |
Send event to CPU 8. More... | |
#define | CSL_CLEC_RTMAP_CPU_9 ((uint32_t)((uint32_t) 0x0009U) << 2U) |
Send event to CPU 9. More... | |
#define | CSL_CLEC_RTMAP_CPU_10 ((uint32_t)((uint32_t) 0x000AU) << 2U) |
Send event to CPU 10. More... | |
#define | CSL_CLEC_RTMAP_CPU_ALL ((uint32_t)((uint32_t) 0x000FU) << 2U) |
Send event to All CPU. More... | |
Functions | |
int32_t | CSL_clecConfigEvent (CSL_CLEC_EVTRegs *pRegs, uint32_t evtNum, const CSL_ClecEventConfig *evtCfg) |
This API sets the event configuration. More... | |
int32_t | CSL_clecSendEvent (CSL_CLEC_EVTRegs *pRegs, uint32_t evtNum) |
This API sends the event specified if the event send is enabled in the event configuration (evtSendEnable) and the output event generated depends on the rtMap, extEvtNum and c7xEvtNum. More... | |
int32_t | CSL_clecClearEvent (CSL_CLEC_EVTRegs *pRegs, uint32_t evtNum) |
This API clear any level interrupt set for the event. More... | |
int32_t | CSL_clecConfigEventLevel (CSL_CLEC_EVTRegs *pRegs, uint32_t evtNum, uint32_t is_level) |
This API does a set or clear of the is_lvl field in CLEC.MRR register. More... | |
int32_t | CSL_clecGetSecureClaimStatus (CSL_CLEC_EVTRegs *pRegs, uint32_t evtNum, uint32_t *secureClaim) |
This API reads the Secure Claim bit field in CLEC.MRR register. More... | |
Variables | |
typedef | __attribute__ |