MCUSW
Eth_Udma_RingEventCfgType Struct Reference

Detailed Description

Eth ring event configuration type Configuration related to ring event.

Data Fields

uint8 ringIdx
 
uint8 eventIdx
 
uint8 virtBitNum
 
uint32 globalEvent
 
uint32 srcOffset
 

Field Documentation

◆ ringIdx

uint8 Eth_Udma_RingEventCfgType::ringIdx

Ring index

◆ eventIdx

uint8 Eth_Udma_RingEventCfgType::eventIdx

Event index

◆ virtBitNum

uint8 Eth_Udma_RingEventCfgType::virtBitNum

Virtual bit number

◆ globalEvent

uint32 Eth_Udma_RingEventCfgType::globalEvent

Global event number

◆ srcOffset

uint32 Eth_Udma_RingEventCfgType::srcOffset

Source Irq offset