![]() |
MCUSW
|
This files defines PWM MCAL configuration structures
Data Structures | |
struct | Pwm_ChannelConfigType_PC |
Pwm channel configuration. More... | |
struct | Pwm_ConfigType_PC |
Pwm configuration structure. More... | |
struct | Pwm_ChannelConfigType |
Pwm channel configuration. More... | |
struct | Pwm_ConfigType |
Pwm configuration structure. More... | |
struct | Pwm_RegisterReadbackType |
PWM register readback structure. More... | |
Functions | |
void | Pwm_Ch11Isr (void) |
PWM Channel 11 ISR. More... | |
Variables | |
const uint32 | Pwm_HwUnitBaseAddr [PWM_MAX_NUM_CHANNELS] |
const struct Pwm_ConfigType_PC_s | PwmChannelConfigSet_PC |
PWM Configuration structure declaration. More... | |
const struct Pwm_ConfigType_s | PwmChannelConfigSet |
Typedefs | |
typedef uint32 | Pwm_PeriodType |
typedef of period value More... | |
typedef uint32 | Pwm_ChannelType |
PWM Channel type. More... | |
typedef uint32 | Pwm_FrequencyType |
typedef of frequency value (Frequency in Hz) More... | |
typedef void(* | Pwm_NotifyFuncType) (void) |
Notification callback function pointer. More... | |
Enumerations | |
enum | Pwm_OutputStateType { PWM_LOW = 0U, PWM_HIGH } |
Possible output states of a PWM channel. More... | |
enum | Pwm_EdgeNotificationType { PWM_RISING_EDGE = 1U, PWM_FALLING_EDGE = 2U, PWM_BOTH_EDGES = 3U } |
Possible edge notification. More... | |
enum | Pwm_ChannelClassType { PWM_FIXED_PERIOD = 0U, PWM_FIXED_PERIOD_SHIFTED, PWM_VARIABLE_PERIOD } |
Period type for pwm channels. Fixed periods prohibit changes to the period length with Pwm_SetPeriod( ). PWM_FIXED_PERIOD_SHIFTED type is not supported due to hardware restrictions of the PWM unit. More... | |
enum | Pwm_epwmOutputCh_t { EPWM_OUTPUT_CH_A = 0U, EPWM_OUTPUT_CH_B = 1U, EPWM_OUTPUT_CH_BOTH_A_AND_B = 2U } |
EPWM outputs in a single epwm channel. More... | |
Macros | |
#define | PWM_PRE_COMPILE_VARIANT (STD_ON ) |
PWM Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time) More... | |
#define | PWM_DEINIT_API (STD_ON) |
Enable/Disable PWM DeInit API. More... | |
#define | PWM_SET_DUTY_CYCLE_API (STD_ON) |
Enable/Disable PWM SetDutyCycle API. More... | |
#define | PWM_SET_OUTPUT_TO_IDLE_API (STD_ON) |
Enable/Disable PWM SetOutputToIdle API. More... | |
#define | PWM_SET_PERIOD_AND_DUTY_API (STD_ON) |
Enable/Disable PWM SetPeriodAndDuty API. More... | |
#define | PWM_VERSION_INFO_API (STD_ON) |
Enable/Disable PWM VersionInfo API. More... | |
#define | PWM_REGISTER_READBACK_API (STD_ON) |
Enable/Disable PWM RegisterReadback API. More... | |
#define | PWM_DUTYCYCLE_UPDATED_ENDPERIOD (STD_ON) |
Enable/Disable PWM Dutycycle update always at the end of the period. More... | |
#define | PWM_PERIOD_UPDATED_ENDPERIOD (STD_ON) |
Enable/Disable PWM Period update always at the end of the period. More... | |
#define | PWM_ISR_TYPE (PWM_ISR_CAT1) |
ISR type. More... | |
#define | PWM_NUM_CHANNELS (1U) |
Number of configured channels. More... | |
#define | PWM_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable PWM dev detect error. More... | |
#define | PWM_NOTIFICATION_SUPPORTED (STD_ON) |
Enable/Disable PWM notifications. More... | |
#define | PWM_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks. More... | |
#define | PWM_INDEX (1U) |
Instance ID for driver module to toggle between GPT and EPWM usage. More... | |
#define | PWM_INSTANCE_ID (PWM_INDEX) |
#define | PWM_USE_GPT |
#define | PWM_TIMEOUT_DURATION (32000U) |
timeout. Each tick is 31.25us (for 32K Counter). Wait for 5s which comes to below value More... | |
#define | PwmConf_PwmChannelConfiguration_PwmChannel_0 (10U) |
Channel ID Symbolic Names Configured channel ID(s) More... | |
#define | PWM_INIT_CONFIG_PC PwmChannelConfigSet |
Pre Compile config macro name. More... | |
#define | PWM_MAX_NUM_CHANNELS (30U) |
#define | PWM_CHANNEL11 (10U) |
GP timer 11 instance, in MCU DOMAIN. More... | |
#define PWM_PRE_COMPILE_VARIANT (STD_ON ) |
PWM Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time)
#define PWM_DEINIT_API (STD_ON) |
Enable/Disable PWM DeInit API.
#define PWM_SET_DUTY_CYCLE_API (STD_ON) |
Enable/Disable PWM SetDutyCycle API.
#define PWM_SET_OUTPUT_TO_IDLE_API (STD_ON) |
Enable/Disable PWM SetOutputToIdle API.
#define PWM_SET_PERIOD_AND_DUTY_API (STD_ON) |
Enable/Disable PWM SetPeriodAndDuty API.
#define PWM_VERSION_INFO_API (STD_ON) |
Enable/Disable PWM VersionInfo API.
#define PWM_REGISTER_READBACK_API (STD_ON) |
Enable/Disable PWM RegisterReadback API.
#define PWM_DUTYCYCLE_UPDATED_ENDPERIOD (STD_ON) |
Enable/Disable PWM Dutycycle update always at the end of the period.
#define PWM_PERIOD_UPDATED_ENDPERIOD (STD_ON) |
Enable/Disable PWM Period update always at the end of the period.
#define PWM_ISR_TYPE (PWM_ISR_CAT1) |
ISR type.
#define PWM_NUM_CHANNELS (1U) |
Number of configured channels.
#define PWM_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable PWM dev detect error.
#define PWM_NOTIFICATION_SUPPORTED (STD_ON) |
Enable/Disable PWM notifications.
#define PWM_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks.
#define PWM_INDEX (1U) |
Instance ID for driver module to toggle between GPT and EPWM usage.
#define PWM_INSTANCE_ID (PWM_INDEX) |
#define PWM_USE_GPT |
#define PWM_TIMEOUT_DURATION (32000U) |
timeout. Each tick is 31.25us (for 32K Counter). Wait for 5s which comes to below value
#define PwmConf_PwmChannelConfiguration_PwmChannel_0 (10U) |
Channel ID Symbolic Names Configured channel ID(s)
Channel identifiers
#define PWM_INIT_CONFIG_PC PwmChannelConfigSet |
Pre Compile config macro name.
#define PWM_MAX_NUM_CHANNELS (30U) |
#define PWM_CHANNEL11 (10U) |
GP timer 11 instance, in MCU DOMAIN.
typedef uint32 Pwm_PeriodType |
typedef of period value
typedef uint32 Pwm_ChannelType |
PWM Channel type.
typedef uint32 Pwm_FrequencyType |
typedef of frequency value (Frequency in Hz)
typedef void(* Pwm_NotifyFuncType) (void) |
Notification callback function pointer.
enum Pwm_OutputStateType |
enum Pwm_ChannelClassType |
Period type for pwm channels. Fixed periods prohibit changes to the period length with Pwm_SetPeriod( ). PWM_FIXED_PERIOD_SHIFTED type is not supported due to hardware restrictions of the PWM unit.
Enumerator | |
---|---|
PWM_FIXED_PERIOD | Period is immutable |
PWM_FIXED_PERIOD_SHIFTED | Period is immutable with phase shift |
PWM_VARIABLE_PERIOD | Period is variable |
enum Pwm_epwmOutputCh_t |
void Pwm_Ch11Isr | ( | void | ) |
PWM Channel 11 ISR.
const uint32 Pwm_HwUnitBaseAddr[PWM_MAX_NUM_CHANNELS] |
const struct Pwm_ConfigType_PC_s PwmChannelConfigSet_PC |
PWM Configuration structure declaration.
const struct Pwm_ConfigType_s PwmChannelConfigSet |