![]() |
MCUSW
|
This files defines GPT MCAL configuration structures
Data Structures | |
struct | Gpt_ChannelConfigType |
Configuration per channel. More... | |
struct | Gpt_ChannelConfigType_PC |
SPI sequence config structure parameters Pre-Compile only. More... | |
struct | Gpt_ConfigType |
global configuration of the driver More... | |
struct | Gpt_RegisterReadbackType |
GPT register readback structure. More... | |
Functions | |
void | Gpt_Ch12Isr (void) |
GPT Channel ISR. More... | |
void | Gpt_Ch7Isr (void) |
void | Gpt_Ch10Isr (void) |
void | Gpt_Ch16Isr (void) |
void | Gpt_Ch30Isr (void) |
Variables | |
const struct Gpt_ConfigType_s | GptChannelConfigSet |
GPT Configuration. More... | |
const uint32 | Gpt_TimerBaseAddr [GPT_CH_GPTIMER_MAX] |
Base Address of the timer peripherals. More... | |
Typedefs | |
typedef uint32 | Gpt_ChannelType |
Type describing the Gpt channel. More... | |
typedef uint32 | Gpt_ValueType |
Type describing the timeout value. More... | |
typedef void(* | Gpt_NotifyType) (void) |
Notification callback function pointer. More... | |
Enumerations | |
enum | Gpt_ModeType { GPT_MODE_NORMAL = 0U, GPT_MODE_SLEEP = 1U, GPT_MODE_INVALID = 0xFFU } |
List of process modes. More... | |
enum | Gpt_PrescaleValueType { GPT_PRESCALER_CLK_DIV_BY_2 = 0x0U, GPT_PRESCALER_CLK_DIV_BY_4 = 0x1U, GPT_PRESCALER_CLK_DIV_BY_8 = 0x2U, GPT_PRESCALER_CLK_DIV_BY_16 = 0x3U, GPT_PRESCALER_CLK_DIV_BY_32 = 0x4U, GPT_PRESCALER_CLK_DIV_BY_64 = 0x5U, GPT_PRESCALER_CLK_DIV_BY_128 = 0x6U, GPT_PRESCALER_CLK_DIV_BY_256 = 0x7U, GPT_PRESCALER_NO_PRESCALE = 0xFFU } |
List of Prescale values for General purpose timer channels The timer counter is prescaled with the value 2^(PTV+1). Example: PTV = 3, counter increases value (if started) after 16 functional clock periods Note: Not applicable to GPT Predef timers. More... | |
enum | Gpt_ChannelMode { GPT_CH_MODE_CONTINUOUS = 0U, GPT_CH_MODE_ONESHOT } |
GPT channel mode macros. More... | |
enum | Gpt_ChannelStateType { GPT_UNINITIALIZED = 0U, GPT_INITIALIZED, GPT_RUNNING, GPT_STOPPED, GPT_EXPIRED } |
GPT channel state GPT will be in one of this state during its lifetime. More... | |
Macros | |
#define | GPT_CH_GPTIMER1 (0U) |
GP timer 1 instance. More... | |
#define | GPT_CH_GPTIMER2 (1U) |
GP timer 2 instance. More... | |
#define | GPT_CH_GPTIMER3 (2U) |
GP timer 3 instance. More... | |
#define | GPT_CH_GPTIMER4 (3U) |
GP timer 4 instance. More... | |
#define | GPT_CH_GPTIMER5 (4U) |
GP timer 5 instance. More... | |
#define | GPT_CH_GPTIMER6 (5U) |
GP timer 6 instance. More... | |
#define | GPT_CH_GPTIMER7 (6U) |
GP timer 7 instance. More... | |
#define | GPT_CH_GPTIMER8 (7U) |
GP timer 8 instance. More... | |
#define | GPT_CH_GPTIMER9 (8U) |
GP timer 9 instance. More... | |
#define | GPT_CH_GPTIMER10 (9U) |
GP timer 10 instance. More... | |
#define | GPT_CH_GPTIMER11 (10U) |
GP timer 11 instance. More... | |
#define | GPT_CH_GPTIMER12 (11U) |
GP timer 12 instance. More... | |
#define | GPT_CH_GPTIMER13 (12U) |
GP timer 13 instance. More... | |
#define | GPT_CH_GPTIMER14 (13U) |
GP timer 14 instance. More... | |
#define | GPT_CH_GPTIMER15 (14U) |
GP timer 15 instance. More... | |
#define | GPT_CH_GPTIMER16 (15U) |
GP timer 16 instance. More... | |
#define | GPT_CH_GPTIMER17 (16U) |
GP timer 17 instance. More... | |
#define | GPT_CH_GPTIMER18 (17U) |
GP timer 18 instance. More... | |
#define | GPT_CH_GPTIMER19 (18U) |
GP timer 19 instance. More... | |
#define | GPT_CH_GPTIMER20 (19U) |
GP timer 20 instance. More... | |
#define | GPT_CH_GPTIMER21 (20U) |
GP timer 21 instance. More... | |
#define | GPT_CH_GPTIMER22 (21U) |
GP timer 22 instance. More... | |
#define | GPT_CH_GPTIMER23 (22U) |
GP timer 23 instance. More... | |
#define | GPT_CH_GPTIMER24 (23U) |
GP timer 24 instance. More... | |
#define | GPT_CH_GPTIMER25 (24U) |
GP timer 25 instance. More... | |
#define | GPT_CH_GPTIMER26 (25U) |
GP timer 26 instance. More... | |
#define | GPT_CH_GPTIMER27 (26U) |
GP timer 27 instance. More... | |
#define | GPT_CH_GPTIMER28 (27U) |
GP timer 28 instance. More... | |
#define | GPT_CH_GPTIMER29 (28U) |
GP timer 29 instance. More... | |
#define | GPT_CH_GPTIMER30 (29U) |
GP timer 30 instance. More... | |
#define | GPT_CH_GPTIMER_MAX (30U) |
maximum GP timer channels available More... | |
#define | GPT_PRE_COMPILE_VARIANT (STD_OFF) |
GPT Pre-Compile Build Variant flag. STD_ON for VariantPreCompile / STD_OFF for VariantPostBuild. More... | |
#define | GPT_DEV_ERROR_DETECT (STD_ON) |
Enable/disable GPT dev detect error. More... | |
#define | GPT_ISR_TYPE (GPT_ISR_CAT1) |
ISR type. More... | |
#define | GPT_REPORT_WAKEUP_SOURCE (STD_ON) |
Enable/disable wakeup source in wakeup related APIs. More... | |
#define | GPT_MAX_CHANNELS (5U) |
No. of channels configured for GPT driver. More... | |
#define | GPT_PREDEF_TIMER_TYPE (GPT_PREDEF_TIMER_DISABLED) |
Macro for enabling predefined timers This is in case to disable GPT Predef Timers if timers can not be supported by hardware reasons. More... | |
#define | GPT_PREDEF_TIMER_1US_ENABLING_GRADE (GPT_PREDEF_TIMER_1US_DISABLED) |
: Specifies the grade of enabling the GPT Predef Timers with 1us tick duration More... | |
#define | GPT_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks. More... | |
#define | GPT_TIMEOUT_DURATION (32000U) |
ETH timeout. Each tick is 31.25us (for 32K Counter). Wait for 5s which comes to below value. More... | |
#define | GPT_REGISTER_READBACK_API (STD_ON) |
Enable/disable GPT register read back API. More... | |
#define | GptConf_GptChannelConfiguration_TIMER1 (11U) |
Channel ID Configured channel ID(s) More... | |
#define | GptConf_GptChannelConfiguration_MCU_TIMER6 (6U) |
#define | GptConf_GptChannelConfiguration_MCU_TIMER9 (9U) |
#define | GptConf_GptChannelConfiguration_TIMER5 (15U) |
#define | GptConf_GptChannelConfiguration_TIMER19 (29U) |
Pre-Compile Switches for API Services | |
#define | GPT_VERSION_INFO_API (STD_ON) |
Enable/disable GPT get version info API. More... | |
#define | GPT_DEINIT_API (STD_ON) |
Enable/disable GPT deinit API. More... | |
#define | GPT_TIME_ELAPSED_API (STD_ON) |
Enable/disable GPT get time elapsed API. More... | |
#define | GPT_TIME_REMAINING_API (STD_ON) |
Enable/disable GPT time remaining API. More... | |
#define | GPT_ENABLE_DISABLE_NOTIFICATION_API (STD_ON) |
Enable/disable GPT enable/disable GPT API. More... | |
#define | GPT_WAKEUP_FUNCTIONALITY_API (STD_ON) |
Enable/disable GPT wakeup functionality API. More... | |
GPT DEM Error codes to report | |
#define | DemConf_DemEventParameter_GPT_DEM_NO_EVENT (0xFFFFU) |
#define | GPT_DEM_NO_EVENT DemConf_DemEventParameter_GPT_DEM_NO_EVENT |
#define | GPT_E_HARDWARE_ERROR (DemConf_DemEventParameter_GPT_E_HARDWARE_ERROR) |
Hardware failed. More... | |
#define GPT_CH_GPTIMER1 (0U) |
GP timer 1 instance.
#define GPT_CH_GPTIMER2 (1U) |
GP timer 2 instance.
#define GPT_CH_GPTIMER3 (2U) |
GP timer 3 instance.
#define GPT_CH_GPTIMER4 (3U) |
GP timer 4 instance.
#define GPT_CH_GPTIMER5 (4U) |
GP timer 5 instance.
#define GPT_CH_GPTIMER6 (5U) |
GP timer 6 instance.
#define GPT_CH_GPTIMER7 (6U) |
GP timer 7 instance.
#define GPT_CH_GPTIMER8 (7U) |
GP timer 8 instance.
#define GPT_CH_GPTIMER9 (8U) |
GP timer 9 instance.
#define GPT_CH_GPTIMER10 (9U) |
GP timer 10 instance.
#define GPT_CH_GPTIMER11 (10U) |
GP timer 11 instance.
#define GPT_CH_GPTIMER12 (11U) |
GP timer 12 instance.
#define GPT_CH_GPTIMER13 (12U) |
GP timer 13 instance.
#define GPT_CH_GPTIMER14 (13U) |
GP timer 14 instance.
#define GPT_CH_GPTIMER15 (14U) |
GP timer 15 instance.
#define GPT_CH_GPTIMER16 (15U) |
GP timer 16 instance.
#define GPT_CH_GPTIMER17 (16U) |
GP timer 17 instance.
#define GPT_CH_GPTIMER18 (17U) |
GP timer 18 instance.
#define GPT_CH_GPTIMER19 (18U) |
GP timer 19 instance.
#define GPT_CH_GPTIMER20 (19U) |
GP timer 20 instance.
#define GPT_CH_GPTIMER21 (20U) |
GP timer 21 instance.
#define GPT_CH_GPTIMER22 (21U) |
GP timer 22 instance.
#define GPT_CH_GPTIMER23 (22U) |
GP timer 23 instance.
#define GPT_CH_GPTIMER24 (23U) |
GP timer 24 instance.
#define GPT_CH_GPTIMER25 (24U) |
GP timer 25 instance.
#define GPT_CH_GPTIMER26 (25U) |
GP timer 26 instance.
#define GPT_CH_GPTIMER27 (26U) |
GP timer 27 instance.
#define GPT_CH_GPTIMER28 (27U) |
GP timer 28 instance.
#define GPT_CH_GPTIMER29 (28U) |
GP timer 29 instance.
#define GPT_CH_GPTIMER30 (29U) |
GP timer 30 instance.
#define GPT_CH_GPTIMER_MAX (30U) |
maximum GP timer channels available
#define GPT_PRE_COMPILE_VARIANT (STD_OFF) |
GPT Pre-Compile Build Variant flag. STD_ON for VariantPreCompile / STD_OFF for VariantPostBuild.
#define GPT_DEV_ERROR_DETECT (STD_ON) |
Enable/disable GPT dev detect error.
#define GPT_ISR_TYPE (GPT_ISR_CAT1) |
ISR type.
#define GPT_REPORT_WAKEUP_SOURCE (STD_ON) |
Enable/disable wakeup source in wakeup related APIs.
#define GPT_VERSION_INFO_API (STD_ON) |
Enable/disable GPT get version info API.
#define GPT_DEINIT_API (STD_ON) |
Enable/disable GPT deinit API.
#define GPT_TIME_ELAPSED_API (STD_ON) |
Enable/disable GPT get time elapsed API.
#define GPT_TIME_REMAINING_API (STD_ON) |
Enable/disable GPT time remaining API.
#define GPT_ENABLE_DISABLE_NOTIFICATION_API (STD_ON) |
Enable/disable GPT enable/disable GPT API.
#define GPT_WAKEUP_FUNCTIONALITY_API (STD_ON) |
Enable/disable GPT wakeup functionality API.
#define GPT_MAX_CHANNELS (5U) |
No. of channels configured for GPT driver.
#define GPT_PREDEF_TIMER_TYPE (GPT_PREDEF_TIMER_DISABLED) |
Macro for enabling predefined timers This is in case to disable GPT Predef Timers if timers can not be supported by hardware reasons.
#define GPT_PREDEF_TIMER_1US_ENABLING_GRADE (GPT_PREDEF_TIMER_1US_DISABLED) |
: Specifies the grade of enabling the GPT Predef Timers with 1us tick duration
#define GPT_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks.
#define GPT_TIMEOUT_DURATION (32000U) |
ETH timeout. Each tick is 31.25us (for 32K Counter). Wait for 5s which comes to below value.
#define DemConf_DemEventParameter_GPT_DEM_NO_EVENT (0xFFFFU) |
#define GPT_DEM_NO_EVENT DemConf_DemEventParameter_GPT_DEM_NO_EVENT |
#define GPT_E_HARDWARE_ERROR (DemConf_DemEventParameter_GPT_E_HARDWARE_ERROR) |
Hardware failed.
#define GPT_REGISTER_READBACK_API (STD_ON) |
Enable/disable GPT register read back API.
#define GptConf_GptChannelConfiguration_TIMER1 (11U) |
Channel ID Configured channel ID(s)
Channel identifiers
#define GptConf_GptChannelConfiguration_MCU_TIMER6 (6U) |
Channel identifiers
#define GptConf_GptChannelConfiguration_MCU_TIMER9 (9U) |
Channel identifiers
#define GptConf_GptChannelConfiguration_TIMER5 (15U) |
Channel identifiers
#define GptConf_GptChannelConfiguration_TIMER19 (29U) |
Channel identifiers
typedef uint32 Gpt_ChannelType |
Type describing the Gpt channel.
typedef uint32 Gpt_ValueType |
Type describing the timeout value.
typedef void(* Gpt_NotifyType) (void) |
Notification callback function pointer.
enum Gpt_ModeType |
List of Prescale values for General purpose timer channels The timer counter is prescaled with the value 2^(PTV+1). Example: PTV = 3, counter increases value (if started) after 16 functional clock periods Note: Not applicable to GPT Predef timers.
enum Gpt_ChannelMode |
enum Gpt_ChannelStateType |
void Gpt_Ch12Isr | ( | void | ) |
GPT Channel ISR.
Channel ISR
void Gpt_Ch7Isr | ( | void | ) |
Channel ISR
void Gpt_Ch10Isr | ( | void | ) |
Channel ISR
void Gpt_Ch16Isr | ( | void | ) |
Channel ISR
void Gpt_Ch30Isr | ( | void | ) |
Channel ISR
const struct Gpt_ConfigType_s GptChannelConfigSet |
GPT Configuration.
const uint32 Gpt_TimerBaseAddr[GPT_CH_GPTIMER_MAX] |
Base Address of the timer peripherals.