MCUSW
|
This file contains interface header for DIO MCAL driver to be used by other AUTOSAR MCAL Layers.
Go to the source code of this file.
Data Structures | |
struct | Dio_ChannelGroupType |
Type definition for identifying channel groups (meaning a set of pins in one port) More... | |
struct | Dio_RegisterReadbackType |
Macros | |
#define | DIO_PORT_WIDTH (32U) |
Width of GPIO register in this platform not to be modified. More... | |
#define | DIO_MCAL_2139_FIXED (0U) |
Read back issue in Maxwell is resolved or not. More... | |
DIO Driver Module SW Version Info | |
Defines for DIO Driver version used for compatibility checks | |
#define | DIO_SW_MAJOR_VERSION (3U) |
Driver Implementation Major Version. More... | |
#define | DIO_SW_MINOR_VERSION (0U) |
Driver Implementation Minor Version. More... | |
#define | DIO_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version. More... | |
DIO Driver Module AUTOSAR Version Info | |
Defines for DIO Driver AUTOSAR version used for compatibility checks | |
#define | DIO_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by DIO Driver. More... | |
#define | DIO_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by DIO Driver. More... | |
#define | DIO_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by DIO Driver. More... | |
DIO Driver ID Info | |
#define | DIO_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID. More... | |
#define | DIO_MODULE_ID ((uint16) 120U) |
DIO Driver Module ID. More... | |
Dio Error Codes | |
Error codes returned by Driver functions | |
#define | DIO_E_PARAM_INVALID_CHANNEL_ID (0x0AU) |
ERROR:API service called with invalid channel ID. More... | |
#define | DIO_E_PARAM_INVALID_PORT_ID (0x14U) |
ERROR:API service called with invalid port ID. More... | |
#define | DIO_E_PARAM_INVALID_GROUP (0x1FU) |
ERROR:API service called with invalid channel group ID. More... | |
#define | DIO_E_PARAM_POINTER (0x20U) |
ERROR:Dio_GetVersionInfo() called with NULL_PTR as parameter. More... | |
Dio Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
#define | DIO_SID_READ_CHANNEL (0U) |
Dio_ReadChannel() More... | |
#define | DIO_SID_WRITE_CHANNEL (1U) |
Dio_WriteChannel() More... | |
#define | DIO_SID_READ_PORT (2U) |
Dio_ReadPort() More... | |
#define | DIO_SID_WRITE_PORT (3U) |
Dio_WritePort() More... | |
#define | DIO_SID_READ_CHL_GROUP (4U) |
Dio_ReadChannelGroup() More... | |
#define | DIO_SID_WRITE_CHL_GROUP (5U) |
Dio_WriteChannelGroup() More... | |
#define | DIO_SID_FLIP_CHANNEL (7U) |
Dio_FlipChannel() More... | |
#define | DIO_SID_GET_VERSION_INFO (18U) |
Dio_GetVersionInfo() More... | |
Typedefs | |
typedef uint32 | Dio_ChannelType |
type definition for identifying DIO channels (meaning single port pins) More... | |
typedef uint32 | Dio_PortType |
type definition for identifying ports More... | |
typedef uint32 | Dio_PortLevelType |
type definition for setting port level values More... | |
typedef uint8 | Dio_LevelType |
type definition for setting DIO channnel level values (allowed values: STD_HIGH and STD_LOW) More... | |
Enumerations | |
enum | Dio_DirectionType { DIO_DIR_INPUT = 0x1U, DIO_DIR_OUTPUT = 0x0U } |
Functions | |
Dio_LevelType | Dio_ReadChannel (Dio_ChannelType ChannelId) |
Returns the value of the specified DIO channel. More... | |
void | Dio_WriteChannel (Dio_ChannelType ChannelId, Dio_LevelType Level) |
Service to set a level of a channel. More... | |
Dio_PortLevelType | Dio_ReadPort (Dio_PortType PortId) |
Returns the level of all channels of that port. More... | |
void | Dio_WritePort (Dio_PortType PortId, Dio_PortLevelType Level) |
Service to set a value of the port. More... | |
Dio_PortLevelType | Dio_ReadChannelGroup (const Dio_ChannelGroupType *ChannelGroupIdPtr) |
This Service reads a subset of the adjoining bits of a port. More... | |
void | Dio_WriteChannelGroup (const Dio_ChannelGroupType *ChannelGroupIdPtr, Dio_PortLevelType Level) |
Service to set a subset of the adjoining bits of a port to a specified level. More... | |
void | Dio_GetVersionInfo (Std_VersionInfoType *versioninfo) |
Service to get the version information of this module. More... | |
Dio_LevelType | Dio_FlipChannel (Dio_ChannelType ChannelId) |
Service to flip (change from 1 to 0 or from 0 to 1) the level of a channel and return the level of the channel. More... | |
Std_ReturnType | Dio_RegisterReadback (Dio_ChannelType ChannelId, Dio_RegisterReadbackType *DioRegRbPtr) |
This function reads the important registers of the hardware unit and returns the value in the structure. More... | |
Dio_LevelType Dio_ReadChannel | ( | Dio_ChannelType | ChannelId | ) |
Returns the value of the specified DIO channel.
* Service name : Dio_ReadChannel * Syntax : Dio_LevelType Dio_ReadChannel( * Dio_ChannelType ChannelId ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : ChannelId * ID of DIO channel * Parameters (inout): None * Parameters (out) : None * Return value : Dio_LevelType - STD_HIGH The physical level of the * corresponding Pin is STD_HIGH * - STD_LOW The physical level of the corresponding Pin * is STD_LOW * Description : Returns the value of the specified DIO channel. *
void Dio_WriteChannel | ( | Dio_ChannelType | ChannelId, |
Dio_LevelType | Level | ||
) |
Service to set a level of a channel.
* Service name : Dio_WriteChannel * Syntax : void Dio_WriteChannel( Dio_ChannelType ChannelId, * Dio_LevelType Level ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : ChannelId - ID of DIO channel * Level - Value to be written * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : Service to set a level of a channel. *
Dio_PortLevelType Dio_ReadPort | ( | Dio_PortType | PortId | ) |
Returns the level of all channels of that port.
* Service name : Dio_ReadPort * Syntax : Dio_PortLevelType Dio_ReadPort( Dio_PortType PortId ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x02 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : PortId - ID of DIO Port * Parameters (inout): None * Parameters (out) : None * Return value : Dio_PortLevelType - Level of all channels of that port * Description : Returns the level of all channels of that port. *
void Dio_WritePort | ( | Dio_PortType | PortId, |
Dio_PortLevelType | Level | ||
) |
Service to set a value of the port.
* Service name : Dio_WritePort * Syntax : void Dio_WritePort( Dio_PortType PortId, * Dio_PortLevelType Level ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x03 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : PortId - ID of DIO Port * Level - Value to be written * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : Service to set a value of the port. *
Dio_PortLevelType Dio_ReadChannelGroup | ( | const Dio_ChannelGroupType * | ChannelGroupIdPtr | ) |
This Service reads a subset of the adjoining bits of a port.
* Service name : Dio_ReadChannelGroup * Syntax : Dio_PortLevelType Dio_ReadChannelGroup( * const Dio_ChannelGroupType* ChannelGroupIdPtr ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : ChannelGroupIdPtr - Pointer to ChannelGroup * Parameters (inout): None * Parameters (out) : None * Return value : Dio_PortLevelType - Level of a subset of the adjoining * bits of a port * Description : This Service read a subset of the adjoining bits of a * port. *
void Dio_WriteChannelGroup | ( | const Dio_ChannelGroupType * | ChannelGroupIdPtr, |
Dio_PortLevelType | Level | ||
) |
Service to set a subset of the adjoining bits of a port to a specified level.
* Service name : Dio_WriteChannelGroup * Syntax : void Dio_WriteChannelGroup( const Dio_ChannelGroupType* * ChannelGroupIdPtr, Dio_PortLevelType Level ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : ChannelGroupIdPtr - Pointer to ChannelGroup * Level - Value to be written * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : Service to set a subset of the adjoining bits of a port * to a specified level *
void Dio_GetVersionInfo | ( | Std_VersionInfoType * | versioninfo | ) |
Service to get the version information of this module.
* Service name : Dio_GetVersionInfo * Syntax : void Dio_GetVersionInfo( * Std_VersionInfoType* versioninfo ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x12 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : versioninfo - Pointer to where to store the version * information of this module. * Return value : None * Description : Service to get the version information of this module *
Dio_LevelType Dio_FlipChannel | ( | Dio_ChannelType | ChannelId | ) |
Service to flip (change from 1 to 0 or from 0 to 1) the level of a channel and return the level of the channel.
* Service name : Dio_FlipChannel * Syntax : Dio_LevelType Dio_FlipChannel( * Dio_ChannelType ChannelId ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x11 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : ChannelId * - ID of DIO channel * Parameters (inout): None * Parameters (out) : None * Return value : Dio_LevelType * Return value : Dio_LevelType - STD_HIGH The physical level of the * corresponding Pin is STD_HIGH * - STD_LOW The physical level of the corresponding Pin is * STD_LOW * Description : Service to flip (change from 1 to 0 or from 0 to 1) the * level of a channel and return the level of the channel * after flip *
Std_ReturnType Dio_RegisterReadback | ( | Dio_ChannelType | ChannelId, |
Dio_RegisterReadbackType * | DioRegRbPtr | ||
) |
This function reads the important registers of the hardware unit and returns the value in the structure.
* This API should be called after DIO initialization in the app. * * This API could be used to readback the register contents * and then the readback value could be compared during DIO execution to * check the correctness of the HW unit. Since this API is used for this * purpose, the register returned are the ones which doesn't * change during execution. * * \verbatim * Service name : Dio_RegisterReadback * Syntax : uint32 Dio_RegisterReadback( * Dio_ChannelType ChannelId ) * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : ChannelId * - ID of DIO channel * Parameters (inout) : None * Parameters (out) : Value of the PID register * Return value : uint32 *