Ethernet Firmware
User Guide

Ethernet Firmware enables multiple client drivers to run independently on the remaining cores in the system. For instance, A-cores can run HLOS like Linux or QNX, and other R5F cores can run FreeRTOS or AUTOSAR software. Client drivers communicate through the central Ethernet Firmware module for any necessary switch configuration. Once setup packet are directly steered to the designated cores based on the flow steered criteria described before.

This user guide presents the list of features supported by the Ethernet Firmware (EthFw), and describes the steps required to build and run the EthFw demo applications.


Supported Features

Feature Comments
L2 switching Support for configuration of the Ethernet Switch to enable L2 switching between external ports with VLAN, multi-cast
Inter-VLAN routing Inter-VLAN routing configuration in hardware with software fall-back support
lwIP integration Integration of TCP/IP stack enabling TCP, UDP.
MAC-only Port configuration in MAC-only mode for traffic exclusively forwarded to host port, excludes the designated port(s) from switching logic
Intercore Virtual Ethernet Shared memory-based virtual Ethernet adapter communication between cores
Multi-core broadcast an multicast support Multi-core concurrent reception of broadcast and multicast traffic using SW based fan-out
Ability to send broadcast and multicast traffic to multiple cores
Remote configuration server Firmware app hosting the IPC server to serve remote clients like Linux Virtual MAC driver
Resource management library Resource management library for CPSW resource sharing across cores

Back To Top


Master Core (EthFw)

The multiport CPSW switch present in devices of the Jacinto family is an Ethernet peripheral shared among the different processing cores within the SoC. Ethernet Firmware acts as the owner of the CPSW switch and provides a remote configuration infrastructure for other processing cores running different operating systems.

Ethernet Firmware enables TCP/IP stack and PTP test stack, includes software and hardware interVLAN demos, as well as helper utils libraries (i.e. network statistics).

The following diagram shows the main components of the Ethernet Firmware software architecture.

switch_software_stack.png
Ethernet Firmware software architecture

The TCP/IP stack integrated in the Ethernet Firmware is based on the open source lwIP stack enabled on top of Enet LLD.

Ethernet Firmware sets up packet classifiers to route traffic to the different remote processing cores. Routing criterias are based on the switch ingress port number or Layer-2 destination MAC address, depending on the virtual port type requested by the remote cores. Packets which don't match any of the configured classifier criteria are routed to a default UDMA flow that is owned by Ethernet Firmware.

For multicast, if the traffic is exclusively requested by a single core it can be directly steered to the designated core by programming the hardware classifier module through EthFw. When multiple cores need to receive the same multicast flow, then it is always steered to the Ethernet Firmware which plays the role of central hub that replicates and fans out. Refer to the Multicast and Broadcast Support section for more information.

Ethernet Firmware operates as a PTP clock slave and supports two-step mode with Layer-2 encapsulation. The integrated PTP stack is a TI implementation meant for testing and demonstration purposes. It must not be used for production. This PTP implementation sets up CPSW ALE classifiers with PTP multicast MAC addresses as match criteria to have PTP traffic routed to a dedicated UDMA RX flow.

The remote configuration infrastructure provided by Ethernet Firmware is built on top of the remote_device framework. Ethernet Firmware plays the role of a server which accepts and processes commands from the remote clients and carry out operations such as attaching/detaching, registering a MAC address or IP, etc, on the client's behalf.

CPSW register configuration is carried out exclusively by Ethernet Firmware, remote cores are not expected/allowed to perform any CPSW5G/CPSW9G register access, though that is not enforced at the time of this writing. Ethernet Firmware uses Enet LLD for low-level CPSW5G/CPSW9G driver support and for Ethernet PHY configuration. Enet LLD internally uses UDMA LLD for packet exchange with the CPSW switch.

The following diagram shows a view of the Ethernet Firmware components and the expected ownership.

building_block_owners.png
Component ownership in EthFw

Back To Top


Remote Core Clients


RTOS Client

Ethernet Firmware component in SDK provides a FreeRTOS client example application running on Main R5F 0 core 1. This application showcases lwIP TCP/IP stack and multicore time synchronization built on top of Ethernet Firmware's IPC-based remote config infrastructure.

rtos_client.png
EthFw with RTOS client

The following lwIP netifs are enabled in the RTOS client application:

  • CPSW client drivers:
    • Virtual MAC port based netif - Dedicated MAC port from CPSW is excluded from regular packet switching and allocated exclusive for this R5F core.
    • Virtual switch port based netif - Virtual port which carries unicast RX traffic from hardware MAC ports and TX traffic to hardware MAC ports.
  • Shared memory virtual driver:
    • Intercore based netif - Used for broadcast/multicast packet exchange with R5F core running Ethernet Firmware. Refer to the Inter-core Virtual Ethernet section for more details about intercore Ethernet.

The two CPSW virtual port netifs reuse the same Enet LLD based lwIP implementation.

The RTOS core attaches to the Ethernet Firmware server using the Eth Remote Config Client library which is built on top of remote_device framework.

The multicore time synchronization mechanism implemented in RTOS client consists of a linear correction in software of a local timer owned by the RTOS core which is periodically synchronized with the CPTS clock via HW push event 2.

Porting RTOS client to Main R5F 1 Core 0

Ethernet Firmware provides RTOS client support only on Main R5F 0 core 1 (mcu2_1) in all supported SoCs. Consequently, it's recommended to use mcu2_1 processing core if virtual network interface support is required on an RTOS core.

However, in SoCs with multiple R5F cores, like J721E, system design may require virtual network support on a different R5F core, instead of Main R5F 0 Core 1. This requires porting effort on top of Enet LLD and Ethernet Firmware provided in standard TI SDK. The scope of the required porting changes will be discussed next, in the context of Main R5F 1 core 0 (mcu3_0) in J721E.

  • Enet LLD:
    • Add mcu3_0 core in driver's CORELIST. This will be enable core Enet LLD support on Main R5F 1 core 0.
    • Replace mcu2_1 with mcu3_0 in intercore and lwipific libraries. Mainly renaming MCU2_1 macros to MCU3_0, but more importantly, updating the IPC core id (IPC_MCU2_1 -> IPC_MCU3_0).
  • Ethernet Firmware (server application):
    • Replace IPC core id of the RTOS client (IPC_MCU2_1 -> IPC_MCU3_0) in EthFw library, CpswProxy server and client, as well as EthFw server application.
    • Update the IPC core id where virtual switch port and virtual MAC port interfaces are enabled on.
    • Update memory addresses used for MCU3_0 IPC (0xA3000000 -> 0xA4000000).
  • RTOS client application:
    • Update IPC multiproc configuration to exclude mcu3_0 and include mcu2_1.
    • Update memory addresses used for MCU3_0 IPC (0xA3000000 -> 0xA4000000).
    • Rename Enet LLD intercore macros as per corresponding changes in Enet LLD for mcu3_0 support.

It's worth noting that above list summarizes the software changes needed for running RTOS client on mcu3_0 instead of mcu2_1. It must not be confused with adding mcu3_0 support in addition to mcu2_1, which is not in the scope of this discussion.

The following Enet LLD and Ethernet Firmware patches are provided as reference to illustrate the actual software changes corresponding to the summary shown earlier. These changes are meant as reference for prototyping, and are provided as is.


Linux Client

TI Linux kernel provides support for the two types of CPSW client drivers, virtual MAC port and virtual switch port, through the j721e-cpsw-virt-mac driver. Both interfaces types are enabled by default in TI Processor SDK Linux.

The following diagram presents a simplified view of the main components involved in the Linux client usecase.

linux_client.png
EthFw with Linux client

The rpmsg_kdrv_switch client driver is compatible with the remote_device server side running on RTOS master core (Ethernet Firmware). This driver is used to exchange control messages with Ethernet Firmware to establish a virtual port connection.

It's important to note that the Ethernet packet exchange doesn't happen via IPC. Instead, it happens completely in hardware via UDMA TX channel and RX flow.

For further information, please refer to CPSWng_virt_mac documentation in Processor SDK Linux.


QNX Client

TI's baseport for QNX provides support for virtual switch port network interface through its devnp_cpsw9g driver. Virtual MAC port (MAC-only mode) is currently not supported by QNX client.

The following diagram shows a simplified view of the main components involved in the QNX client's virtual port implementation.

qnx_client.png
EthFw with QNX client

TI's devnp_cpsw9g driver implements the driver interface of the QNX networking stack (io-pkt), so the virtual MAC port network interface is exposed transparently to the user as any other native networking interface.

devnp_cpsw9g driver uses Ethernet Firmware's remote configuration infrastructure in order to attach/detach the virtual port, register its MAC address, IP address, etc. This is the same remote configuration API used by other remote clients such as RTOS core, and consequently also sits on top of the remote_device framework. The lower level IPC functionality is provided by the IPC RM (QNX resmgr).

Ethernet packet exchange with the CPSW switch happens in hardware through an UDMA TX channel and RX flow, completely independent of the Ethernet Firmware. devnp_cpsw9g driver uses Enet LLD data path APIs natively to submit and retrieve Ethernet packets.


AUTOSAR Client

Ethernet Firmware is also able to attach to a remote client running AUTOSAR. The AUTOSAR client must use TI's MCAL Eth VirtMAC driver. This is a MCAL Eth driver with TI customizations for virtual MAC functionality.

A simplified view of the main entities involved in the AUTOSAR remote client usecase are shown in the following diagram.

autosar_client.png
EthFw with AUTOSAR client

The remote core configuration is implemented on top of TI MCAL IPC CDD. The remote_core framework used for RTOS and Linux clients is not relevant in the AUTOSAR scenario.

Ethernet packet exchange with the CPSW switch doesn't happen via IPC, but in hardware via UDMA TX channel and RX flow.

In the current release, AUTOSAR client only supports virtual switch port. Virtual MAC port (MAC-only mode) is not supported.

Note that the AUTOSAR client in the SDK has enabled only on Main R5F 0 core 1.


Component Location

The location within the SDK directory structure of the software components which are relevant for Ethernet Firmware usecases is shown in the following figure. Note that this figure presents a consolidated view of the Ethernet Firmware and all the supported remote clients, but that doesn't mean that all clients can be supported simultaneously.

EthFw_component_location.png
Location of the Ethernet Firmware related components in SDK

Back To Top


MAC-only

CPSW switch supports a feature called MAC-only mode which allows all incoming traffic from a given MAC port to be transferred only to the host port. This effectively excludes the MAC ports configured in this mode for rest of packet switching happening in the CPSW switch.

Starting with SDK 8.1, Ethernet Firmware has enabled MAC-only mode on selected MAC ports. To better understand the physical and logical entities involved in a system where MAC-only mode has been enabled, let's start by defining key concepts:

  • Hardware physical ports - The CPSW switch MAC ports.
  • Logical switch ports - Defined based on packet header match criteria, typically created based on destination MAC address, VLAN IDs, etc. Two possible types:
  • Logical MAC-only ports - Defined with 1-to-1 correspondence to physical ports (port configured in MAC-only mode), owned by remote clients.
EthFw_PortCfg_generic.png
Ethernet Firmware logical ports and hardware ports

The default port configuration for J721E and J7200 are shown in J721E Port Configuration J7200 Port Configuration and J784S4 Port Configuration subsections, respectively.

The port's default VLAN for MAC ports configured in MAC-only mode is 0, and for MAC ports configured in switch mode is 1. They can be changed via EthFw_Config::dfltVlanIdMacOnlyPorts and EthFw_Config::dfltVlanIdSwitchPorts, respectively.

Hardware physical ports

These are the actual hardware MAC ports of the CPSW switch. They can be configured in MAC-only or switch (non MAC-only) mode.

The MAC ports which are to be enabled by the Ethernet Firmware as passed as a parameter of EthFw_Config structure. For example, below code snippet shows a configuration which enables all 8 MAC ports in J721E CPSW9G.

static Enet_MacPort gEthAppPorts[] =
{
ENET_MAC_PORT_1, /* RGMII */
ENET_MAC_PORT_3, /* RGMII */
ENET_MAC_PORT_4, /* RGMII */
ENET_MAC_PORT_8, /* RGMII */
#if defined(ENABLE_QSGMII_PORTS)
ENET_MAC_PORT_2, /* QSGMII main */
ENET_MAC_PORT_5, /* QSGMII sub */
ENET_MAC_PORT_6, /* QSGMII sub */
ENET_MAC_PORT_7, /* QSGMII sub */
#endif
};
static int32_t EthApp_initEthFw(void)
{
EthFw_Config ethFwCfg;
...
ethFwCfg.ports = &gEthAppPorts[0];
ethFwCfg.numPorts = ARRAY_SIZE(gEthAppPorts);
...
}

Local switch port

This is a logical port owned by the Ethernet Firmware.

Ethernet packets are exchanged with the CPSW switch through its host port using a UDMA RX flow and a TX channel.

CPSW's default thread is set to this port's UDMA RX flow, also called default RX flow. Traffic which is not matched by any CPSW classifier gets routed to this port.

Virtual switch port

This is the traditional logical port owned by remote client cores, controlled via Ethernet Firmware's IPC-based remote API.

Ethernet packets are also exchanged with the CPSW switch through its host port using a UDMA RX flow and a TX channel.

RX traffic (to remote core) is segregated via CPSW ALE classifier with unicast MAC address match criteria. TX traffic (from remote core) is sent as non-directed packets.

It's worth noting that virtual switch ports are not directly associated with any specific hardware MAC port, as these virtual ports can received traffic from any MAC port as long as the packets match the unicast MAC address classification criteria.

SDK 8.0 or older supported only this type of virtual port.

Virtual port (virtual switch or virtual MAC) are allocated to a specific core. For example, below code snippet shows a configuration where virtual switch 0 is allocated for A72 core, and virtual switch port 1 is allocated for Main R5F 0 Core 1.

static EthFw_VirtPortCfg gEthApp_virtPortCfg[] =
{
{
.remoteCoreId = IPC_MPU1_0,
.portId = ETHREMOTECFG_SWITCH_PORT_0,
},
{
.remoteCoreId = IPC_MCU2_1,
.portId = ETHREMOTECFG_SWITCH_PORT_1,
},
{
.remoteCoreId = IPC_MPU1_0,
.portId = ETHREMOTECFG_MAC_PORT_1,
},
{
.remoteCoreId = IPC_MCU2_1,
.portId = ETHREMOTECFG_MAC_PORT_4,
},
};
static EthFw_VirtPortCfg gEthApp_autosarVirtPortCfg[] =
{
{
.remoteCoreId = IPC_MCU2_1,
.portId = ETHREMOTECFG_SWITCH_PORT_1,
},
};
static int32_t EthApp_initEthFw(void)
{
EthFw_Config ethFwCfg;
...
/* Set virtual port configuration parameters */
ethFwCfg.virtPortCfg = &gEthApp_virtPortCfg[0];
ethFwCfg.numVirtPorts = ARRAY_SIZE(gEthApp_virtPortCfg);
/* Set AUTOSAR virtual port configuration parameters */
ethFwCfg.autosarVirtPortCfg = &gEthApp_autosarVirtPortCfg[0];
ethFwCfg.numAutosarVirtPorts = ARRAY_SIZE(gEthApp_autosarVirtPortCfg);
...
}

Virtual MAC port

This is also a logical port owned by remote clients and controlled via Ethernet Firmware's IPC-based remote API.

Ethernet packets are also exchanged with the CPSW switch through its host port using a UDMA RX flow and a TX channel.

RX traffic (to remote core) is segregated via CPSW ALE classifier with port match criteria. TX traffic (from remote core) is sent as directed packets.

These virtual ports are directly associated with a hardware MAC port which is configured in MAC-only mode.

Below code snippet (which is same as shown in previous section for Virtual switch port) shows a configuration where virtual MAC port 1 is allocated for A72, and virtual MAC port 2 is allocated for Main R5F 0 Core 1. It's worth noting that virtual MAC ports are only supported in Linux and RTOS client, hence no virtual MAC ports are allocated for AUTOSAR client.

static EthFw_VirtPortCfg gEthApp_virtPortCfg[] =
{
{
.remoteCoreId = IPC_MPU1_0,
.portId = ETHREMOTECFG_SWITCH_PORT_0,
},
{
.remoteCoreId = IPC_MCU2_1,
.portId = ETHREMOTECFG_SWITCH_PORT_1,
},
{
.remoteCoreId = IPC_MPU1_0,
.portId = ETHREMOTECFG_MAC_PORT_1,
},
{
.remoteCoreId = IPC_MCU2_1,
.portId = ETHREMOTECFG_MAC_PORT_4,
},
};
static EthFw_VirtPortCfg gEthApp_autosarVirtPortCfg[] =
{
{
.remoteCoreId = IPC_MCU2_1,
.portId = ETHREMOTECFG_SWITCH_PORT_1,
},
};
static int32_t EthApp_initEthFw(void)
{
EthFw_Config ethFwCfg;
...
/* Set virtual port configuration parameters */
ethFwCfg.virtPortCfg = &gEthApp_virtPortCfg[0];
ethFwCfg.numVirtPorts = ARRAY_SIZE(gEthApp_virtPortCfg);
/* Set AUTOSAR virtual port configuration parameters */
ethFwCfg.autosarVirtPortCfg = &gEthApp_autosarVirtPortCfg[0];
ethFwCfg.numAutosarVirtPorts = ARRAY_SIZE(gEthApp_autosarVirtPortCfg);
...
}

Configuring additional ports in MAC-only mode

The default port configuration of Ethernet Firmware can be changed to fit the specific architecture requirements of each system.

If additional ports need to be configured in MAC-only mode, one needs to follow these steps:

  1. Add the new MAC port to the port array passed via EthFw_Config::port config parameter.
  2. Add a new virtual MAC port corresponding to the hardware MAC port of interest. The virtual port configuration is passed via EthFw_Config::virtPortCfg config parameter. The virtual port mode must be set to ETHREMOTECFG_MAC_PORT_<n> which is an enum of type EthRemoteCfg_VirtPort.
static Enet_MacPort gEthAppPorts[] =
{
...
ENET_MAC_PORT_5, /* new MAC port being added */
};
static EthFw_VirtPortCfg gEthApp_virtPortCfg[] =
{
...
{
.remoteCoreId = IPC_MCU2_1, /* new MAC port allocated for MCU2_1 RTOS usage */
.portId = ETHREMOTECFG_MAC_PORT_5, /* new MAC port in MAC-only mode */
},
};
static int32_t EthApp_initEthFw(void)
{
EthFw_Config ethFwCfg;
...
ethFwCfg.ports = &gEthAppPorts[0];
ethFwCfg.numPorts = ARRAY_SIZE(gEthAppPorts);
ethFwCfg.virtPortCfg = &gEthApp_virtPortCfg[0];
ethFwCfg.numVirtPorts = ARRAY_SIZE(gEthApp_virtPortCfg);
...
}

On the other hand, if the new MAC port or an existing one needs to be changed from MAC-only mode to switch mode, one can simply remove it from the EthFw_VirtPortCfg array.

Resource availability and allocation must be taken into account when adding additional virtual ports, not only in MAC-only mode but also in switch mode. Each virtual port will require one UDMA TX channel and one UDMA RX flow, both are resources partitioned for each core in the SoC, hence repartitioning might be needed. Additionally, each virtual port will require a MAC address which is also a limited resource.

Ethernet Firmware relies on Enet LLD's utils library to populate its MAC address pool (see EnetAppUtils_initResourceConfig()). The MAC address pool is populated with addresses read from EEPROMs located in the different expansion boards in TI EVM. Note that a static MAC address pool is used as a workaround in TI EVMs for cases where I2C bus contention could happen (i.e. when integrating with Linux). It's expected that the MAC address pool population mechanism is adapted when integrating Ethernet Firmware to different platforms.

The utilization of these resources by Ethernet Firmware on Main R5F 0 Core 0 is as follows:

Resource Count EthFw Usage (mcu2_0)
TX channel 3
  • lwIP netif (1)
  • PTP (1)
  • SW interVLAN (1)
RX flow 5
  • lwIP netif (1)
  • Proxy ARP (1)
  • PTP (1)
  • SW interVLAN (1)
  • Enet LLD default flow (1)
MAC address 1
  • lwIP netif (1)

UDMA TX channels are a resource especially limited as there is only a total of 8 TX channels available. So, there are 5 TX channels to be shared among the differrent remote client cores and their virtual ports.

With Ethernet Firmware's default port configuration, the following resources will be used by Linux remote client on A72 core.

Resource Count Linux Client Usage
TX channel 2
  • Virtual switch port (1)
  • Virtual MAC port (1)
RX flow 2
  • Virtual switch port (1)
  • Virtual MAC port (1)
MAC address 2
  • Virtual switch port (1)
  • Virtual MAC port (1)

With Ethernet Firmware's default port configuration, the following resources will be used by RTOS remote client on Main R5F 0 Core 1.

Resource Count RTOS Client Usage
TX channel 2
  • Virtual switch lwIP netif (1)
  • Virtual MAC port lwIP netif (1)
RX flow 2
  • Virtual switch lwIP netif (1)
  • Virtual MAC port lwIP netif (1)
MAC address 2
  • Virtual switch lwIP netif (1)
  • Virtual MAC port lwIP netif (1)

Back To Top

Default Port Configuration

J721E Port Configuration

There are four MAC ports enabled by default in Ethernet Firmware for J721E SoC. These are the RGMII MAC ports in GESI board.

Two MAC ports are configured in MAC-only mode and allocated for A72 (Linux) and Main R5F Core 1 (RTOS) usage. The remaining two MAC ports are configured in switch mode.

EthFw_PortCfg_j721e_evm.png
J721E default port configuration

The following table shows the full list of MAC ports in J721E EVM, the board they are located and their MAC mode.

MAC Port PHY Addr Board MAC mode
MAC Port 1 12 GESI MAC-only
MAC Port 2 16 QSGMII Switch Port
MAC Port 3 0 GESI Switch Port
MAC Port 4 3 GESI MAC-only
MAC Port 5 17 QSGMII Switch Port
MAC Port 6 18 QSGMII Switch Port
MAC Port 7 19 QSGMII Switch Port
MAC Port 8 15 GESI Switch Port

Note: All MAC ports are configured as switch ports in QNX build (i.e. BUILD_QNX_A72=yes) because QNX virtual MAC driver does not support MAC-only mode.

J7200 Port Configuration

All the four MAC ports of CPSW5G are enabled by default in Ethernet Firmware for J7200 SoC. These are the four QSGMII MAC ports in QSGMII (QpENet) expansion board.

Two MAC ports are configured in MAC-only mode and allocated for A72 (Linux) and Main R5F Core 1 (RTOS) usage. The remaining two MAC ports are configured in switch mode.

EthFw_PortCfg_j7200_evm.png
J7200 default port configuration

The following table shows the full list of MAC ports in J7200 EVM, the board they are located and their MAC mode.

MAC Port PHY Addr Board MAC mode
MAC Port 1 16 QSGMII MAC-only
MAC Port 2 17 QSGMII Switch Port
MAC Port 3 18 QSGMII Switch Port
MAC Port 4 19 QSGMII MAC-only

Note: All MAC ports are configured as switch ports in QNX build (i.e. BUILD_QNX_A72=yes) because QNX virtual MAC driver does not support MAC-only mode.

Back To Top

J784S4 Port Configuration

J784S4 EVM provides two Enet expansion connectors (ENET-EXP-1 and ENET-EXP-2) where two expansion boards can be connected. QSGMII (QpENet) board can be connected to either expansion connector, but two QSGMII boards cannot be connected simultaneously due to board limitation.

Only four MAC ports of CPSW9G are enabled by default in Ethernet Firmware for J784S4 SoC. These are the four QSGMII MAC ports in QSGMII (QpENet) expansion board when connected in slot 1 (ENET-EXP-1).

Two MAC ports are configured in MAC-only mode and allocated for A72 (Linux) and Main R5F Core 1 (RTOS) usage. The remaining two MAC ports are configured in switch mode.

EthFw_PortCfg_j784s4_evm.png
J784S4 default port configuration

The following table shows the full list of MAC ports in J784S4 EVM, the board they are located and their MAC mode.

MAC Port PHY Addr Board MAC mode
MAC Port 1 16 QSGMII MAC-only
MAC Port 3 17 QSGMII Switch Port
MAC Port 4 18 QSGMII MAC-only
MAC Port 5 19 QSGMII Switch Port

MAC ports 2, 6, 7 and 8 are not enabled.

Note: All enabled MAC ports are configured as switch ports in QNX build (i.e. BUILD_QNX_A72=yes) because QNX virtual MAC driver does not support MAC-only mode.

Back To Top


Inter-core Virtual Ethernet

Starting with SDK 8.1, the EthFw integrates Inter-core Virtual Ethernet driver which allows shared memory based Ethernet frame exchange between cores. This is modelled as virtual Ethernet adapter at each end.

  1. Topology and Design overview
  2. EthFw Server integration
  3. R5F RTOS Client integration
  4. A72 Linux Client integration

Back To Top


Topology and Design overview

Inter-core virtual network uses a star topology with the R5F_0 master core (EthFw server) acting as the central hub. Each node (core) in the network communicates directly with the master while communication between other nodes (A72 and R5F_1) is routed through the master. In addition to the Enet LLD network interfaces used to communicate with the CPSW switch, each participating core creates an inter-core network interface, which allows it to communicate with another core using standard TCP/IP protocol suite. This is aimed at modeling Ethernet-like communication between software running on-chip processing cores (R5Fs, A72). Traffic external to the SoC is handled through CPSW hardware IP that can steer traffic based on traffic flows directly to the respective cores.

The topology diagram below shows the integration of inter-core virtual Ethernet in Ethernet Firmware.

Intercore_eth_topology_overview.png
Inter-core Virtual Ethernet Topology

The main entities shown in this diagram are listed below:

  1. R5F_0 master: EthFw server core which forms the central hub of the inter-core network. Both client cores have a direct inter-core link to the R5F_0 master, as shown with green arrows. Inter-core communication between client cores e.g. A72 Linux client trying to ping R5F_1 client, goes through the R5F_0 master.
  2. R5F_1 client: This is the EthFw RTOS remote client.
  3. A72 Linux client: This is the EthFw Linux remote client.
  4. Shared memory transport: The software based packet transport used by inter-core network driver to exchange Ethernet packets. There is a dedicated set of shared queues and shared buffer pools for each pair of directly connected nodes. Please refer to the Enet LLD user guide for more details on the inter-core virtual Ethernet driver.
  5. Multicast replication manager: This software component on R5F_0 master (EthFw server) manages the fanout of shared multicast packets to the interested cores. It does so by dynamically updating the lwIP bridge FDB database to add/remove cores to/from the given multicast MAC address in response to the multicast filter API commands from the remote cores.
  6. Data paths/flows: Different data paths are used to route packets according to the type of traffic (Unicast, Broadcast and Multicast). The black arrows show core specific dedicated hardware flows which are used for unicast traffic originating from or bound to a given core as well as incoming exclusive multicast traffic for a given core. Please refer to Multicast and Broadcast Support for details on shared multicast and exclusive_multicast traffic.

Broadcast and shared multicast packets are always sent to the R5F_0 master core using the default flow shown by the red arrow. The master core creates copies of such packets in software which is shown by the blue arrows and sends them out to other cores using the inter-core Ethernet links shown by green arrows.

On RTOS cores, the inter-core virtual Ethernet driver provides a standard lwIP netif (network interface) to the application using which the application can exchange Ethernet packets with another core. The inter-core netifs are seamlessly integrated in EthFw (client and server) using lwIP bridgeif interface which allows the inter-core netifs to co-exist along-side the Enet LLD native or virtual client interface on the server and client respectively. The bridgeif provides a single unified network interface using which the application communicates with the CPSW switch or other cores without worrying about which netif to use for sending and receiving packets.

Intercore_virt_eth_rtos.png
Inter-core virtual Ethernet architecture: RTOS <-> RTOS

Inter-core virtual Ethernet can also be used on Linux through a user space demo application provided in the SDK. This demo application creates a Linux TAP networking device and passes Ethernet packets back and forth between the TAP device and the inter-core transport shared queues to communicate with the inter-core netif on EthFw server. The TAP network interface can be bridged with the Enet LLD client driver interface to provide a single unified network interface to the network stack, just like the R5F cores. The bridge will automatically select the correct interface to send the packets based on the destination IP address.

Intercore_virt_eth_linux.png
Inter-core virtual Ethernet architecture: RTOS <-> Linux

Back To Top


EthFw Server integration

The EthFw server acts as the central hub of the inter-core virtual network, therefore it instantiates two inter-core netifs, one to communicate with the EthFw R5F remote client and another for the A72 (Linux) remote client. The inter-core netifs, along-with the Enet LLD netif are all added to the lwIP bridgeif which provides a single unified interface to the network stack/application. Refer to Topology and Design overview diagram which shows the various netifs, including the lwIP bridge, created on the R5F_0 server core.

Note: The network stack / application sees only a single set of IP and MAC addresses which belong to the bridgeif. The individual netifs, including the Enet LLD netif, are neither visible to the network stack / application, nor do they get IP or MAC addresses.

Please refer to the following code in <ethfw>/apps/app_remoteswitchcfg_server/mcu_2_0/main.c to understand how these netifs are instantiated and added to the bridge:

#if defined(ETHAPP_ENABLE_INTERCORE_ETH)
/* Create Enet LLD ethernet interface */
netif_add(&netif, NULL, NULL, NULL, NULL, LWIPIF_LWIP_init, tcpip_input);
/* Create inter-core virtual ethernet interface: MCU2_0 <-> MCU2_1 */
netif_add(&netif_ic[ETHAPP_NETIF_IC_MCU2_0_MCU2_1_IDX], NULL, NULL, NULL,
(void*)&netif_ic_state[IC_ETH_IF_MCU2_0_MCU2_1],
LWIPIF_LWIP_IC_init, tcpip_input);
/* Create inter-core virtual ethernet interface: MCU2_0 <-> A72 */
netif_add(&netif_ic[ETHAPP_NETIF_IC_MCU2_0_A72_IDX], NULL, NULL, NULL,
(void*)&netif_ic_state[IC_ETH_IF_MCU2_0_A72],
LWIPIF_LWIP_IC_init, tcpip_input);
/* Create bridge interface */
bridge_initdata.max_ports = ETHAPP_LWIP_BRIDGE_MAX_PORTS;
bridge_initdata.max_fdb_dynamic_entries = ETHAPP_LWIP_BRIDGE_MAX_DYNAMIC_ENTRIES;
bridge_initdata.max_fdb_static_entries = ETHAPP_LWIP_BRIDGE_MAX_STATIC_ENTRIES;
EnetUtils_copyMacAddr(&bridge_initdata.ethaddr.addr[0U], &gEthAppObj.hostMacAddr[0U]);
netif_add(&netif_bridge, &ipaddr, &netmask, &gw, &bridge_initdata, bridgeif_init, netif_input);
/* Add all netifs to the bridge and create coreId to bridge portId map */
bridgeif_add_port(&netif_bridge, &netif);
gEthApp_lwipBridgePortIdMap[IPC_MCU2_0] = ETHAPP_BRIDGEIF_CPU_PORT_ID;
bridgeif_add_port(&netif_bridge, &netif_ic[0]);
gEthApp_lwipBridgePortIdMap[IPC_MCU2_1] = ETHAPP_BRIDGEIF_PORT1_ID;
bridgeif_add_port(&netif_bridge, &netif_ic[1]);
gEthApp_lwipBridgePortIdMap[IPC_MPU1_0] = ETHAPP_BRIDGEIF_PORT2_ID;
/* Set bridge interface as the default */
netif_set_default(&netif_bridge);
#else

Back To Top


R5F RTOS Client integration

The EthFw client on R5F_1 instantiates only one inter-core netif to communicate directly with the EthFw server on R5F_0. Similar to the EthFW server, an lwIP bridgeif is created and both the inter-core netif and the Enet LLD virtual netif are added to the bridge to provide a unified network interface to the application.

Refer to Topology and Design overview diagram which shows the various netifs, including the lwIP bridge, created on the R5F_1 client core.

Note: The network stack / application sees only a single set of IP and MAC addresses which belong to the bridgeif. The individual netifs, including the Enet LLD netif, are neither visible to the network stack / application, nor do they get IP or MAC addresses.

Please refer to the following code in <ethfw>/apps/app_remoteswitchcfg_client/mcu_2_1/main.c to understand how these netifs are instantiated and added to the bridge:

#if defined(ETHAPP_ENABLE_INTERCORE_ETH)
/* Create Enet LLD ethernet interface */
netif_add(netif, NULL, NULL, NULL, NULL, LWIPIF_LWIP_init, tcpip_input);
/* Create inter-core virtual ethernet interface: MCU2_1 <-> MCU2_0 */
netif_add(&netif_ic, NULL, NULL, NULL,
(void*)&netif_ic_state[IC_ETH_IF_MCU2_1_MCU2_0],
LWIPIF_LWIP_IC_init, tcpip_input);
/* Create bridge interface */
bridge_initdata.max_ports = ETHAPP_LWIP_BRIDGE_MAX_PORTS;
bridge_initdata.max_fdb_dynamic_entries = ETHAPP_LWIP_BRIDGE_MAX_DYNAMIC_ENTRIES;
bridge_initdata.max_fdb_static_entries = ETHAPP_LWIP_BRIDGE_MAX_STATIC_ENTRIES;
EnetUtils_copyMacAddr(&bridge_initdata.ethaddr.addr[0U], &virtNetif->macAddr[0U]);
netif_add(&netif_bridge, &ipaddr, &netmask, &gw, &bridge_initdata, bridgeif_init, netif_input);
/* Add all network interfaces to the bridge */
bridgeif_add_port_with_opts(&netif_bridge, netif, BRIDGEIF_PORT_CPSW);
bridgeif_add_port_with_opts(&netif_bridge, &netif_ic, BRIDGEIF_PORT_VIRTUAL);
/* Set bridge interface as the default */
netif_set_default(&netif_bridge);
netif_set_status_callback(&netif_bridge, EthApp_lwipNetifStatusCb);
#else

Back To Top


A72 Linux Client integration

Inter-core virtual Ethernet can also be used on the A72 Linux remote client, however lwIP is not used on Linux so we cannot use the inter-core virtual driver directly. Instead, the adaptation layer between the Linux network stack and the inter-core transport is implemented in a user space demo application called TAP, which is provided under <ethfw>/apps/tap/. This user space application creates a Linux TAP networking device and passes Ethernet packets back and forth between the TAP device and the inter-core transport shared queues to communicate with the inter-core netif on EthFw server. Further, the TAP network interface can be bridged with the Enet LLD client interface to provide a single unified interface to the network stack, just like the R5F cores.

Note: The TAP driver implementation is provided as a reference only to demonstrate and test the intercore functionality in Linux. It comes with limited feature support, such as polling mode operation only, basic packet handling.

Please refer to the following code in <ethfw>/apps/tap/tapif.c:

/* Open TAP device and get TAP device descriptor */
tap_fd = tap_open(tap_device_name);
if (tap_fd < 0) {
perror("Allocating interface");
assert(tap_fd >= 0);
}
printf("Opened TAP Device successfully\n");
fflush(stdout);
/* Try to open the memory and fetch its file descriptor */
mem_fd = open("/dev/mem", O_RDWR | O_SYNC);
if (mem_fd == -1) {
printf("Failed to open /dev/mem\n");
fflush(stdout);
assert(0 && "Failed to access shared memory");
}
/*Create a mapping between the physical addresses and virtual addresses */
/* for the Queue Region using mmap*/
IcQ_globalQTable_Handle =
(IcQ_Handle)mmap(NULL, q_len, PROT_READ | PROT_WRITE,
MAP_SHARED, mem_fd, q_base_addr);
/* Check for failure in mapping */
assert(IcQ_globalQTable_Handle != MAP_FAILED && "Queue Mapping Failed");
printf("Queue Mapping Succeeded\n");
fflush(stdout);
/*Create a mapping between the physical addresses and virtual addresses */
/* for the Buffer Region using mmap*/
BufpoolTable_Handle = (Bufpool_Handle)mmap(NULL, bufpool_len,
PROT_READ | PROT_WRITE, MAP_SHARED,
mem_fd, bufpool_base_addr);
/* Check for failure in mapping */
assert(BufpoolTable_Handle != MAP_FAILED && "Bufpool Mapping Failed");
printf("Bufpool Mapping Succeeded\n");
fflush(stdout);
/* Define txQ_Handle and rxQ_Handle */
txQ_Handle =
(IcQ_Handle)&(IcQ_globalQTable_Handle[tx_q_id]);
rxQ_Handle =
(IcQ_Handle)&(IcQ_globalQTable_Handle[rx_q_id]);
printf("Assigned Queue Handles\n");

Back To Top


Multicast and Broadcast Support

Starting with SDK 8.1, the Ethernet firmware supports client cores to receive multicast and broadcast traffic.

Broadcast support is automatically enabled through inter-core virtual Ethernet mechanism which allows sending broadcast traffic to all the client cores, provided that inter-core virtual Ethernet is enabled on that client.

For multicast support, a new multicast filter API is provided by EthFw which allows client cores to subscribe-to/unsubscribe-from multicast addresses. The Ethernet Firmware differentiates between two types of multicast addresses:

  1. Shared Multicast
  2. Exclusive Multicast
  3. Reserved Multicast

Note that the cores requesting a multicast address do not need to know if a particular multicast address is shared or exclusive. This accounting is handled by the EthFw server and is completely transparent to the requesting client core.

Back To Top


Shared Multicast

Shared multicast allows multiple client cores to subscribe to the same multicast address. To support this, EthFw maintains a list of pre-defined multicast addresses which are treated as shared.

  1. More than one core can request these multicast addresses through the multicast filter API.
  2. Traffic for these multicast addresses is always routed to the EthFw server from where it is fanned out to all the client cores that requested that particular multicast address.
  3. Shared multicast fanout is performed in software using inter-core virtual Ethernet mechanism, therefore it is suited for low to medium bandwidth multicast traffic only.
  4. The shared multicast address list is defined in source as shown below so the user will need to modify and rebuild the EthFw binaries if they need to change these addresses:

Please refer to the following code in <ethfw>/apps/app_remoteswitchcfg_server/mcu_2_0/main.c:

/* Must not exceed ETHAPP_MAX_SHARED_MCAST_ADDR entries */
static EthApp_SharedMcastAddrTable gEthApp_sharedMcastAddrTable[] =
{
{
/* MCast IP ADDR: 224.0.0.1 */
.macAddr = {0x01,0x00,0x5E,0x00,0x00,0x01},
.portMask= 0U,
},
{
/* MCast IP ADDR: 224.0.0.251 */
.macAddr = {0x01,0x00,0x5E,0x00,0x00,0xFB},
.portMask= 0U,
},
{
/* MCast IP ADDR: 224.0.0.252 */
.macAddr = {0x01,0x00,0x5E,0x00,0x00,0xFC},
.portMask= 0U,
},
{
.macAddr = {0x33,0x33,0x00,0x00,0x00,0x01},
.portMask= 0U,
},
{
.macAddr = {0x33,0x33,0xFF,0x1D,0x92,0xC2},
.portMask= 0U,
},
{
.macAddr = {0x01,0x80,0xC2,0x00,0x00,0x00},
.portMask= 0U,
},
{
.macAddr = {0x01,0x80,0xC2,0x00,0x00,0x03},
.portMask= 0U,
},
};

Back To Top


Exclusive Multicast

Exclusive multicast addresses are allocated to only one core at any given time and the corresponding multicast traffic is routed to that core directly using a dedicated hardware flow.

  1. Any multicast addresses that do not belong to the shared multicast address list are considered exclusive and ownership of such multicast addresses is granted to the first requesting core. Any other cores requesting the same exclusive multicast address after it has already been allocated, will get a failure.
  2. Exclusive multicast traffic is routed directly to the allocated core through a dedicated hardware flow therefore it is suitable for high bandwidth single-core multicast traffic.

Reserved Multicast

Reserved multicast addresses are exclusive multicast addresses that are allocated only to the core running Ethernet Firmware. Any other core requesting for a reserved multicast address will get a failure.

PTP-related multicast addresses are defined as reserved multicast addresses in Ethernet Firmware's default configuration. This is needed because Ethernet Firmware runs the PTP stack and is the sole destination of PTP packets.

/* Note: Must not exceed ETHFW_RSVD_MCAST_LIST_LEN */
static uint8_t gEthApp_rsvdMcastAddrTable[][ENET_MAC_ADDR_LEN] =
{
/* PTP - Peer delay messages */
{
0x01, 0x80, 0xc2, 0x00, 0x00, 0x0E,
},
/* PTP - Non peer delay messages */
{
0x01, 0x1b, 0x19, 0x00, 0x00, 0x00,
},
};

Back To Top


EthFw Demos

The EthFw demos showcase the integration and usage of the Ethernet Firmware which provides a high-level interface for applications to configure and use the integrated Ethernet switch peripheral (CPSW5G/CPSW9G).

The following sample applications are key to demonstrate the capabilities of the CPSW9G/CPSW5G hardware as well as the EthFw stack.

Demo Comments
L2 Switching Configures CPSW5G/CPSW9G switch to enable switching between its external ports
L2/L3 address based classification Illustrates traffic steering to A72 (Linux) and R5F (RTOS) based on Layer-2 Ethernet header. iperf tool and web servers are used to demonstrate traffic steering to/from PCs connected to the switch
Inter-VLAN Routing (SW) Showcases inter-VLAN routing using lookup and forward operations being done in SW (R5F). It also showcases low-level lookup and forwarding on top of Enet LLD
Inter-VLAN Routing (HW) Illustrates hardware offload support for inter-VLAN routing, demonstrating the CPSW5G/CPSW9G hardware capabilities to achieve line rate routing without additional impact on R5F CPU load

EthFw Switching & TCP/IP Apps Demo

This demo showcases switching capabilities of the integrated Ethernet Switch (CPSW9G or CPSW5G) found in J721E, J7200 and J784S4 devices for features like VLAN, Multicast, etc. It also demonstrates lwIP (TCP/IP stack) integration into the EthFw.

Inter-VLAN Routing Demo

This demo illustrates hardware and software based inter-VLAN routing. The hardware inter-VLAN routing makes use of the CPSW9G/CPSW5G hardware features which enable line-rate inter-VLAN routing without any additional CPU load on the EthFw core. The software inter-VLAN routing is implemented as a fall-back alternative.

The hardware inter-VLAN route demo exercises the CPSW ALE classifier feature, which is used per flow to characterize the route and configure the egress operation.

Available egress operations:

  • Replace Destination (MAC) Address
  • Replace Source (MAC) Address
  • Replace VLAN ID
  • Optional decrement of Time To Live (TTL)
  • Supports IPv4 (TTL) and IPv6 (Hop Limit) fields
  • Packets with 0 or 1 TTL/Hop Limit are sent to the host for error processing

For further information, please refer to the Ethernet Firmware differentiating features demos demo application documentation.

Back To Top


Dependencies

Dependencies can be categorized as follows:

  1. Hardware Dependencies
  2. Software Dependencies

Please note that the dependencies vary depending on the intended use (e.g. for integration vs running demo applications only).

Back To Top


Hardware Dependencies

EthFw is supported on the following EVMs and expansion boards listed below:

SoC EVM Expansion boards
J721E J721E/J7200 EVM J721E GESI Expansion Board
J721E Quad-Port Eth Expansion Board
J7200 J721E/J7200 EVM J7200 Quad-Port Eth Expansion Board
J784S4 J784S4 EVM J784S4 Quad-Port Eth Expansion Board

Note: Quad-Port Eth expansion board is supported in all EVMs, but with different MAC port number assignments, hence they are listed in separate sections.

J721E/J7200 EVM

J7EVM_CPSW_TopView.png
J721E/J7200 EVM connections

J721E GESI Expansion Board

GESI_Board.png
J721E EVM GESI Board Top View

There are four RGMII PHYs in the J721E GESI board as shown in the following image. They will be referred to as MAC Port 1, MAC Port 3, MAC Port 4 and MAC Port 8 throughout this document.

GESI_RJ45_SideView.png
GESI Board connections

Please refer to the SDK Description for details about installation and getting started of J721E EVM.

Note: GESI expansion board is also available in J7200 EVM, but only one MAC port is routed to the CPSW5G in J7200, hence GESI board is not enabled and used by default in the Ethernet Firmware for J7200.

Back To Top

J721E Quad-Port Eth Expansion Board

The Quad-Port Eth expansion board in J721E EVM provides four MAC ports in addition to the four MAC ports in GESI board.

It enables four MAC ports: MAC Port 2, MAC Port 5, MAC Port 6 and MAC Port 7.

J721E_QPENet_Board.png
Quad Port Eth Board connections in J7200 EVM

Please refer to the SDK for more details about installation and getting started on J721E EVM.

Back To Top

J7200 Quad-Port Eth Expansion Board

The Quad-Port Eth expansion board provides the connectivity to the four MAC ports in J7200's CPSW5G: MAC Port 1, MAC Port 2, MAC Port 3 and MAC Port 4.

J7200_QPENet_Board.png
Quad Port Eth Board connections in J7200 EVM

Please refer to the SDK for more details about installation and getting started on J7200 EVM.

Back To Top

J784S4 EVM

J784S4EVM_CPSW_TopView.png
J784S4 EVM connections

J784S4 Quad-Port Eth Expansion Board

Currently, Ethernet Firmware supports only one Quad-Port Eth expansion board connected in expansion connectors labeled as ENET-EXP-1.

It enables four MAC ports: MAC Port 1, MAC Port 3, MAC Port 4 and MAC Port 5.

J784S4_QPENet_Board.png
Quad Port Eth Board connections in J784S4 EVM

Please refer to the SDK for more details about installation and getting started on J784S4 EVM.

Back To Top


Software Dependencies

Below listed dependencies are part of Processor SDK package.

PDK

Platform Development Kit (PDK) is a component within the Processor SDK RTOS which provides Chip Support Library (CSL), Low-Level Drivers (LLD), Boot, Diagnostics, etc.

The following sections list the PDK subcomponents that are required by the EthFw package.

Please refer to the Release Notes that came with this release for the compatible version of PDK/SDK.

CSL

Chip Support Library (CSL) implements peripheral register level and functional level APIs. CSL also provides peripheral base addresses, register offset, C macros to program peripheral registers.

EthFw uses CSL to determine peripheral addresses and program peripheral registers.

UDMA

Unified DMA (UDMA) is an integral part of the Jacinto 7 devices and is in charge of moving data between peripherals and memory.

PDK includes an UDMA LLD which provides APIs that the Enet LLD relies on to send and receive packets to the CPSW's host port.

Enet LLD

This is Ethernet driver module used to program the CPSW5G or CPSW9G (Switch) IP. EthFw receives commands/configuration from application and uses Enet LLD to configure CPSW5G/CPSW9G.

Enet LLD supports other Ethernet peripherals available in TI SoCs and provides a unified interface to program them.

lwIP

lwIP is a free TCP/IP stack developed by Adam Dunkels at the Swedish Institute of Computer Science (SICS) and licensed under a modified BSD license (completely open-source).

The focus of the LwIP TCP/IP implementation is to reduce RAM usage while keeping a full scale TCP/IP stack thus making it suitable for our requirements.

LwIP supports the following features:

  • IPv4 and IPv6 (Internet Protocol v4 and v6)
  • ICMP (Internet Control Message Protocol) for network maintenance and debugging
  • IGMP (Internet Group Management Protocol) for multicast traffic management
  • UDP (User Datagram Protocol)
  • TCP (Transmission Control Protocol)
  • DNS (Domain Name Server)
  • SNMP (Simple Network Management Protocol)
  • DHCP (Dynamic Host Configuration Protocol)
  • PPP (Point to Point Protocol)
  • ARP (Address Resolution Protocol)

Starting in SDK 8.0, Ethernet Firmware has been migrated to lwIP stack. The actual integration of lwIP into J721E/J7200/J784S4 devices is done through Enet LLD, which implements the lwIP netif driver interface.

The Enet LLD lwIP driver interface implementation can be located at: <pdk>/packages/ti/drv/enet/lwipif/src.

The lwIP configuration file (lwipopts.h) contains the lwIP stack features that are enabled by default in the Enet LLD driver implementation, such as TCP, UDP, DHCP, etc. It's located at <pdk>/packages/ti/transport/lwip/lwip-port/freertos/include/lwipopts.h. User should also refer to this file if interested on enabling any of the different lwIP debug options.

The lwIP pool configuration file (lwippools.h) contains the different pools and their sizes required by the Enet LLD lwIP interface implementation. This file is located at <pdk>/packages/ti/drv/transport/lwip/lwip-port/freertos/include/lwippools.h.

Ethernet Firmware Proxy ARP

Enet LLD lwIP interface implementation provides a hook to let application process a packet and indicate whether the packet needs additional handling (i.e. be passed to the lwIP stack) or if the packet can be recycled (i.e. already handled by the application).

This feature enables Ethernet Firmware to implement Proxy ARP functionality needed to respond to ARP Request packets on behalf of Ethernet Firmware's remote core clients as broadcast packets are passed exclusively to Main R5F core 0, not to each individual remote core.

Ethernet Firmware sets up a dedicated UDMA RX flow where packets that have ARP EtherType and broadcast destination MAC address are routed to. While lwIP interface is processing packets from this RX flow, it will call the packet processing function registered by Ethernet Firmware. Ethernet Firmware then checks if the packet is meant for any of its remote core clients, if so, it responds on its behalf and packet is recycled as it needs not be passed to lwIP stack. If the packet is not meant to any of the remote cores, it's simply passed to the lwIP stack, ARP request packets meant for Ethernet Firmware itself fall into this processing category.

SafeRTOS

Ethernet Firmware requires the following SafeRTOS kernel versions, depending on the SoC being used.

SoC ISA SafeRTOS package version
J721E R5F 009-004-199-024-219-001
J7200 R5F 009-002-199-024-243-001
J784S4 R5F 009-004-199-024-251-001

Back To Top


IDE (CCS)

Install Code Composer Studio and setup a Target Configuration for use with J721E, J7200 or J784S4 EVM. Refer to the instructions in CCS Setup section of the Processor SDK RTOS documentation.

Back To Top


Installation Steps


Ethernet Firmware and its dependencies are part of the SDK, separate installation is not required.

Back To Top


Directory Structure

Post installation of SDK, the following directory would be created. Please note that this is an indicative snap-shot, modules could be added/modified.

The top-level EthFw makefile as well as the auxiliary makefiles for build flags (ethfw_build_flags.mak) and build paths (ethfw_tools_path.mak) can be found at the EthFw top-level directory.

Post Install Directory Structure

c_ug_dir_top.png
Top Level Directory Structure

Utilities Directory Structure

The utils directory contains miscellaneous utilities required by the EthFw applications.

c_ug_dir_utils.png
Utilities Directory Structure

Demo Application Sources Directory Structure

Source code of the EthFw demo applications is in the apps directory. For instance, below image shows the directory structure of the server application which implements L2 switch, inter-VLAN routing, etc.

c_ug_dir_l2_switching_demo.png
EthFw Server-side Application Directory Structure

Pre-compiled binaries are also provided as part of the EthFw release, which can be found in the out directory. For instance, below image shows the EthFw output directory structure with pre-compiled server and client binaries.

c_ug_dir_j721_r5f_demo.png
Demo Binaries Directory Structure

Back To Top


EthFw Demonstration Applications

Refer to EthFw Demo Applications section for a full list of EthFw demo applications.

Back To Top


Build


EthFw employs Concerto makefile-based build system. When building on a Windows based machine, tools such as Cygwin could be used.

Back To Top


Setup Environment

The tool paths required by the build system are defined in the ethfw_tools_path.mak makefile. The default paths in ethfw_tools_path.mak are defined based on the assumption that the EthFw package has been installed inside the Processor SDK main directory.

Typically, the Processor SDK installation path is ~/ti in Linux-based systems. So, a typical EthFw installation would be at ~/ti/ti-processor-sdk-rtos-j721e-evm-08_xx_yy_zz or similarly for other SoCs. In this case, no additional environment setup steps are required.

If either Processor SDK or EthFw have been installed at different locations that those mentioned in previous paragraph, the following variables can be passed to the make command:

make <target> PSDK_PATH=<Processor SDK installation path> ETHFW_PATH=<EthFw installation path>

Please refer to the Build and Clean sections for a list of recommended targets. Alternatively, run the following command to get the full list of valid targets:

make help

Back To Top


Build

The make commands listed below require the environment setup according to Setup Environment section.

Build All

Build EthFw components as well as its dependencies, including PDK, lwIP, etc.

For J721E:

make ethfw_all BUILD_SOC_LIST=J721E

For J7200:

make ethfw_all BUILD_SOC_LIST=J7200

For J784S4:

make ethfw_all BUILD_SOC_LIST=J784S4

By default, above commands will build Ethernet Firmware for FreeRTOS.

Verbose build can be enabled by setting the SHOW_COMMANDS variable as shown below:

make ethfw_all BUILD_SOC_LIST=<SOC> SHOW_COMMANDS=1

On successful compilation, the output folder would be created at <ethfw>/out.

SafeRTOS Build

The RTOS used in Ethernet Firmware build is determined by the following flags, which can be set in ethfw_build_flags.mk or passed to the make command:

  • BUILD_APP_FREERTOS enables FreeRTOS build of EthFw and RTOS client.
  • BUILD_APP_SAFERTOS enables SafeRTOS build of EthFw and RTOS client. It requires SafeRTOS kernel installed in SDK installation path.

The location of the SafeRTOS package can be changed through the SAFERTOS_KERNEL_INSTALL_r5f_<SOC> variable in ethfw_tools_path.mak. The SafeRTOS version validated for each SoC can also be found in ethfw_tools_path.mak.

Build for SafeRTOS only, FreeRTOS build disabled:

make ethfw_all BUILD_SOC_LIST=<SOC> BUILD_APP_FREERTOS=no BUILD_APP_SAFERTOS=yes

Build for SafeRTOS and FreeRTOS:

make ethfw_all BUILD_SOC_LIST=<SOC> BUILD_APP_FREERTOS=yes BUILD_APP_SAFERTOS=yes

QNX Build

Build EthFw components for QNX OS integration running on A72.

make ethfw_all BUILD_SOC_LIST=<SOC> BUILD_QNX_A72=yes

For QNX integration, the BUILD_QNX_A72 flag will make sure that EthFW would not load the IPC resource table, unlike in Linux.

When building for Linux, the BUILD_QNX_A72 can be omitted.

Back To Top


Clean

The make commands listed below require the environment setup according to Setup Environment section.

Clean All

Clean EthFw components as well as its dependencies:

make ethfw_all_clean BUILD_SOC_LIST=<SOC>

Remove build output

Remove EthFw build output directory only.

make scrub

Back To Top


Profiles

  • Debug: Mostly used to development or debugging
    make ethfw_all BUILD_SOC_LIST=<SOC> PROFILE=debug
    
  • Release: Recommended to be used for optimized components and production builds
    make ethfw_all BUILD_SOC_LIST=<SOC> PROFILE=release
    

Back To Top


Examples Linker File (Select memory location to hold example binary)

The example applications use different memories and this could be changed and/or re-configured via linker command files.

  • linker_mem_map.cmd is auto generated file using PyTI_PSDK_RTOS tool which defines memory layout (addresses and sizes)
    • Available at <ethfw_xx_yy_zz_bb>/apps/app_<name>/<core>/linker_mem_map.cmd
  • linker.cmd defines the section mappings used by EthFw application
    • Sets optimal memories for time critical symbols ("text_fast")
    • Available at <ethfw_xx_yy_zz_bb>/apps/app_<name>/<core>/linker.cmd

Back To Top


Running Examples


Load Example Binaries

Refer to EthFw Demo Applications section for a full list of EthFw demo applications.

For detailed steps to load and run the demo application, please refer to the Demo Setup section.

Back To Top


Un Installation


Delete the complete ethfw_xx_yy_zz_bb folder.

Back To Top


Known issues

Please refer to the Ethernet Firmware Release Notes.

Back To Top


Compiler Flags used


Demo Application - Profile: Debug

Flag Description
-O0 Optimization level 0
-D=MAKEFILE_BUILD Makefile-based build type
-D=TARGET_BUILD=2 Identifies the build profile as 'debug'
-D_DEBUG_=1 Identifies as debug build
-D=ETHFW_CCS Identifies ETHFW build for CCS boot, disabled for U-Boot/SBL build
-D=SOC_J721E Identifies the J721E SoC type
-D=J721E Identifies the J721E device type
-D=SOC_J7200 Identifies the J7200 SoC type
-D=J7200 Identifies the J7200 device type
-D=SOC_J784S4 Identifies the J784S4 SoC type
-D=J784s4 Identifies the J784S4 device type
-D=R5Ft="R5Ft" Identifies the core type as ARM R5F with Thumb2 enabled
-D=TARGET_NUM_CORES=2 Identifies the core id as mcu2_0 (ETHFW server)
-D=TARGET_NUM_CORES=3 Identifies the core id as mcu2_1 (RTOS client)
-D=TARGET_ARCH=32 Identifies the target architecture as 32-bit
-D=ARCH_32 Identifies the architecture as 32-bit
-D=FREERTOS Identifies as FreeRTOS operating system build
-D=SAFERTOS Identifies as SafeRTOS operating system build
-D=ETHFW_PROXY_ARP_SUPPORT Enable Proxy ARP support on EthFw server
-D=ETHAPP_INTERCORE_ETH_SUPPORT Enable Intercore Virtual Ethernet support (disabled if BUILD_QNX_A72 is defined)
-D=ENABLE_QSGMII_PORTS Enable QSGMII ports in QpENet expansion board (applicable only to J721E)

Other common flags:

-Wno-extra -Wno-exceptions -ferror-limit=100 -Wno-parentheses-equality -Wno-unused-command-line-argument -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -Wno-inconsistent-missing-override -Wno-address-of-packed-member -Wno-self-assign -Wno-ignored-attributes -Wno-bitfield-constant-conversion -Wno-unused-const-variable -Wno-unused-variable -Wno-format-security -Wno-excess-initializers -Wno-sometimes-uninitialized -Wno-empty-body -Wno-extern-initializer -Wno-absolute-value -Wno-missing-braces -Wno-ti-macros -Wno-pointer-sign -Wno-macro-redefined -Wno-main-return-type -Werror -O0 -ggdb3 -mfloat-abi=hard -mfpu=vfpv3 -D16 -mcpu=cortex-r5 -march=armv7-r -mthumb -fno-strict-aliasing -ffunction-sections

Back To Top


Demo Application - Profile: Release

Flag Description
-O3 Optimization level 3
-D=MAKEFILE_BUILD Makefile-based build type
-D=TARGET_BUILD=1 Identifies the build profile as 'release'
-D=ETHFW_CCS Identifies ETHFW build for CCS boot, disabled for U-Boot/SBL build
-D=SOC_J721E Identifies the J721E SoC type
-D=J721E Identifies the J721E device type
-D=SOC_J7200 Identifies the J7200 SoC type
-D=J7200 Identifies the J7200 device type
-D=SOC_J784S4 Identifies the J784S4 SoC type
-D=J784S4 Identifies the J784S4 device type
-D=R5Ft="R5Ft" Identifies the core type as ARM R5F with Thumb2 enabled
-D=TARGET_NUM_CORES=2 Identifies the core id as mcu2_0 (ETHFW server)
-D=TARGET_NUM_CORES=3 Identifies the core id as mcu2_1 (RTOS client)
-D=TARGET_ARCH=32 Identifies the target architecture as 32-bit
-D=ARCH_32 Identifies the architecture as 32-bit
-D=FREERTOS Identifies as FreeRTOS operating system build
-D=SAFERTOS Identifies as SafeRTOS operating system build
-D=ETHFW_PROXY_ARP_SUPPORT Enable Proxy ARP support on EthFw server
-D=ETHAPP_INTERCORE_ETH_SUPPORT Enable Intercore Virtual Ethernet support (disabled if BUILD_QNX_A72 is defined)
-D=ENABLE_QSGMII_PORTS Enable QSGMII ports in QpENet expansion board (applicable only to J721E)

Other common flags:

-Wno-extra -Wno-exceptions -ferror-limit=100 -Wno-parentheses-equality -Wno-unused-command-line-argument -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -Wno-inconsistent-missing-override -Wno-address-of-packed-member -Wno-self-assign -Wno-ignored-attributes -Wno-bitfield-constant-conversion -Wno-unused-const-variable -Wno-unused-variable -Wno-format-security -Wno-excess-initializers -Wno-sometimes-uninitialized -Wno-empty-body -Wno-extern-initializer -Wno-absolute-value -Wno-missing-braces -Wno-ti-macros -Wno-pointer-sign -Wno-macro-redefined -Wno-main-return-type -Werror -O3 -mfloat-abi=hard -mfpu=vfpv3 -D16 -mcpu=cortex-r5 -march=armv7-r -mthumb -fno-strict-aliasing -ffunction-sections

Back To Top


Supported Device Families


Device Family Variant Known by other names
Jacinto 7 J721E -
J7200 -
J784S4 -

Back To Top


Document Revision History


Revision Date Author Description
0.1 01 Apr 2019 Prasad J, Misael Lopez Created for v.0.08.00
0.2 02 Apr 2019 Prasad J 0.8 Docs review meeting fixes
0.3 12 Jun 2019 Prasad J Updates for EVM demo (.85 release)
0.4 17 Jul 2019 Misael Lopez Updates for v.0.09.00
0.5 15 Oct 2019 Misael Lopez, Santhana Bharathi Updates for v.1.00.00
1.0 28 Jan 2020 Misael Lopez Updates for SDK 6.02.00
1.1 31 Aug 2020 Misael Lopez Added J7200 support for SDK 7.01 EA
1.2 02 Nov 2020 Misael Lopez Updated for Enet LLD migration
1.3 01 Dec 2021 Nitin Sakhuja Adedd Inter-core Ethernet support for SDK 8.1
1.4 07 Dec 2021 Misael Lopez Adedd MAC-only, server and client doc
1.5 01 Jul 2021 Misael Lopez Updates for J784S4 support and SDK 8.02.01
1.6 10 Feb 2023 Misael Lopez Added SafeRTOS build info

Back To Top (User Guide)