![]() |
![]() |
|
XDAIS
dais-x04
|
Defines the creation time parameters for all IVIDDEC1 instance objects. More...
#include <ividdec1.h>

Data Fields | |
| XDAS_Int32 | size |
| XDAS_Int32 | maxHeight |
| XDAS_Int32 | maxWidth |
| XDAS_Int32 | maxFrameRate |
| XDAS_Int32 | maxBitRate |
| XDAS_Int32 | dataEndianness |
| XDAS_Int32 | forceChromaFormat |
| Chroma formats. | |
Defines the creation time parameters for all IVIDDEC1 instance objects.
size parameter. size field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. | XDAS_Int32 IVIDDEC1_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
| XDAS_Int32 IVIDDEC1_Params::maxHeight |
Maximum video height in pixels.
| XDAS_Int32 IVIDDEC1_Params::maxWidth |
Maximum video width in pixels.
| XDAS_Int32 IVIDDEC1_Params::maxFrameRate |
Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.
| XDAS_Int32 IVIDDEC1_Params::maxBitRate |
Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000
| XDAS_Int32 IVIDDEC1_Params::dataEndianness |
Endianness of output data.
| XDAS_Int32 IVIDDEC1_Params::forceChromaFormat |
Chroma formats.