TIOVX User Guide

Object descriptor. More...

#include <tivx_obj_desc.h>

Data Fields

volatile uint16_t obj_desc_id
 ID of object in shared memory.
 
volatile uint16_t type
 Type of object descritor, see tivx_obj_desc_type_e.
 
volatile uint16_t scope_obj_desc_id
 object descriptor ID of the scope in which this object is created For element of pyramid and object array, this is obj_desc_id of excompassing pyramid, object array
 
volatile uint16_t in_node_done_cnt
 number of input nodes that have consumed this obj_desc, used in pipelining mode only for data references
 
volatile uint64_t host_ref
 Host reference, accessible only on HOST side.
 
volatile uint32_t flags
 reference flags
 
volatile uint32_t element_idx
 holds the index ID in the case that this is an element within a pyramid or object array
 
volatile uint64_t timestamp
 reference timestamp
 
volatile uint32_t host_cpu_id
 holds the CPU ID of the OpenVX host for this object descriptor
 
volatile uint32_t rsv0
 reserved to make 64b aligned
 
volatile uint16_t host_port_id [TIVX_OBJ_DESC_MAX_HOST_PORT_ID_CPU]
 holds the index of the IPC port on OpenVX host for this object descriptor for each remote CPU More...
 

Detailed Description

Object descriptor.

Must be first element of any objects descriptors placed in shared memory

Make sure this structure is multiple of 64b

Definition at line 292 of file tivx_obj_desc.h.

Field Documentation

◆ host_port_id

volatile uint16_t tivx_obj_desc_t::host_port_id[TIVX_OBJ_DESC_MAX_HOST_PORT_ID_CPU]

holds the index of the IPC port on OpenVX host for this object descriptor for each remote CPU

A connection to each remote CPU could be on a different host_port_id, hence this needs to hold host_port_id for each remote CPU, this array is indexed by TIOVX CPU ID. TIVX_OBJ_DESC_MAX_HOST_PORT_ID_CPU MUST be <= TIVX_CPU_ID_MAX

Definition at line 333 of file tivx_obj_desc.h.


The documentation for this struct was generated from the following file: