APIs for real-time event trace operations on the host.
◆ tivxLogRtTraceEnable()
Enable run-time logging of graph trace.
- By default run-time logging is disabled.
- This API MUST be called after vxVerifyGraph and before starting the graph execution
- Parameters
-
◆ tivxLogRtTraceDisable()
Sisable run-time logging of graph trace.
- By default run-time logging is disabled.
- This API MUST be called after graph executions have stopped and before calling vxReleaseGraph
- Parameters
-
◆ tivxLogRtTraceExportToFile()
Saved current log events to file and clear the event log memory.
- This API can be called while graphs are executing
- Each time API is called, current log events are saved to the file 'filename' and existing log is cleared.
- Calling this API periodically avoids the event log from getting full.
- Thus this API allows to continously store data to a file on the filesystem, limited only by the size of free space on the filesystem.
- The data stored in the file can be visualized by doing below
- Copy the saved file(s) to PC
- Convert the binary data to 'VCD - Value Change Dump' format
- Use a opensource tool like gtkwave to visualize the data
- Parameters
-
[in] | filename | Filename to save the log data into. When filename is NULL, data is not saved, only the event log is cleared. |
- Precondition
- tivxLogRtTraceEnable
◆ tivxLogRtTraceKernelInstanceAddEvent()
void tivxLogRtTraceKernelInstanceAddEvent |
( |
vx_node |
node, |
|
|
uint16_t |
event_index, |
|
|
char * |
event_name |
|
) |
| |
Add real-time log event in host side initilize callback for user kernel.
- This API is intended to be called from within the initialization callback of a user kernel.
- For a given node, multiple such events can be added, therefore each one should be given a different index used to identify the event within the node.
- Since the scope of the indexing is within a single node, it is permissible to reuse index values across nodes without any issue (for example, event_index of 0 can be used at most once per node).
- Parameters
-
[in] | node | The node object that the event is to be asociated with |
[in] | event_index | Unique identifier of specific event within node |
[in] | *event_name | The node object associated with the event |
◆ tivxLogRtTraceKernelInstanceRemoveEvent()
void tivxLogRtTraceKernelInstanceRemoveEvent |
( |
vx_node |
node, |
|
|
uint16_t |
event_index |
|
) |
| |
Remove real-time log event in host side deinitilize callback for user kernel.
- This API is intended to be called from within the deinitialization callback of a user kernel.
- Parameters
-
[in] | node | The node object that the event is to be asociated with |
[in] | event_index | Unique identifier of specific event within node |
- Precondition
- tivxLogRtTraceKernelInstanceAddEvent