TIOVX User Guide
ch03_graph Directory Reference

Directories

Files

file  phase_rgb_user_kernel.c [code]
 
file  phase_rgb_user_kernel.h [code]
 
file  vx_tutorial_graph_image_gradients.c [code]
 
file  vx_tutorial_graph_image_gradients_pytiovx_uc.py [code]
 This file show example of using basic PyTIOVX APIs to describe an OpenVX graph.
 
file  vx_tutorial_graph_user_kernel.c [code]
 
file  vx_tutorial_graph_user_kernel_pytiovx.c [code]
 
file  vx_tutorial_graph_user_kernel_pytiovx_uc.py [code]
 This file show example of using basic PyTIOVX APIs to describe user/target kernel class and use it within an OpenVX graph.