PDK API Guide for J721E
|
OSPI Parameters.
OSPI Parameters are used to with the OSPI_open() call. Default values for these parameters are set using OSPI_Params_init().
Data Fields | |
OSPI_TransferMode | transferMode |
uint32_t | transferTimeout |
OSPI_CallbackFxn | transferCallbackFxn |
OSPI_Mode | mode |
uint32_t | bitRate |
uint32_t | dataSize |
OSPI_FrameFormat | frameFormat |
void * | custom |
OSPI_TransferMode OSPI_Params::transferMode |
Blocking or Callback mode
uint32_t OSPI_Params::transferTimeout |
Transfer timeout in system ticks (Not supported with all implementations
OSPI_CallbackFxn OSPI_Params::transferCallbackFxn |
Callback function pointer
OSPI_Mode OSPI_Params::mode |
Master or Slave mode
uint32_t OSPI_Params::bitRate |
SPI bit rate in Hz
uint32_t OSPI_Params::dataSize |
SPI data frame size in bits
OSPI_FrameFormat OSPI_Params::frameFormat |
SPI frame format
void* OSPI_Params::custom |
Custom argument used by driver implementation