![]() |
PDK API Guide for J721E
|
Parameter structure for creating VirtIO table for each core combinations.
Data Fields | |
void * | vqObjBaseAddr |
uint32_t | vqBufSize |
void * | vringBaseAddr |
uint32_t | vringBufSize |
uint32_t | timeoutCnt |
void* Ipc_VirtIoParams::vqObjBaseAddr |
Base address for storing VQ Object
uint32_t Ipc_VirtIoParams::vqBufSize |
Size of the Buffer for storing VQ objects
void* Ipc_VirtIoParams::vringBaseAddr |
Base address for Shared VRing for all cores
uint32_t Ipc_VirtIoParams::vringBufSize |
Buffer Size. Recommemded Size is 0x40000 * NumOfCores
uint32_t Ipc_VirtIoParams::timeoutCnt |
timeoutCnt. Set 0xFFFFFFFF for wait forever