PDK API Guide for J721E
|
This is CSITX driver event related configuration parameters and API
Files | |
file | csitx_event.h |
CSITX event related parameters and API. | |
Data Structures | |
struct | Csitx_EventPrms |
CSITX event related parameters. More... | |
struct | Csitx_EventStatus |
CSITX event status parameters. Instance of this structure will passed to the application call-back. More... | |
Functions | |
void | Csitx_eventPrmsInit (Csitx_EventPrms *eventPrms) |
Csitx_EventPrms structure init function. More... | |
Typedefs | |
typedef void(* | CsitxDrv_EventCallback) (Csitx_EventStatus eventStatus, void *appData) |
CSITX event callback function. More... | |
Macros | |
#define | CSITX_EVENT_INVALID ((uint32_t) CSL_CSITXP_NO_EVENT) |
Macro used to specify that event ID is invalid. More... | |
#define | CSITX_INTR_INVALID ((uint32_t) 0xFFFF0000U) |
Macro used to specify that interrupt number is invalid. More... | |
#define | CSITX_EVENT_TYPE_ERR_ALL |
Mask for all Error interrupts/events. More... | |
#define | CSITX_EVENT_TYPE_FRAME_IRQ |
Mask for all Frame interrupts/events. More... | |
#define | CSITX_EVENT_PIXEL_IF_SHIFT_WIDTH |
shift width between events of each Pixel interface. More... | |
CSITX Event Group | |
CSITX events groups per CSI instance supported. | |
#define | CSITX_EVENT_GROUP_TX_IRQ ((uint32_t) 0U) |
Event Group: Tx Interrupts. Tx interrupts event group. More... | |
#define | CSITX_EVENT_GROUP_MAX |
CSITX Tx Interrupts Event Type | |
CSITX Tx interrupt events supported. This is valid if event group is 'CSITX_EVENT_GROUP_TX_IRQ' | |
#define | CSITX_EVENT_TYPE_TX_IRQ_ALL |
Mask for all interrupts/events. More... | |
#define CSITX_EVENT_INVALID ((uint32_t) CSL_CSITXP_NO_EVENT) |
Macro used to specify that event ID is invalid.
#define CSITX_INTR_INVALID ((uint32_t) 0xFFFF0000U) |
Macro used to specify that interrupt number is invalid.
#define CSITX_EVENT_GROUP_TX_IRQ ((uint32_t) 0U) |
Event Group: Tx Interrupts. Tx interrupts event group.
Tx Event Group: Tx Interrupts.
#define CSITX_EVENT_GROUP_MAX |
#define CSITX_EVENT_TYPE_TX_IRQ_ALL |
Mask for all interrupts/events.
#define CSITX_EVENT_TYPE_ERR_ALL |
Mask for all Error interrupts/events.
#define CSITX_EVENT_TYPE_FRAME_IRQ |
Mask for all Frame interrupts/events.
#define CSITX_EVENT_PIXEL_IF_SHIFT_WIDTH |
shift width between events of each Pixel interface.
typedef void(* CsitxDrv_EventCallback) (Csitx_EventStatus eventStatus, void *appData) |
CSITX event callback function.
eventType | Event that occurred |
appData | Callback pointer passed during event register |
void Csitx_eventPrmsInit | ( | Csitx_EventPrms * | eventPrms | ) |
Csitx_EventPrms structure init function.
Note: 'eventPrms' cannot be NULL while calling this function. Also, before call 'Csitx_eventPrmsInit()', 'eventGroup' from 'eventPrms' should be set.
eventPrms | Pointer to Csitx_EventPrms structure. |