![]() |
![]() |
XDAIS
dais-x04
|
Defines the run time output arguments for all IAUDDEC1 instance objects. More...
#include <iauddec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDAS_Int32 | bytesConsumed |
XDAS_Int32 | numSamples |
XDAS_Int32 | channelMode |
XDAS_Int32 | lfeFlag |
XDAS_Int32 | dualMonoMode |
XDAS_Int32 | sampleRate |
Defines the run time output arguments for all IAUDDEC1 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IAUDDEC1_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDDEC1_OutArgs::extendedError |
Extended error information.
XDAS_Int32 IAUDDEC1_OutArgs::bytesConsumed |
Number of bytes consumed during the process() call.
XDAS_Int32 IAUDDEC1_OutArgs::numSamples |
Number of output samples per channel.
XDAS_Int32 IAUDDEC1_OutArgs::channelMode |
Output Channel Configuration.
XDAS_Int32 IAUDDEC1_OutArgs::lfeFlag |
Flag indicating the precense of LFE channel in the output. When the LFE channel is not in the output, this is set to XDAS_FALSE.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
XDAS_Int32 IAUDDEC1_OutArgs::dualMonoMode |
Mode to indicate type of Dual Mono. Only used in case of Dual Mono output.
XDAS_Int32 IAUDDEC1_OutArgs::sampleRate |
Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.