TIOVX User Guide
|
TIDL Network Kernels.
Data Structures | |
struct | tivxTIDLJ7Params |
TIDL params structure. More... | |
Defines | |
#define | TIVX_KERNEL_TIDL_NAME "com.ti.tidl" |
tidl kernel name | |
Functions | |
vx_kernel | tivxAddKernelTIDL (vx_context context, uint32_t num_input_tensors, uint32_t num_output_tensors) |
Used for the Application to create the tidl kernel from the context. More... | |
VX_API_ENTRY vx_node VX_API_CALL | tivxTIDLNode (vx_graph graph, vx_kernel kernel, vx_reference appParams[], vx_tensor input_tensors[], vx_tensor output_tensors[]) |
[Graph] Creates a TIDL Node. More... | |
void | tivxRegisterTIDLTargetKernels (void) |
Function to register TIDL Kernels on the TIDL Target. | |
void | tivxUnRegisterTIDLTargetKernels (void) |
Function to un-register TIDL Kernels on the TIDL Target. | |
static void | tivx_tidl_j7_params_init (tivxTIDLJ7Params *tidlParams) |
TIDL params initialization. | |
vx_kernel tivxAddKernelTIDL | ( | vx_context | context, |
uint32_t | num_input_tensors, | ||
uint32_t | num_output_tensors | ||
) |
Used for the Application to create the tidl kernel from the context.
[in] | context | OpenVX context which must be created using vxCreateContext |
[in] | num_input_tensors | Number of input vx_tensor objects to be created |
[in] | num_output_tensors | Number of output vx_tensor objects to be created |
VX_API_ENTRY vx_node VX_API_CALL tivxTIDLNode | ( | vx_graph | graph, |
vx_kernel | kernel, | ||
vx_reference | appParams[], | ||
vx_tensor | input_tensors[], | ||
vx_tensor | output_tensors[] | ||
) |
[Graph] Creates a TIDL Node.
[in] | graph | Reference to vx_graph. |
[in] | kernel | Reference to vx_kernel. |
[in,out] | appParams | is an array of 5 parameters:
|
[in] | input_tensors | Array of input tensors This parameter is ignored when the first layer of the network is a data layer, which is most of the time. Only networks that are dependent on the output of a previous networks have first layer that are not data layer. |
[out] | output_tensors | Array of output tensors |
vx_node
. vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |