TIOVX User Guide

Detailed Description

APIs for kernel operations on the target.

Typedefs

typedef struct _tivx_target_kernel * tivx_target_kernel
 Handle to kernel on a target.
 
typedef struct _tivx_target_kernel_instance * tivx_target_kernel_instance
 Handle to instance of kernel on a target.
 
typedef vx_status(VX_CALLBACKtivx_target_kernel_f) (tivx_target_kernel_instance kernel, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg)
 The target kernel callback. More...
 
typedef vx_status(VX_CALLBACKtivx_target_kernel_control_f) (tivx_target_kernel_instance kernel, uint32_t node_cmd_id, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg)
 The target kernel callback for control command. More...
 

Functions

VX_API_ENTRY tivx_target_kernel VX_API_CALL tivxAddTargetKernel (vx_enum kernel_id, const char *target_name, tivx_target_kernel_f process_func, tivx_target_kernel_f create_func, tivx_target_kernel_f delete_func, tivx_target_kernel_control_f control_func, void *priv_arg)
 Allows users to add native kernels implementation to specific targets. More...
 
VX_API_ENTRY tivx_target_kernel VX_API_CALL tivxAddTargetKernelByName (const char *kernel_name, const char *target_name, tivx_target_kernel_f process_func, tivx_target_kernel_f create_func, tivx_target_kernel_f delete_func, tivx_target_kernel_control_f control_func, void *priv_arg)
 Allows users to add native kernels implementation to specific targets. More...
 
VX_API_ENTRY vx_status VX_API_CALL tivxRemoveTargetKernel (tivx_target_kernel target_kernel)
 Allows users to remove native kernels implementation to specific targets.
 
VX_API_ENTRY vx_status VX_API_CALL tivxQueryNumTargetKernel (vx_uint32 *ptr)
 Queries the framework to determine the number of target kernels on the target from which it is called. More...
 
VX_API_ENTRY vx_status VX_API_CALL tivxSetTargetKernelInstanceContext (tivx_target_kernel_instance target_kernel_instance, void *kernel_context, uint32_t kernel_context_size)
 Associate a kernel function context or handle with a target kernel instance. More...
 
VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelInstanceContext (tivx_target_kernel_instance target_kernel_instance, void **kernel_context, uint32_t *kernel_context_size)
 Get a kernel function context or handle with a target kernel instance. More...
 
VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelInstanceState (tivx_target_kernel_instance target_kernel_instance, vx_enum *state)
 Get a kernel state with a target kernel instance. More...
 
VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelTargetId (tivx_target_kernel_instance target_kernel_instance, uint32_t *targetId)
 Get a kernel target id with a target kernel instance. More...
 
VX_API_ENTRY void tivxGetTargetKernelInstanceBorderMode (tivx_target_kernel_instance target_kernel_instance, vx_border_t *border_mode)
 Get the border mode for the target kernel instance. More...
 
VX_API_ENTRY vx_bool tivxIsTargetKernelInstanceReplicated (tivx_target_kernel_instance kernel_instance)
 Checks if supplied node is replicated. Returns vx_true if the given node is replicated and vx_false if not.
 
void * tivxPlatformGetDmaObj (void)
 Utility function to obtain DMA handle.
 

Typedef Documentation

◆ tivx_target_kernel_f

typedef vx_status(VX_CALLBACK * tivx_target_kernel_f) (tivx_target_kernel_instance kernel, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg)

The target kernel callback.

For create_func, delete_func and process_func callbacks 'obj_desc' points to array of data object descriptor parameters

For control_func, 'obj_desc' points to array of objects descriptors where obj_desc[0] points to the node object descriptors obj_desc[1..num_params-1] points to target kernel defined parameters

Parameters
[in]kernelThe kernel for which the callback is called
[in]obj_descObject descriptor passed as input to this callback

Definition at line 107 of file tivx_target_kernel.h.

◆ tivx_target_kernel_control_f

typedef vx_status(VX_CALLBACK * tivx_target_kernel_control_f) (tivx_target_kernel_instance kernel, uint32_t node_cmd_id, tivx_obj_desc_t *obj_desc[], uint16_t num_params, void *priv_arg)

The target kernel callback for control command.

For create_func, delete_func and process_func callbacks 'obj_desc' points to array of data object descriptor parameters

For control_func, 'obj_desc' points to array of objects descriptors for control parameter. It could be any vx_(object)

Parameters
[in]kernelThe kernel for which the callback is called
[in]CommandID to be processed in the given node
[in]obj_descObject descriptor passed as input to this callback
[in]num_paramsvalid entries in object descriptor (obj_desc) array

Definition at line 127 of file tivx_target_kernel.h.

Function Documentation

◆ tivxAddTargetKernel()

VX_API_ENTRY tivx_target_kernel VX_API_CALL tivxAddTargetKernel ( vx_enum  kernel_id,
const char *  target_name,
tivx_target_kernel_f  process_func,
tivx_target_kernel_f  create_func,
tivx_target_kernel_f  delete_func,
tivx_target_kernel_control_f  control_func,
void *  priv_arg 
)

Allows users to add native kernels implementation to specific targets.

This is different from vxAddUserKernel() in that this is called on the target CPU. This is a TI prorietary API and not part of OpenVX or TI OpenVX extention.

This allows users to implement and plugin specific target optimized kernels on TI platforms

A equivalent vxAddUserKernel is typically called to pair the target kernel with OpenVX user kernel.

◆ tivxAddTargetKernelByName()

VX_API_ENTRY tivx_target_kernel VX_API_CALL tivxAddTargetKernelByName ( const char *  kernel_name,
const char *  target_name,
tivx_target_kernel_f  process_func,
tivx_target_kernel_f  create_func,
tivx_target_kernel_f  delete_func,
tivx_target_kernel_control_f  control_func,
void *  priv_arg 
)

Allows users to add native kernels implementation to specific targets.

Same as tivxAddTargetKernel except that it take a string name as input instead of kernel_id

◆ tivxQueryNumTargetKernel()

VX_API_ENTRY vx_status VX_API_CALL tivxQueryNumTargetKernel ( vx_uint32 ptr)

Queries the framework to determine the number of target kernels on the target from which it is called.

Parameters
[out]ptrThe location at which to store the resulting value.

◆ tivxSetTargetKernelInstanceContext()

VX_API_ENTRY vx_status VX_API_CALL tivxSetTargetKernelInstanceContext ( tivx_target_kernel_instance  target_kernel_instance,
void *  kernel_context,
uint32_t  kernel_context_size 
)

Associate a kernel function context or handle with a target kernel instance.

Typically set by the kernel function during create phase

◆ tivxGetTargetKernelInstanceContext()

VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelInstanceContext ( tivx_target_kernel_instance  target_kernel_instance,
void **  kernel_context,
uint32_t *  kernel_context_size 
)

Get a kernel function context or handle with a target kernel instance.

Typically used by the kernel function during run, control, delete phase

◆ tivxGetTargetKernelInstanceState()

VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelInstanceState ( tivx_target_kernel_instance  target_kernel_instance,
vx_enum state 
)

Get a kernel state with a target kernel instance.

Typically used by a capture kernel function during process to track state

◆ tivxGetTargetKernelTargetId()

VX_API_ENTRY vx_status VX_API_CALL tivxGetTargetKernelTargetId ( tivx_target_kernel_instance  target_kernel_instance,
uint32_t *  targetId 
)

Get a kernel target id with a target kernel instance.

Typically used by nodes having multi priority implementation

◆ tivxGetTargetKernelInstanceBorderMode()

VX_API_ENTRY void tivxGetTargetKernelInstanceBorderMode ( tivx_target_kernel_instance  target_kernel_instance,
vx_border_t border_mode 
)

Get the border mode for the target kernel instance.

Used by the kernel implemention to get border mode