![]() |
SDL API Guide for J721E
|
Header file containing various enumerations, structure definitions and function declarations for the KSBUS RAT Ip. =
(C) Copyright 2016-2020, Texas Instruments, Inc.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Go to the source code of this file.
Functions | |
int32_t | SDL_RAT_isRegionTranslationEnabled (const SDL_ratRegs *pRatRegs, uint32_t regionIndex) |
This function returns the enable status of the specified region address translation. More... | |
int32_t | SDL_RAT_setErrMsgDestId (SDL_ratRegs *pRatRegs, uint32_t destId) |
This function is used to set the destination ID for error messages. More... | |
int32_t | SDL_RAT_getErrMsgDestId (const SDL_ratRegs *pRatRegs, uint32_t *pDestId) |
This function is used to read the destination ID for error messages. More... | |
int32_t | SDL_RAT_enableExceptionLog (SDL_ratRegs *pRatRegs) |
This function enables the exception logging capability. It also enables exception interrupt generation. The module's exception interrupt signal is asserted if the exception logging capability is enabled and the exception interrupt source is enabled by calling the. More... | |
int32_t | SDL_RAT_disableExceptionLog (SDL_ratRegs *pRatRegs) |
This function disables the exception logging capability. It also disables the module's exception interrupt signal generation, regardless of whether the exception interrupt source is enabled or disabled. More... | |
int32_t | SDL_RAT_isIntrPending (const SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function returns the pending interrupt status of the specified interrupt source. More... | |
int32_t | SDL_RAT_setIntrPending (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function is used to forceably set the pending status of the specified interrupt source. More... | |
int32_t | SDL_RAT_clrIntrPending (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function is used to clear the pending status of the specified interrupt source. More... | |
int32_t | SDL_RAT_ackIntr (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function is used to acknowledge the specified interrupt source. More... | |
int32_t | SDL_RAT_enableIntr (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function enables the specified interrupt source. It also calls SDL_RAT_enableExceptionLog to enable exception logging as there is no valid reason to enable the exception interrupt source and not log the exception information and assert the module's exception interrupt signal. More... | |
int32_t | SDL_RAT_disableIntr (SDL_ratRegs *pRatRegs, SDL_RAT_intrSrcTypes intrSrc) |
This function disables the specified interrupt source. This prevents the module's exception interrupt signal from being asserted. Note that software can still call SDL_RAT_isIntrPending to poll for an exception event and call SDL_RAT_getExceptionInfo to read exception event information if exception logging is enabled. More... | |
int32_t | SDL_RAT_getExceptionInfo (SDL_ratRegs *pRatRegs, SDL_ratExceptionInfo *pExceptionInfo) |
This function is used to get information for the last boundary crossing transaction exception captured. The log is automatically cleared by this function so that a future exception can be captured. More... | |
int32_t | SDL_RAT_enableRegionTranslation (SDL_ratRegs *pRatRegs, uint32_t regionIndex) |
This function enables address translation for the specified region. More... | |
int32_t | SDL_RAT_disableRegionTranslation (SDL_ratRegs *pRatRegs, uint32_t regionIndex) |
This function disables address translation for the specified region. More... | |
int32_t | SDL_RAT_configRegionTranslation (SDL_ratRegs *pRatRegs, uint32_t regionIndex, SDL_ratTranslationCfgInfo *pTranslationCfg) |
This function is used to configure a region address translation for the specified region index. The translation is automatically enabled after it is configured. More... | |
int32_t | SDL_RAT_verifyConfigRegionTranslation (const SDL_ratRegs *pRatRegs, uint32_t regionIndex, SDL_ratTranslationCfgInfo *pTranslationCfg) |
This function is used to configure a region address translation for the specified region index. The translation is automatically enabled after it is configured. More... | |
int32_t | SDL_RAT_getStaticRegs (SDL_ratRegs *pRatRegs, uint32_t regionIndex, SDL_ratStaticRegs *pStaticRegs) |
This function returns the enable status of the specified region address translation. More... | |