![]() |
SDL API Guide for J721E
|
This file contains the SDL OSAL API's.
Go to the source code of this file.
Data Structures | |
struct | SDL_OSAL_hwipParams |
This structure contains the parameters for interrupt registration through the SDL OSAL interface.More... | |
struct | SDL_OSAL_Interface |
This structure contains the pointers for the OSAL interfaces provided by the application to SDL_OSAL_init.More... | |
Typedefs | |
typedef void(* | pSDL_OSAL_interruptCallbackFunction) (uintptr_t arg) |
Prototype for the interrupt callback functionMore... | |
typedef void * | pSDL_OSAL_hwipHandle |
typedef int32_t(* | pSDL_OSAL_interruptFunction) (int32_t intNum) |
Prototype for the interrupt enable/disable functionsMore... | |
typedef pSDL_OSAL_hwipHandle(* | pSDL_OSAL_registerFunction) (SDL_OSAL_hwipParams *pParams) |
Prototype for the interrupt registration functionMore... | |
typedef int32_t(* | pSDL_OSAL_deregisterFunction) (pSDL_OSAL_hwipHandle handle) |
Prototype for the interrupt de-register functionMore... | |
typedef int32_t(* | pSDL_OSAL_globalDisableInterruptsFunction) (uintptr_t *key) |
Prototype for the interrupt global disable functionMore... | |
typedef int32_t(* | pSDL_OSAL_globalRestoreInterruptsFunction) (uintptr_t key) |
Prototype for the interrupt global restore functionMore... | |
typedef void(* | pSDL_OSAL_printFunction) (const char *traceBuf) |
Prototype for the print functionMore... | |
typedef int32_t(* | pSDL_OSAL_delayFunction) (int32_t ndelay) |
Prototype for the delay functionMore... | |
typedef void *(* | pSDL_OSAL_addrTranslateFunction) (uint64_t addr, uint32_t size) |
Prototype for address translation function. More... | |
Functions | |
int32_t | SDL_OSAL_init (SDL_OSAL_Interface *osalInterface) |
OSAL init. More... | |
int32_t | SDL_OSAL_enableInterrupt (int32_t intNum) |
OSAL enable interrupt. More... | |
int32_t | SDL_OSAL_disableInterrupt (int32_t intNum) |
OSAL disable interrupt. More... | |
int32_t | SDL_OSAL_registerInterrupt (SDL_OSAL_hwipParams *pParams, pSDL_OSAL_hwipHandle *handle) |
OSAL register interrupt. More... | |
int32_t | SDL_OSAL_deregisterInterrupt (pSDL_OSAL_hwipHandle handle) |
OSAL deregister interrupt. More... | |
int32_t | SDL_OSAL_globalDisableInterrupts (uintptr_t *key) |
OSAL globally disable interrupts. More... | |
int32_t | SDL_OSAL_globalRestoreInterrupts (uintptr_t key) |
OSAL globally enable interrupts. More... | |
void | SDL_OSAL_printf (const char *traceBuf) |
OSAL print function. More... | |
int32_t | SDL_OSAL_delay (int32_t ndelay) |
OSAL delay. More... | |
void * | SDL_OSAL_addrTranslate (uint64_t addr, uint32_t size) |
OSAL Address translation function. More... | |