34 #ifndef SDL_MCU_ARMSS_CCMR5_H 35 #define SDL_MCU_ARMSS_CCMR5_H 41 #include "sdlr_mcu_armss_ccmr5.h" 79 typedef enum SDL_McuArmssCcmR5RegId_e
104 typedef enum SDL_McuArmssCcmR5ModuleId_e
123 typedef enum SDL_McuArmssCcmR5OpModeKey_e
166 uintptr_t baseAddress,
168 uint32_t *pValToBeRead,
194 uintptr_t baseAddress,
196 uint32_t valToBeWritten,
223 uintptr_t baseAddress,
252 uintptr_t baseAddress,
294 uintptr_t baseAddress,
322 uintptr_t baseAddress,
int32_t SDL_armR5CCMSetOperationModeKey(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey opModeKey, int32_t *pMetaInfo)
Configure Operating mode for CPU, VIM, CCM Inactivity monitor.
Definition: sdl_mcu_armss_ccmr5.h:110
int32_t SDL_armR5CCMClearCompareError(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, int32_t *pMetaInfo)
Clear Compare Error value for CPU, VIM, CCM Inactivity monitor.
Definition: sdl_mcu_armss_ccmr5.h:108
Definition: sdl_mcu_armss_ccmr5.h:85
Definition: sdl_mcu_armss_ccmr5.h:81
Definition: sdl_mcu_armss_ccmr5.h:95
int32_t SDL_armR5CCMGetCompareError(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, uint32_t *pCmpError, int32_t *pMetaInfo)
Read Compare Error status for CPU, VIM, CCM Inactivity monitor.
int32_t SDL_armR5ConfigureCCMRegister(uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t valToBeWritten, int32_t *pMetaInfo)
Configure CCM Regiser.
Definition: sdl_mcu_armss_ccmr5.h:125
Definition: sdl_mcu_armss_ccmr5.h:87
Definition: sdl_mcu_armss_ccmr5.h:93
SDL_McuArmssCcmR5OpModeKey
This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 ...
Definition: sdl_mcu_armss_ccmr5.h:123
Definition: sdl_mcu_armss_ccmr5.h:131
Definition: sdl_mcu_armss_ccmr5.h:83
Definition: sdl_mcu_armss_ccmr5.h:91
int32_t SDL_armR5ReadCCMRegister(uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t *pValToBeRead, int32_t *pMetaInfo)
Read CCM Regiser.
int32_t SDL_armR5CCMGetOperationModeKey(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey *pOpModeKey, int32_t *pMetaInfo)
Get Operation mode key value for CPU, VIM, CCM Inactivity monitor.
SDL_McuArmssCcmR5ModuleId
This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs...
Definition: sdl_mcu_armss_ccmr5.h:104
Definition: sdl_mcu_armss_ccmr5.h:129
SDL_McuArmssCcmR5RegId
This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs...
Definition: sdl_mcu_armss_ccmr5.h:79
Definition: sdl_mcu_armss_ccmr5.h:112
Definition: sdl_mcu_armss_ccmr5.h:106
Definition: sdl_mcu_armss_ccmr5.h:89
Definition: sdl_mcu_armss_ccmr5.h:127