![]() |
SDL API Guide for J721E
|
Functions | |
int32_t | SDL_armR5ReadCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t *pValToBeRead, int32_t *pMetaInfo) |
Read CCM Regiser. More... | |
int32_t | SDL_armR5ConfigureCCMRegister (uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t valToBeWritten, int32_t *pMetaInfo) |
Configure CCM Regiser. More... | |
int32_t | SDL_armR5CCMSetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey opModeKey, int32_t *pMetaInfo) |
Configure Operating mode for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMGetCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, uint32_t *pCmpError, int32_t *pMetaInfo) |
Read Compare Error status for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMGetOperationModeKey (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey *pOpModeKey, int32_t *pMetaInfo) |
Get Operation mode key value for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t | SDL_armR5CCMClearCompareError (uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, int32_t *pMetaInfo) |
Clear Compare Error value for CPU, VIM, CCM Inactivity monitor. More... | |
int32_t SDL_armR5ReadCCMRegister | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5RegId | regId, | ||
uint32_t * | pValToBeRead, | ||
int32_t * | pMetaInfo | ||
) |
Read CCM Regiser.
This function reads the contents of a given CCM register and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
regId | [IN] CCMR5 register ID to be read |
pValToBeRead | [OUT] pointer to address of Register value read |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5ConfigureCCMRegister | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5RegId | regId, | ||
uint32_t | valToBeWritten, | ||
int32_t * | pMetaInfo | ||
) |
Configure CCM Regiser.
This function configures a given CCM register and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
regId | [IN] CCMR5 register ID to be configured |
valToBeWritten | [OUT] Register value to be written to |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMSetOperationModeKey | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
SDL_McuArmssCcmR5OpModeKey | opModeKey, | ||
int32_t * | pMetaInfo | ||
) |
Configure Operating mode for CPU, VIM, CCM Inactivity monitor.
This function configures a Operation mode key and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
opModeKey | [OUT] Operating mode to be set in KEY register |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMGetCompareError | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
uint32_t * | pCmpError, | ||
int32_t * | pMetaInfo | ||
) |
Read Compare Error status for CPU, VIM, CCM Inactivity monitor.
This function reads the a Compare Error status and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
pCmpError | [OUT] Pointer to Compare Error for the module |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMGetOperationModeKey | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
SDL_McuArmssCcmR5OpModeKey * | pOpModeKey, | ||
int32_t * | pMetaInfo | ||
) |
Get Operation mode key value for CPU, VIM, CCM Inactivity monitor.
This function reads the a Operation mode key and returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
pOpModeKey | [OUT] Pointer to Operation Mode for the module |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |
int32_t SDL_armR5CCMClearCompareError | ( | uintptr_t | baseAddress, |
SDL_McuArmssCcmR5ModuleId | moduleId, | ||
int32_t * | pMetaInfo | ||
) |
Clear Compare Error value for CPU, VIM, CCM Inactivity monitor.
This function clears the a Compare Error Statusand returns the status of the operation for API caller to indicate success or failure on the operation.
Consult the CCM module documentation for a description of the registers under MCU_ARMSS_CCMR5 registers section of the techinical reference manual https://www.ti.com/lit/pdf/spruid7
baseAddress | [IN] Base address of MCU_ARMSS_CCMR5 registers |
moduleId | [IN] CCMR5 module ID to be configured |
pMetaInfo | [OUT] pointer to meta info (Optional) for SDL_EFAIL: reason for API failure as defined under SDL_ErrType_t for SDL_PASS: Not applicable |