![]() |
PDK API Guide for J721E
|
CPSW CPTS object.
EnetMod_Obj CpswCpts_Obj::enetMod |
EnetMod must be the first member
volatile bool CpswCpts_Obj::tsPushInFifo |
Flag to indicate that a SW push event is already active
uint64_t CpswCpts_Obj::tsVal |
Current time stamp value maintained by driver, gets updated at every TS_PUSH_EVENT
CpswCpts_EventNotifyCb CpswCpts_Obj::eventNotifyCb |
Notify callback function for registered stack
void* CpswCpts_Obj::eventNotifyCbArg |
Notify callback function argument for registered stack
uint32_t CpswCpts_Obj::hwPushCnt |
Maximum hardware push instances supported in hardware
CpswCpts_HwPushNotifyCb CpswCpts_Obj::hwPushNotifyCb[CPSW_CPTS_HWPUSH_COUNT_MAX] |
Hardware push event notify callback function pointers
void* CpswCpts_Obj::hwPushNotifyCbArg[CPSW_CPTS_HWPUSH_COUNT_MAX] |
Hardware push event notify callback function arguments
CpswCpts_EventMemObj CpswCpts_Obj::ethTxEventPool |
Event memory object for ethernet Tx event
CpswCpts_EventMemObj CpswCpts_Obj::ethRxEventPool |
Event memory object for ethernet Rx event
CpswCpts_EventMemObj CpswCpts_Obj::hwPushEventPool |
Event memory object for hardware Ts Push event
CpswCpts_EventMemObj CpswCpts_Obj::cmpEventPool |
Event memory object for compare event
CpswCpts_EventMemObj CpswCpts_Obj::hostTxEventPool |
Event memory object for host Tx event
CpswCpts_EventStats CpswCpts_Obj::eventStats |
Event statistics