![]() |
PDK API Guide for J721E
|
CPTS event.
Data Fields | |
uint64_t | tsVal |
CpswCpts_EventType | eventType |
EnetTimeSync_MsgType | msgType |
uint32_t | seqId |
uint32_t | portNum |
uint32_t | domain |
CpswCpts_HwPush | hwPushNum |
uint64_t CpswCpts_Event::tsVal |
Time stamp value when the event occurred
CpswCpts_EventType CpswCpts_Event::eventType |
CPTS event type information
EnetTimeSync_MsgType CpswCpts_Event::msgType |
CPTS event message type
uint32_t CpswCpts_Event::seqId |
Sequence id of the event
uint32_t CpswCpts_Event::portNum |
MAC port number corresponding to the CPTS event
uint32_t CpswCpts_Event::domain |
Domain number of the event
CpswCpts_HwPush CpswCpts_Event::hwPushNum |
Hardware push instance number which triggered the event